This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP-EXP430FR6968 UART中断RX不工作

Guru**** 2535150 points
Other Parts Discussed in Thread: MSP430FR6989

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1097175/msp-exp430fr6968-uart-interrupt-rx-doesn-t-work

主题中讨论的其他部件:MSP430FR6989

我在 这个线程中使用来自Peter Spevak的代码

所有跳线均已连接。 当我 向PC发送字符时工作正常,但当我尝试从PC接收字符时,中断不会释放。 我使用了德州仪器(TI)的原始代码,使用UCA0, 从 “桥接”接头(J101)上卸下了RXD/TXD跳线,并将WFP 2.0 (J101) 1.8 插针安装到TXD上,将WFP 2.1 (RTOD)插针安装到RXD上,将2.19 (RTOD)插针安装到RXD上,遇到同样的问题。 我可以从launchpad发送字符,但从PC接收(中断不启动)。 有什么想法吗?

/* --COPYRIGHT--,BSD_EX
 * Copyright (c) 2014, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 *******************************************************************************
 *
 *                       MSP430 CODE EXAMPLE DISCLAIMER
 *
 * MSP430 code examples are self-contained low-level programs that typically
 * demonstrate a single peripheral function or device feature in a highly
 * concise manner. For this the code may rely on the device's power-on default
 * register values and settings such as the clock configuration and care must
 * be taken when combining code from several examples to avoid potential side
 * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
 * for an API functional library-approach to peripheral configuration.
 *
 * --/COPYRIGHT--*/
//******************************************************************************
//  MSP430FR69xx Demo - eUSCI_A0 UART echo at 9600 baud using BRCLK = 8MHz
//
//  Description: This demo echoes back characters received via a PC serial port.
//  SMCLK/ DCO is used as a clock source and the device is put in LPM3
//  The auto-clock enable feature is used by the eUSCI and SMCLK is turned off
//  when the UART is idle and turned on when a receive edge is detected.
//  Note that level shifter hardware is needed to shift between RS232 and MSP
//  voltage levels.
//
//  The example code shows proper initialization of registers
//  and interrupts to receive and transmit data.
//  To test code in LPM3, disconnect the debugger.
//
//  ACLK = VLO, MCLK =  DCO = SMCLK = 8MHz
//
//                MSP430FR6989
//             -----------------
//       RST -|     P2.0/UCA0TXD|----> PC (echo)
//            |                 |
//            |                 |
//            |     P2.1/UCA0RXD|<---- PC
//            |                 |
//
//   William Goh
//   Texas Instruments Inc.
//   April 2014
//   Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0
//******************************************************************************
// modified by: Peter Spevak
//
// last change: April 7th 2020
//
// 04/07/2020 changing the UART to eUSCIA1, as this is the UART for
//            backchannel on virtual COM port to PC
//
//*****************************************************************************
#include <msp430.h>

int main(void)
{
  WDTCTL = WDTPW | WDTHOLD;                 // Stop Watchdog

  // Configure GPIO
  //P2SEL0 |= BIT0 | BIT1;                    // USCI_A0 UART operation         // 04/07/2020
  //P2SEL1 &= ~(BIT0 | BIT1);                                                   // 04/07/2020
  P3SEL0 |= BIT4 + BIT5;                    // eUSCI_A1 UART                    // 04/07/2020
  P3SEL1 &= ~(BIT4 + BIT5);                 // eUSCI_A1 UART                    // 04/07/2020

  // Disable the GPIO power-on default high-impedance mode to activate
  // previously configured port settings
  PM5CTL0 &= ~LOCKLPM5;

  // Startup clock system with max DCO setting ~8MHz
  CSCTL0_H = CSKEY >> 8;                    // Unlock clock registers
  CSCTL1 = DCOFSEL_3 | DCORSEL;             // Set DCO to 8MHz
  CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;
  CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1;     // Set all dividers
  CSCTL0_H = 0;                             // Lock CS registers

  // Configure USCI_A0 for UART mode
  /*UCA0CTLW0 = UCSWRST;                      // Put eUSCI in reset             // 04/07/2020
  UCA0CTLW0 |= UCSSEL__SMCLK;               // CLK = SMCLK
  // Baud Rate calculation
  // 8000000/(16*9600) = 52.083
  // Fractional portion = 0.083
  // User's Guide Table 21-4: UCBRSx = 0x04
  // UCBRFx = int ( (52.083-52)*16) = 1
  UCA0BR0 = 52;                             // 8000000/16/9600
  UCA0BR1 = 0x00;
  UCA0MCTLW |= UCOS16 | UCBRF_1 | 0x4900;
  UCA0CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
  UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
*/

  // Configure USCI_A1 for UART mode
  UCA1CTLW0 = UCSWRST;                      // Put eUSCI in reset               // 04/07/2020
  UCA1CTLW0 |= UCSSEL__SMCLK;               // CLK = SMCLK                      // 04/07/2020
  // Baud Rate calculation
  // 8000000/(16*9600) = 52.083
  // Fractional portion = 0.083
  // User's Guide Table 21-4: UCBRSx = 0x04
  // UCBRFx = int ( (52.083-52)*16) = 1
  UCA1BR0 = 52;                             // 8000000/16/9600                  // 04/07/2020
  UCA1BR1 = 0x00;                                                               // 04/07/2020
  UCA1MCTLW |= UCOS16 | UCBRF_1 | 0x4900;                                       // 04/07/2020
  UCA1CTLW0 &= ~UCSWRST;                    // Initialize eUSCI                 // 04/07/2020
  UCA1IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt      // 04/07/2020

  __bis_SR_register(LPM3_bits | GIE);       // Enter LPM3, interrupts enabled
  __no_operation();                         // For debugger
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
  switch(__even_in_range(UCA0IV, USCI_UART_UCTXCPTIFG))
  {
    case USCI_NONE: break;
    case USCI_UART_UCRXIFG:
      while(!(UCA0IFG&UCTXIFG));
      UCA0TXBUF = UCA0RXBUF;
      __no_operation();
      break;
    case USCI_UART_UCTXIFG: break;
    case USCI_UART_UCSTTIFG: break;
    case USCI_UART_UCTXCPTIFG: break;
  }
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)            // 04/07/2020
#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A1_VECTOR))) USCI_A1_ISR (void)
#else
#error Compiler not supported!
#endif
{
  switch(__even_in_range(UCA1IV, USCI_UART_UCTXCPTIFG))
  {
    case USCI_NONE: break;
    case USCI_UART_UCRXIFG:
      while(!(UCA1IFG&UCTXIFG));
      UCA1TXBUF = UCA1RXBUF;
      __no_operation();
      break;
    case USCI_UART_UCTXIFG: break;
    case USCI_UART_UCSTTIFG: break;
    case USCI_UART_UCTXCPTIFG: break;
  }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Jose,

    您是否在使用CCS? 如果正在运行的调试会话可能会干扰Backchannel/PC UART连接。 是否可以尝试刷新程序,终止调试会话,重置设备并再次执行测试?

    此致,

    Evan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的回复Evan,但我提供了您的建议,但不起作用。 我无法从UCA1 (或UCA0)启动中断RX。 是否有人可以在launchpad MSP430FR6989上测试此代码?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您能否说明您的预期配置? 在上面发布的代码中,您使用的是USI_A1。 USI_A1连接到WFP端口3.4 和WFP 3.5 ,它们直接连接到J101跳线。  

    但是,您还会说您正在移除J101上的RXD和TXD跳线,并将WFP 2.0 和WFP 2.1 连接到J101的TXD/RXD ezFET侧。  

    听起来您有一半的配置,一半的配置。 您必须:

    • 将USI_A1与J101上TXD/RXD之间的跳线配合使用
    • 使用USI_A0和一根电线从2.0 和WFP 2.1 连接到J101侧面的TXD/RXD。

    此致,

    Evan