This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR6043:ADC12 -读取多个通道

Guru**** 2538950 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1102427/msp430fr6043-adc12---reading-multiple-channels

部件号:MSP430FR6043

您好,

我尝试从ADC读取2个通道。   问题是我得到其中一个(ADC12MEM0)的值,但另一个不正确,它保持不变(ADC12MEM1)。 我搜索 了其他类似的线程,我的代码似乎没有问题。 转换通过计时器开始。

#include <msp430.h>
#include <stdio.h>
#include <stdlib.h>
#include <math.h>
volatile unsigned int result = 0;

int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;               // Stop WDT

    // GPIO Setup
    P1SEL1 |= BIT0;                         // Configure P.1.0 for ADC
    P1SEL0 |= BIT0;
    P1SEL1 |= BIT1;                         // Configure P1.1 for ADC
    P1SEL0 |= BIT1;

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;

    // Configure ADC12
    ADC12CTL0 = ADC12SHT0_2 | ADC12ON;
    ADC12CTL1 = ADC12SHP;                   // ADCCLK = MODOSC; sampling timer
    ADC12CTL2 |= ADC12RES_2;                // 12-bit conversion results
    ADC12IER0 |= ADC12IE0;                  // Enable ADC conv complete interrupt

    ADC12MCTL0 |= ADC12INCH_0;              // A0 ADC input select; Vref=AVCC // PRESSURE
    ADC12MCTL1 |= ADC12INCH_1+ADC12EOS;              // A1 ADC input select; Vref=AVCC // TEMPERATURE

    // TIMER CONFIGURATION
    WDTCTL = WDTPW | WDTHOLD;               // Stop WDT

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;

    /********** TIMER ***********/
    TA0CCTL0 = CCIE;                        // TACCR0 interrupt enabled
    //TA0CCR0 = 50000;
    TA0CCR0 = 32768/2;
    TA0CTL = TASSEL_1 | MC__CONTINOUS; // He cambiado al ACLK->32768 Hz (antes SMCLK), continuous mode
    __bis_SR_register(LPM0_bits | GIE);     // Enter LPM0 w/ interrupt. Aquí salta la interrupción
    __no_operation();                       // For debugger

    while(!(REFCTL0 & REFGENRDY));          // Wait for reference generator
                                            // to settle

    __bis_SR_register(LPM0_bits + GIE); // LPM0, ADC10_ISR will force exit
    __no_operation();                   // For debug only

}

// Timer0_A0 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = TIMER0_A0_VECTOR
__interrupt void Timer0_A0_ISR (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMER0_A0_VECTOR))) Timer0_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
    TA0CCR0 += 32768/2;
    ADC12CTL0 |= ADC12ENC | ADC12SC;    // Sampling and conversion start
    __bis_SR_register(LPM0_bits + GIE); // LPM0, ADC10_ISR will force exit
    __no_operation();                   // For debug only
}


// ADC interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = ADC12_B_VECTOR
__interrupt void ADC12_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_B_VECTOR))) ADC12_ISR (void)
#else
#error Compiler not supported!
#endif
{
    switch (__even_in_range(ADC12IV, ADC12IV__ADC12RDYIFG))
    {
    float volt;
    float resistance;
    float pressure;
        case ADC12IV__NONE:        break;   // Vector  0:  No interrupt
        case ADC12IV__ADC12OVIFG:  break;   // Vector  2:  ADC12MEMx Overflow
        case ADC12IV__ADC12TOVIFG: break;   // Vector  4:  Conversion time overflow
        case ADC12IV__ADC12HIIFG:  break;   // Vector  6:  ADC12BHI
        case ADC12IV__ADC12LOIFG:  break;   // Vector  8:  ADC12BLO
        case ADC12IV__ADC12INIFG:  break;   // Vector 10:  ADC12BIN
        case ADC12IV__ADC12IFG0:            // Vector 12:  ADC12MEM0 Interrupt // PRESSURE
            result = ADC12MEM0;
            printf("Resultado presion: %d\n",result);
            result = ADC12MEM1;
            printf("Resultado temperatura: %d\n",result);

            __bic_SR_register_on_exit(LPM0_bits); // Exit active CPU
            break;                          // Clear CPUOFF bit from 0(SR)
        case ADC12IV__ADC12IFG1:   break;   // Vector 14:  ADC12MEM1 // TEMPERATURE
        case ADC12IV__ADC12IFG2:   break;   // Vector 16:  ADC12MEM2
        case ADC12IV__ADC12IFG3:   break;   // Vector 18:  ADC12MEM3
        case ADC12IV__ADC12IFG4:   break;   // Vector 20:  ADC12MEM4
        case ADC12IV__ADC12IFG5:   break;   // Vector 22:  ADC12MEM5
        case ADC12IV__ADC12IFG6:   break;   // Vector 24:  ADC12MEM6
        case ADC12IV__ADC12IFG7:   break;   // Vector 26:  ADC12MEM7
        case ADC12IV__ADC12IFG8:   break;   // Vector 28:  ADC12MEM8
        case ADC12IV__ADC12IFG9:   break;   // Vector 30:  ADC12MEM9
        case ADC12IV__ADC12IFG10:  break;   // Vector 32:  ADC12MEM10
        case ADC12IV__ADC12IFG11:  break;   // Vector 34:  ADC12MEM11
        case ADC12IV__ADC12IFG12:  break;   // Vector 36:  ADC12MEM12
        case ADC12IV__ADC12IFG13:  break;   // Vector 38:  ADC12MEM13
        case ADC12IV__ADC12IFG14:  break;   // Vector 40:  ADC12MEM14
        case ADC12IV__ADC12IFG15:  break;   // Vector 42:  ADC12MEM15
        case ADC12IV__ADC12IFG16:  break;   // Vector 44:  ADC12MEM16
        case ADC12IV__ADC12IFG17:  break;   // Vector 46:  ADC12MEM17
        case ADC12IV__ADC12IFG18:  break;   // Vector 48:  ADC12MEM18
        case ADC12IV__ADC12IFG19:  break;   // Vector 50:  ADC12MEM19
        case ADC12IV__ADC12IFG20:  break;   // Vector 52:  ADC12MEM20
        case ADC12IV__ADC12IFG21:  break;   // Vector 54:  ADC12MEM21
        case ADC12IV__ADC12IFG22:  break;   // Vector 56:  ADC12MEM22
        case ADC12IV__ADC12IFG23:  break;   // Vector 58:  ADC12MEM23
        case ADC12IV__ADC12IFG24:  break;   // Vector 60:  ADC12MEM24
        case ADC12IV__ADC12IFG25:  break;   // Vector 62:  ADC12MEM25
        case ADC12IV__ADC12IFG26:  break;   // Vector 64:  ADC12MEM26
        case ADC12IV__ADC12IFG27:  break;   // Vector 66:  ADC12MEM27
        case ADC12IV__ADC12IFG28:  break;   // Vector 68:  ADC12MEM28
        case ADC12IV__ADC12IFG29:  break;   // Vector 70:  ADC12MEM29
        case ADC12IV__ADC12IFG30:  break;   // Vector 72:  ADC12MEM30
        case ADC12IV__ADC12IFG31:  break;   // Vector 74:  ADC12MEM31
        case ADC12IV__ADC12RDYIFG: break;   // Vector 76:  ADC12RDY
        default: break;
    }
}

我是否错过了一些东西?

提前感谢!

Alberto

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,Alberto,

    您需要将ADC12CONSEQx设置为通道序列或重复通道序列。

    此致,

    Evan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我将 ADC12CONSEQ_1添加到此行,如下所示,它工作正常。

    ADC12CTL1 = ADC12SHP + ADC12CONSEQ_1;

    非常感谢您的快速响应。

    此致,

    Alberto