This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F5232:UART RX 中断在 UART 回波示例中无法触发。

Guru**** 2782575 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1117904/msp430f5232-uart-rx-interrupt-fails-to-fire-in-the-uart-echo-example

器件型号:MSP430F5232

大家好、

我在 MSP430´m´ve 发送和接收 UART 等基本工作、如果我签入 while (1)但从未触发中断、则轮询工作正常、我在没有 触发中断的情况下尝试了此示例和 driverlib 示例。

//******************************************************************************
//   MSP430F524x Demo - USCI_A0, UART Echo received character
//                     (ACLK 9600/SMCLK 9600/SMCLK 115200)
//
//   Description: The device will wait in LPM0/LPM3 (based on clock source)
//   until a UART character is received.
//   Then the device will echo the received character.
//   The UART can operate using ACLK at 9600, SMCLK at 115200 or SMCLK at 9600.
//   To configure the UART mode, change the following line:
//
//      #define UART_MODE       SMCLK_115200
//      to any of:
//      #define UART_MODE       SMCLK_115200
//      #define UART_MODE       SMCLK_9600
//      #define UART_MODE       ACLK_9600
//
//   UART RX ISR is used to handle communication.
//   ACLK = 32.768kHz, MCLK = SMCLK = DCO 16MHz.
//
//
//                   MSP430F5249
//                 -----------------
//            /|\ |             P5.4|--- XIN
//             |  |                 |   |
//             ---|RST              |   32kHz
//                |                 |   |
//                |             P5.5|--- XOUT
//                |             P3.4|<------- Receive Data (UCA0RXD)
//                |             P3.3|-------> Transmit Data (UCA0TXD)
//                |                 |
//                |                 |
//
//   Nima Eskandari and Ryan Meredith
//   Texas Instruments Inc.
//   January 2018
//   Built with CCS V7.3
//******************************************************************************

#include "msp430.h"
#include <stdbool.h>
#include <stdint.h>

//******************************************************************************
// UART Initialization *********************************************************
//******************************************************************************

#define SMCLK_115200     0
#define SMCLK_9600      1
#define ACLK_9600       2

#define UART_MODE       SMCLK_115200//SMCLK_115200//

void initUART()
{
    // Configure USCI_A0 for UART mode
    UCA0CTLW0 = UCSWRST;                      // Put eUSCI in reset
#if UART_MODE == SMCLK_115200

    UCA0CTLW0 |= UCSSEL__SMCLK;               // CLK = SMCLK
    // Baud Rate calculation
    // 16000000/(16*115200) = 8.6805
    // Fractional portion = 0.6805
    // Use Table 24-5 in Family User Guide
    UCA0BR0 = 8;                               // 16000000/16/9600
    UCA0BR1 = 0x00;
    UCA0MCTL |= UCOS16 | UCBRF_11 | UCBRS_0;

#elif UART_MODE == SMCLK_9600

    UCA0CTLW0 |= UCSSEL__SMCLK;               // CLK = SMCLK
    // Baud Rate calculation
    // 16000000/(16*9600) = 104.1667
    // Fractional portion = 0.1667
    // Use Table 24-5 in Family User Guide
    UCA0BR0 = 104;                            // 16000000/16/9600
    UCA0BR1 = 0x00;
    UCA0MCTL |= UCOS16 | UCBRF_3 | UCBRS_0;

#elif UART_MODE == ACLK_9600

    UCA0CTLW0 |= UCSSEL__ACLK;               // CLK = ACLK
    // Baud Rate calculation
    // 32768/(9600) = 3.4133
    // Fractional portion = 0.4133
    // Use Table 24-5 in Family User Guide
    UCA0BR0 = 3;                             // 32768/9600
    UCA0BR1 = 0x00;
    UCA0MCTL |= UCBRS_3;    //0x0300 is UCBRSx = 0x03

#else
# error "Please specify baud rate to 115200 or 9600"
#endif

    UCA0CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
    UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
}

//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************

void initGPIO()
{
    P3SEL = BIT3 | BIT4;                        // P3.4,5 = USCI_A0 TXD/RXD
    P5SEL |= BIT4 | BIT5;                         // Select XT1
}

void initClockTo16MHz()
{
    UCSCTL3 |= SELREF_2;                      // Set DCO FLL reference = REFO
    UCSCTL4 |= SELA_0;                        // Set ACLK = XT1CLK
    __bis_SR_register(SCG0);                  // Disable the FLL control loop
    UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx
    UCSCTL1 = DCORSEL_5;                      // Select DCO range 16MHz operation
    UCSCTL2 = FLLD_0 + 487;                   // Set DCO Multiplier for 16MHz
    // (N + 1) * FLLRef = Fdco
    // (487 + 1) * 32768 = 16MHz
    // Set FLL Div = fDCOCLK
    __bic_SR_register(SCG0);                  // Enable the FLL control loop

    // Worst-case settling time for the DCO when the DCO range bits have been
    // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
    // UG for optimization.
    // 32 x 32 x 16 MHz / 32,768 Hz = 500000 = MCLK cycles for DCO to settle
    __delay_cycles(500000);//
    // Loop until XT1,XT2 & DCO fault flag is cleared
    do
    {
        UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags
        SFRIFG1 &= ~OFIFG;                          // Clear fault flags
    }while (SFRIFG1&OFIFG);                         // Test oscillator fault flag
}

uint16_t setVCoreUp(uint8_t level){
    uint32_t PMMRIE_backup, SVSMHCTL_backup, SVSMLCTL_backup;

    //The code flow for increasing the Vcore has been altered to work around
    //the erratum FLASH37.
    //Please refer to the Errata sheet to know if a specific device is affected
    //DO NOT ALTER THIS FUNCTION

    //Open PMM registers for write access
    PMMCTL0_H = 0xA5;

    //Disable dedicated Interrupts
    //Backup all registers
    PMMRIE_backup = PMMRIE;
    PMMRIE &= ~(SVMHVLRPE | SVSHPE | SVMLVLRPE |
            SVSLPE | SVMHVLRIE | SVMHIE |
            SVSMHDLYIE | SVMLVLRIE | SVMLIE |
            SVSMLDLYIE
    );
    SVSMHCTL_backup = SVSMHCTL;
    SVSMLCTL_backup = SVSMLCTL;

    //Clear flags
    PMMIFG = 0;

    //Set SVM highside to new level and check if a VCore increase is possible
    SVSMHCTL = SVMHE | SVSHE | (SVSMHRRL0 * level);

    //Wait until SVM highside is settled
    while((PMMIFG & SVSMHDLYIFG) == 0)
    {
        ;
    }

    //Clear flag
    PMMIFG &= ~SVSMHDLYIFG;

    //Check if a VCore increase is possible
    if((PMMIFG & SVMHIFG) == SVMHIFG)
    {
        //-> Vcc is too low for a Vcore increase
        //recover the previous settings
        PMMIFG &= ~SVSMHDLYIFG;
        SVSMHCTL = SVSMHCTL_backup;

        //Wait until SVM highside is settled
        while((PMMIFG & SVSMHDLYIFG) == 0)
        {
            ;
        }

        //Clear all Flags
        PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
                SVMLVLRIFG | SVMLIFG |
                SVSMLDLYIFG
        );

        //Restore PMM interrupt enable register
        PMMRIE = PMMRIE_backup;
        //Lock PMM registers for write access
        PMMCTL0_H = 0x00;
        //return: voltage not set
        return false;
    }

    //Set also SVS highside to new level
    //Vcc is high enough for a Vcore increase
    SVSMHCTL |= (SVSHRVL0 * level);

    //Wait until SVM highside is settled
    while((PMMIFG & SVSMHDLYIFG) == 0)
    {
        ;
    }

    //Clear flag
    PMMIFG &= ~SVSMHDLYIFG;

    //Set VCore to new level
    PMMCTL0_L = PMMCOREV0 * level;

    //Set SVM, SVS low side to new level
    SVSMLCTL = SVMLE | (SVSMLRRL0 * level) |
            SVSLE | (SVSLRVL0 * level);

    //Wait until SVM, SVS low side is settled
    while((PMMIFG & SVSMLDLYIFG) == 0)
    {
        ;
    }

    //Clear flag
    PMMIFG &= ~SVSMLDLYIFG;
    //SVS, SVM core and high side are now set to protect for the new core level

    //Restore Low side settings
    //Clear all other bits _except_ level settings
    SVSMLCTL &= (SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 +
            SVSMLRRL1 + SVSMLRRL2
    );

    //Clear level settings in the backup register,keep all other bits
    SVSMLCTL_backup &=
            ~(SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 + SVSMLRRL1 + SVSMLRRL2);

    //Restore low-side SVS monitor settings
    SVSMLCTL |= SVSMLCTL_backup;

    //Restore High side settings
    //Clear all other bits except level settings
    SVSMHCTL &= (SVSHRVL0 + SVSHRVL1 +
            SVSMHRRL0 + SVSMHRRL1 +
            SVSMHRRL2
    );

    //Clear level settings in the backup register,keep all other bits
    SVSMHCTL_backup &=
            ~(SVSHRVL0 + SVSHRVL1 + SVSMHRRL0 + SVSMHRRL1 + SVSMHRRL2);

    //Restore backup
    SVSMHCTL |= SVSMHCTL_backup;

    //Wait until high side, low side settled
    while(((PMMIFG & SVSMLDLYIFG) == 0) &&
            ((PMMIFG & SVSMHDLYIFG) == 0))
    {
        ;
    }

    //Clear all Flags
    PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
            SVMLVLRIFG | SVMLIFG | SVSMLDLYIFG
    );

    //Restore PMM interrupt enable register
    PMMRIE = PMMRIE_backup;

    //Lock PMM registers for write access
    PMMCTL0_H = 0x00;

    return true;
}

bool increaseVCoreToLevel2()
{
    uint8_t level = 2;
    uint8_t actlevel;
    bool status = true;

    //Set Mask for Max. level
    level &= PMMCOREV_3;

    //Get actual VCore
    actlevel = PMMCTL0 & PMMCOREV_3;

    //step by step increase or decrease
    while((level != actlevel) && (status == true))
    {
        if(level > actlevel)
        {
            status = setVCoreUp(++actlevel);
        }
    }

    return (status);
}

//******************************************************************************
// Main ************************************************************************
// Enters LPM0 if SMCLK is used and waits for UART interrupts. If ACLK is used *
// then the device will enter LPM3 mode instead. The UART RX interrupt handles *
// the received character and echoes it.                                       *
//******************************************************************************

int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;                 // Stop Watchdog

    initGPIO();
    increaseVCoreToLevel2();
    initClockTo16MHz();
    initUART();

    P1DIR &= ~0x06; //pines del puerto de programación BSL: configurados como entradas.
    P6DIR |=  0x08u;                  // configure P1.0 as output
    P6OUT |= 0x08u;              // toggle P1.0


    long i=0;

    while(1)
    {
        P6OUT ^= 0x08u;              // toggle P1.0
        switch(__even_in_range(UCA0IV,4))
        {
        case 0:break;                             // Vector 0 - no interrupt
        case 2:                                   // Vector 2 - RXIFG
            while (!(UCA0IFG & UCTXIFG));             // USCI_A0 TX buffer ready?
            //UCA0TXBUF = UCA0RXBUF;                  // TX -> RXed character commented to use interrupt.
            break;
        case 4:break;                             // Vector 4 - TXIFG
        default: break;
        }
    }
}

//******************************************************************************
// UART RX Interrupt ***********************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
    switch(__even_in_range(UCA0IV,4))
    {
    case 0:break;                             // Vector 0 - no interrupt
    case 2:                                   // Vector 2 - RXIFG
        while (!(UCA0IFG & UCTXIFG));             // USCI_A0 TX buffer ready?
        UCA0TXBUF = UCA0RXBUF;                  // TX -> RXed character
        break;
    case 4:break;                             // Vector 4 - TXIFG
    default: break;
    }
}

该代码在主函数中以115200波特进行轮询时效果非常好、但中断从未触发、而且我不想这么做。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Javier 好、

    请尝试以下示例:

    https://dev.ti.com/tirex/explore/node?node=AOwdTuDBMI9KI0jX.t9zaw__IOGqZri__LATEST

    谢谢!

    此致

    Johnson

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    不起作用、只是在以防万一的情况下尝试过、但我 已经尝试过 driverlib 示例、没有触发它、尝试使用较旧版本进行编译、以防万一、但运气不佳。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我看不到您在哪里启用中断(GIE)。 尝试添加:

    >_enable_interrupt (); // GIE=1

    示例 Johnson 向您展示了这一点(实际上是__ bis_SR_register (GIE))、因此我不知道您为什么会遇到这个问题。

    主动式:混合轮询(在 main()中读取 UCA0IV)和类似的中断会产生混合结果--大多数 ISR 将获得 Rx 字节,但偶尔主函数将获得该字节。 我建议您不要在 main()中读取 UCA0IV。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢你,不知道为什么要添加 _disable_interrupts();在主代码和  _enable_interrupts()之前;在初始化之后使其工作。

    我知道混合轮询是一件麻烦事、但之所以这样做是因为中断永远不起作用、并且检查它是否是与硬件相关的问题、发现将它包含在主函数中可以将它减少为中断触发问题。