This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F2274-EP:尝试对 LMX2694进行编程

Guru**** 2931100 points

Other Parts Discussed in Thread: MSP430F2274, MSP-FET

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1133703/msp430f2274-ep-trying-to-program-lmx2694

器件型号:MSP430F2274-EP
主题中讨论的其他器件:MSP430F2274MSP-FET

您好!

我正在尝试对 LMX2694 PLL 进行编程。 我有用于它的 EVAL 板以及用于微控制器 MSP430F2274的 EVAL 板。 我使用 N5181信号发生器作为参考振荡器信号。 在使用 MSP-FET 和 TI Code Composer Studio 构建我的项目并将代码加载到微控制器时、PLL 似乎不会输出它应该输出的信号(在频谱分析仪上看不到任何信号); 但是、当我在代码中放置断点然后运行它时、PLL 似乎能够输出信号(在所选频率的频谱分析仪上可以看到锁定信号)。  

我将介绍我用来使 PLL 不工作和工作的两个过程。 在这两种情况下、我都有一个为 PLL 的 EVAL 板供电的电源:  

PLL 不能用于以下过程:
(1)打开 PLL 电源。
(2)将插入的代码加载到微控制器中。 然后微控制器打开并执行整个 int main()。
(3) PLL 不会在频谱分析仪上显示信号。

PLL 使用以下过程:
(1)在调试模式下将插入的代码加载到微控制器中。
(2)加载插入的代码后按"Resume"、int main()将运行到第261行的断点。
(3)此时、微控制器应该已经完成了 CPU 时钟、SPI 总线和 GPIO 端口的初始化。
(4)打开 PLL 电源。
(5)按"恢复"。
(6)代码一直运行到代码末尾第266行上的断点(返回0)。
(7) PLL 能够显示频谱分析仪检测到的信号。

我感觉 PLL 上电时的初始化例程在某种程度上阻止了 PLL 的正确编程。 是这样吗? 当我运行只针对 PLL 的代码时、PLL 看起来工作正常。 也许微控制器会将信号输出到 SPI 总线、以便在 PLL 上电时使其发生混淆? 我可以对此做些什么、还是有人可能提出任何建议? 我认为、微控制器在现场启动后、不会有用于切换 PLL 功率的选项。 谢谢!!

#include <msp430.h> 
#include <stdint.h>

int i;
unsigned int j;
unsigned int t;
volatile char dummy = 0;
volatile char probe1 = 0;
volatile char probe2 = 0;
volatile char probe3 = 0;
volatile char probe4 = 0;
volatile char probe5 = 0;
volatile char probe6 = 0;
volatile char probe7 = 0;
volatile char probe8 = 0;

uint8_t reg_matrix[80][3] =
{
     {0x00, 0x21, 0x14},
     {0x01, 0x08, 0x0C},
     {0x02, 0x05, 0x00},
     {0x03, 0x06, 0x42},
     {0x04, 0x0E, 0x43},
     {0x05, 0x03, 0xE8},
     {0x06, 0x78, 0x02},
     {0x07, 0x00, 0xB2},
     {0x08, 0x20, 0x00},
     {0x09, 0x16, 0x04},
     {0x0A, 0x10, 0xD8},
     {0x0B, 0x00, 0x18},
     {0x0C, 0x50, 0x01},
     {0x0D, 0x40, 0x00},
     {0x0E, 0x1E, 0x70},
     {0x0F, 0x06, 0x4F},
     {0x10, 0x00, 0x80},
     {0x11, 0x01, 0x2C},
     {0x12, 0x00, 0x64},
     {0x13, 0x27, 0xB7},
     {0x14, 0xF8, 0x48},
     {0x15, 0x04, 0x01},
     {0x16, 0x00, 0x01},
     {0x17, 0x00, 0x7C},
     {0x18, 0x07, 0x1A},
     {0x19, 0x06, 0x24},
     {0x1A, 0x0D, 0xB0},
     {0x1B, 0x00, 0x02},
     {0x1C, 0x04, 0x88},
     {0x1D, 0x31, 0x8C},
     {0x1E, 0x31, 0x8C},
     {0x1F, 0x43, 0xEC},
     {0x20, 0x03, 0x93},
     {0x21, 0x1E, 0x21},
     {0x22, 0x00, 0x00},
     {0x23, 0x00, 0x04},
     {0x24, 0x00, 0x36},
     {0x25, 0x84, 0x04},
     {0x26, 0xFD, 0x51},
     {0x27, 0xDA, 0x80},
     {0x28, 0x00, 0x00},
     {0x29, 0x00, 0x00},
     {0x2A, 0x00, 0x00},
     {0x2B, 0x00, 0x00},
     {0x2C, 0x1F, 0x63},
     {0x2D, 0xC8, 0xDF},
     {0x2E, 0x07, 0xFD},
     {0x2F, 0x03, 0x00},
     {0x30, 0x03, 0x00},
     {0x31, 0x41, 0x80},
     {0x32, 0x00, 0x00},
     {0x33, 0x00, 0x80},
     {0x34, 0x04, 0x20},
     {0x35, 0x00, 0x00},
     {0x36, 0x00, 0x00},
     {0x37, 0x00, 0x00},
     {0x38, 0x00, 0x00},
     {0x39, 0x00, 0x20},
     {0x3A, 0x80, 0x01},
     {0x3B, 0x00, 0x01},
     {0x3C, 0x09, 0xC4},
     {0x3D, 0x00, 0xA8},
     {0x3E, 0x03, 0x22},
     {0x3F, 0x00, 0x00},
     {0x40, 0x13, 0x88},
     {0x41, 0x00, 0x00},
     {0x42, 0x01, 0xF4},
     {0x43, 0x00, 0x00},
     {0x44, 0x03, 0xE8},
     {0x45, 0x00, 0x00},
     {0x46, 0xC3, 0x50},
     {0x47, 0x00, 0x80},
     {0x48, 0x00, 0x01},
     {0x49, 0x00, 0x3F},
     {0x4A, 0x00, 0x00},
     {0x4B, 0x08, 0x00},
     {0x4C, 0x00, 0x0C},
     {0x4D, 0x00, 0x00},
     {0x4E, 0x00, 0x64},
     {0x4F, 0x00, 0x00}
};

void delay(unsigned int count)
{
    //P3OUT = 0x00;
        for (t = 0; t<count; ++t)
        {
        }
    //P3OUT = 0x08;
}

void initClockTo16MHz()
{
    if (CALBC1_16MHZ==0xFF)                     // If calibration constant erased
    {
        while(1);                               // do not load, trap CPU!!
    }
    DCOCTL = 0;                                 // Select lowest DCOx and MODx settings
    BCSCTL1 = CALBC1_16MHZ;                     // Set DCO
    DCOCTL = CALDCO_16MHZ;
}

void initSPI()
{
    UCA0CTL1 |= UCSWRST;                        //Performs a software reset on A0.
    UCA0CTL1 |= UCSSEL_2;                       //Using SMCLK.
    UCA0BR0 = 0x0A;                             //Divide by 10 (both UCA0BR0 and UCA0BR1 on the next line set this).
    UCA0BR1 = 0;
    UCA0MCTL = 0;                               //Modulation not used in SPI mode. Clearing UCA0MCTL register.
    UCA0CTL0 = 0xAB;                            //UCCKPH + !UCCKPL + UCMSB + !UC7BIT + UCMST + 4-pin SPI w. ACTIVE Master (2 bits) + Synchronous.
    //UCA0CTL1 = 0x00;                          //Releases the module from being in reset mode and initializes the USCI state machine.
}

void initGPIO()
{
    //initialize GPIO
    P3OUT = 0x00;                               //Reset all channels on port 3.
    P3OUT = 0x0C;
    P3DIR = 0x0C;                               //Configures P3.2 and P3.3 channels to be outputs.
    P3SEL = 0x11;                               //Configures channel 0 to be in UC0CLK mode, channel 4 to be in UC0SIMO mode, and all other channels to be in I/O mode.
    ADC10AE0 = 0;

    //Configure all unused ports to be reset, and configured as outputs in I/O mode to reduce power consumption.
    P1OUT = 0x00;
    P2OUT = 0x00;
    P4OUT = 0x00;

    P1DIR = 0xFF;
    P2DIR = 0xFF;
    P4DIR = 0xFF;

    P1SEL = 0x00;
    P2SEL = 0x00;
    P4SEL = 0x00;

    UCA0CTL1 &= ~UCSWRST;                       //Releases the module from being in reset mode and initializes the USCI state machine.
}

//void writeSPI(char addr, char value)
//{
//    TI_CC_CSn_PxOUT &= ~TI_CC_CSn_PIN; // /CS enable
//    while (TI_CC_SPI_USCIB0_PxIN&TI_CC_SPI_USCIB0_SOMI);// Wait for CCxxxx ready
//    IFG2 &= ~UCB0RXIFG; // Clear flag
//    UCB0TXBUF = addr; // Send address
//    while (!(IFG2&UCB0RXIFG)); // Wait for TX to finish
//    IFG2 &= ~UCB0RXIFG; // Clear flag
//    UCB0TXBUF = value; // Send data
//    while (!(IFG2&UCB0RXIFG)); // Wait for TX to finish
//    TI_CC_CSn_PxOUT |= TI_CC_CSn_PIN; // /CS disable
//}

void init_mainPLL()
{
    //Resets the PLL
    P3OUT = 0x00;                               //Select main PLL
    while (!(IFG2 & UCA0TXIFG));                // USCI_A0 TX buffer ready?
    UCA0TXBUF = 0b00000000;
    while (!(IFG2 & UCA0TXIFG));
    UCA0TXBUF = 0b00100001;
    while (!(IFG2 & UCA0TXIFG));
    UCA0TXBUF = 0b00010110;
    while (!(IFG2 & UCA0RXIFG));                //USCI_A0 RX Received?
    dummy = UCA0RXBUF;                          //Read back from RXBuffer.
    while (!(IFG2 & UCA0TXIFG));                //Ensure buffer is empty before unselecting main PLL
    delay(7);                                   //Delay to allow bits to transfer to PLL
    P3OUT = 0x08;                               //Unselect main PLL

    //Removes reset on PLL
    P3OUT = 0x00;                               //Select main PLL
    while (!(IFG2 & UCA0TXIFG));                //USCI_A0 TX buffer ready?
    UCA0TXBUF = 0b00000000;
    while (!(IFG2 & UCA0TXIFG));
    UCA0TXBUF = 0b00100001;
    while (!(IFG2 & UCA0TXIFG));
    UCA0TXBUF = 0b00010100;
    while (!(IFG2 & UCA0RXIFG));                //USCI_A0 RX Received?
    dummy = UCA0RXBUF;                          //Read back from RXBuffer
    while (!(IFG2 & UCA0TXIFG));                //Ensure buffer is empty before unselecting main PLL
    delay(7);                                   //Delay to allow bits to transfer to PLL
    P3OUT = 0x08;                               //Unselect main PLL
}

void program_mainPLL()
{
    for (i = 79; i>-1; --i)
    {
        P3OUT = 0x00;                           //Select main PLL
        for (j = 0; j<3; ++j)
        {
            while (!(IFG2 & UCA0TXIFG));        // USCI_A0 TX buffer ready?
            UCA0TXBUF = reg_matrix[i][j];       //Send byte
        }
        while (!(IFG2 & UCA0RXIFG));            //USCI_A0 RX Received?
        dummy = UCA0RXBUF;                      //Read back from RXBuffer
        while (!(IFG2 & UCA0TXIFG));
        delay(7);
        P3OUT = 0x08;                           //Unselect main PLL
    }
}

void ready_mainPLL()
{
    P3OUT = 0x00;                               //Select main PLL
    while (!(IFG2 & UCA0TXIFG));                //USCI_A0 TX buffer ready?
    UCA0TXBUF = 0x00;
    while (!(IFG2 & UCA0TXIFG));                //USCI_A0 TX buffer ready?
    UCA0TXBUF = 0x21;
    while (!(IFG2 & UCA0TXIFG));                //USCI_A0 TX buffer ready?
    UCA0TXBUF = 0x1C;
    while (!(IFG2 & UCA0RXIFG));                //USCI_A0 RX Received?
    dummy = UCA0RXBUF;
    while (!(IFG2 & UCA0TXIFG));
    delay(7);
    P3OUT = 0x08;                               //Unselect main PLL
}

void testloop()
{
    while(1)
    {
        while (!(IFG2 & UCA0TXIFG));
        //IFG2 |= UCA0TXIFG;
        probe1 = IFG2;
        probe2 = !(IFG2 & UCA0TXIFG);
        probe3 = UCA0TXBUF;
        probe4 = UCA0RXBUF;
        UCA0TXBUF = 0x4D;
        //IFG2 |= UCA0TXIFG;
        probe5 = IFG2;
        probe6 = !(IFG2 & UCA0TXIFG);
        probe7 = UCA0TXBUF;
        probe8 = UCA0RXBUF;
    }
}

int main(void)
{
    WDTCTL = WDTPW | WDTHOLD;                   //Stop watchdog timer
    initClockTo16MHz();
    initSPI();
    initGPIO();
    //testloop();
    init_mainPLL();
    program_mainPLL();
    delay(1500);
    ready_mainPLL();

    return 0;
}

 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我可以帮助调试与 MSP430相关的代码。 但是、如果我们无法继续、我会将其分配给负责 LMX2694的团队。

    您是否可以访问示波器或逻辑分析仪? 您能否查看工作用例和非工作用例的 SPI 波形以查看是否存在任何重要差异?

    此致、

    Evan

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    P3.2连接到什么? 我想知道这里是否有有关 CE 的内容。

    [编辑:在按下按钮之前完成我的想法。]

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    我似乎无法重复我之前所遇到的问题。 我没有更改任何硬件设置或更改代码、但我对我的所有测试仪器执行了重启电源。
    我在每个子例程的开头使用断点单步执行代码、尝试查看是否有任何瞬变耦合到 CS#线路上、但在单步执行代码时、示波器不会触发、直到出现预期的"init_mainPLL();"例程。
    无论如何、我已经尝试在最后一个小时左右重复此问题、但无法这样做、所以我只想说问题已经解决了。 无论如何、感谢您的帮助!
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢你的帮助。 要回答您的问题、P3.2是系统中另一个 PLL 器件的 CS#引脚。 但是、我的问题似乎只是从设备的功率循环中自行解决、但我非常感谢您的努力!  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    好的。 第二个 PLL 是否位于同一个 SPI 上? 在程序的第二个"半部分"期间、它看起来一直有效 CS 编号(P3.2)、所以它会聆听所有内容。 如果没有其他内容、您可能会在 MUXOUT 上看到总线-线冲突。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您指出这一点
    我 一定会错过这个。 我将确保我修复它。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、它位于同一 SPI 总线上。