Other Parts Discussed in Thread: MSP430F149
大家好、
问题:
MSP430F149的 IPP 目前处于调试阶段、客户编写了简单引导文件和应用文件、并且在引导文件中包含了中断跳转指令。 如果应用文件中没有中断、程序可以执行、一旦应用程序中的串行接收中断被打开、程序就会在串行发送指令之后停止。 串行中断向量也在引导程序中重新定义。
客户想知道原因是什么、它与应用程序中断程序是否相关?
引导程序如下所示:
#include "io430.h"
#include "flash.h"
void USART_Init(void);
void main( void )
{
char i=0;
WDTCTL = WDTPW + WDTHOLD;
flash_init();
USART_Init();
while(1)
{
while (IFG1 & URXIFG0)
{
rec[i]=RXBUF0;
i++;
if(i==count)
{
i=0;
flash_write(rec);
asm(" br &0x8100;");//Jump after receiving the upgrade
}
}
}
}
void USART_Init(void)
{
P3SEL |= BIT4+BIT5; // P3.4,5 is selected as the UART transceiver port
ME1 |= UTXE0 + URXE0; // Enable USART0 transmit and receive
UCTL0 |= CHAR; // 8-bit character
UTCTL0 |= SSEL0; // UCLK = ACLK
UBR00 = 0x03; // 32k/9600 - 3.41
UBR10 = 0x00; //
UMCTL0 = 0x4A; // Modulation
UCTL0 &= ~SWRST; // Initialize the UART0 state machine
IE1 |= URXIE0; // Enable to receive interrupts
// _EINT();
}
#pragma vector=USART0RX_VECTOR
__interrupt void USART0RX_ISR(void)
{
asm(" br &0x81A2;");//Serial interrupt redefined
}
应用程序如下所示:
#include "msp430x14x.h"
#define CPU_F ((double)8000000) //Accurate time delay
#define delay_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0))
#define delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0))
void USART_Init(void);
void main( void )
{
WDTCTL = WDTPW + WDTHOLD;
BCSCTL1 &= ~XT2OFF; //Turn on the XT2 high-frequency crystal oscillator
do
{
IFG1 &= ~OFIFG; //Clear the crystal fail flag
for (char z = 0xFF; z > 0; z--); //Wait for the 8-MHz crystal to oscillation
}
while ((IFG1 & OFIFG)); //Crystal failure flag still present?
BCSCTL2 |= SELM_2 + SELS; //MCLK and SMCLK select high frequency crystal
USART_Init();
P2DIR|=0XFF;
P2OUT=0X00;
delay_ms(2000);
P2OUT=0Xff;
delay_ms(2000);
P2OUT=0X00;
while(1)
{
LPM0;
}
}
#pragma vector=USART0RX_VECTOR
__interrupt void USART0RX_ISR(void)
{
char r;
r=RXBUF0;
P2OUT^=0xFF;
}
void USART_Init(void)
{
P3SEL |= 0x30; // P3.4,5 is selected as the UART transceiver port
ME1 |= UTXE0 + URXE0; // Enable USART0 transmit and receive
UCTL0 |= CHAR; // 8-bit character
UTCTL0 |= SSEL0; // UCLK = ACLK
UBR00 = 0x03; // 32k/9600 - 3.41
UBR10 = 0x00; //
UMCTL0 = 0x4A; // Modulation
UCTL0 &= ~SWRST; // Initialize the UART0 state machine
IE1 |= URXIE0; // Enable to receive interrupts
_EINT();
}
您可以帮助检查此问题吗? 谢谢。
此致、
樱桃