This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP-EXP430F5529LP:连接 d'unmaitre SPI MSP430F5529 A unesclave SPI MSP430FR2433

Guru**** 2782555 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1137800/msp-exp430f5529lp-connection-d-un-maitre-spi-msp430f5529-a-un-esclave-spi-msp430fr2433

器件型号:MSP-EXP430F5529LP
主题中讨论的其他器件:MSP430F5529

Bonjour、

JE drais 连接器、unmsp430F5529 en tant que maiter SPI a un MSP4302433 en vantant que esclave SPI。

JE PREND 滴注代码 CI 滴注口领器:

MSP430F55xx_USCI_SPI_standard_master.c

//******************************************************************************
//   MSP430F552x Demo - USCI_A0, SPI 3-Wire Master multiple byte RX/TX
//
//   Description: SPI master communicates to SPI slave sending and receiving
//   3 different messages of different length. SPI master will enter LPM0 mode
//   while waiting for the messages to be sent/receiving using SPI interrupt.
//   SPI Master will initially wait for a port interrupt in LPM0 mode before
//   starting the SPI communication.
//   ACLK = NA, MCLK = SMCLK = DCO 16MHz.
//
//
//                   MSP430F5529
//                 -----------------
//            /|\ |             P2.0|-> Slave Chip Select (GPIO)
//             |  |                 |
//             ---|RST          P1.5|-> Slave Reset (GPIO)
//                |                 |
//                |             P3.3|-> Data Out (UCA0SIMO)
//                |                 |
//       Button ->|P1.1         P3.4|<- Data In (UCA0SOMI)
//                |                 |
//                |             P2.7|-> Serial Clock Out (UCA0CLK)
//
//   Nima Eskandari
//   Texas Instruments Inc.
//   April 2017
//   Built with CCS V7.0
//******************************************************************************

#include <msp430.h> 
#include <stdint.h>
#include <stdbool.h>


//******************************************************************************
// Example Commands ************************************************************
//******************************************************************************

#define DUMMY   0xFF

#define SLAVE_CS_OUT    P2OUT
#define SLAVE_CS_DIR    P2DIR
#define SLAVE_CS_PIN    BIT0

/* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
 * The slave will send example SlaveTypeX buffers in response.
 *
 * CMD_TYPE_X_MASTER are example commands the master sends to the slave.
 * The slave will initialize itself to receive MasterTypeX example buffers.
 * */

#define CMD_TYPE_0_SLAVE              0
#define CMD_TYPE_1_SLAVE              1
#define CMD_TYPE_2_SLAVE              2

#define CMD_TYPE_0_MASTER              3
#define CMD_TYPE_1_MASTER              4
#define CMD_TYPE_2_MASTER              5

#define TYPE_0_LENGTH              1
#define TYPE_1_LENGTH              2
#define TYPE_2_LENGTH              6

#define MAX_BUFFER_SIZE     20

/* MasterTypeX are example buffers initialized in the master, they will be
 * sent by the master to the slave.
 * SlaveTypeX are example buffers initialized in the slave, they will be
 * sent by the slave to the master.
 * */

uint8_t MasterType0[TYPE_0_LENGTH] = {0x11};
uint8_t MasterType1[TYPE_1_LENGTH]= {8, 9};
uint8_t MasterType2[TYPE_2_LENGTH] = {'F', '4' , '1' , '9', '2', 'B'};

uint8_t SlaveType0[TYPE_0_LENGTH] = {0};
uint8_t SlaveType1[TYPE_1_LENGTH] = {0};
uint8_t SlaveType2[TYPE_2_LENGTH] = {0};


//******************************************************************************
// General SPI State Machine ***************************************************
//******************************************************************************

typedef enum SPI_ModeEnum{
    IDLE_MODE,
    TX_REG_ADDRESS_MODE,
    RX_REG_ADDRESS_MODE,
    TX_DATA_MODE,
    RX_DATA_MODE,
    TIMEOUT_MODE
} SPI_Mode;

/* Used to track the state of the software state machine*/
SPI_Mode MasterMode = IDLE_MODE;

/* The Register Address/Command to use*/
uint8_t TransmitRegAddr = 0;

/* ReceiveBuffer: Buffer used to receive data in the ISR
 * RXByteCtr: Number of bytes left to receive
 * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
 * TransmitBuffer: Buffer used to transmit data in the ISR
 * TXByteCtr: Number of bytes left to transfer
 * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
 * */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;

/* SPI Write and Read Functions */

/* For slave device, writes the data specified in *reg_data
 *
 * reg_addr: The register or command to send to the slave.
 *           Example: CMD_TYPE_0_MASTER
 * *reg_data: The buffer to write
 *           Example: MasterType0
 * count: The length of *reg_data
 *           Example: TYPE_0_LENGTH
 *  */
SPI_Mode SPI_Master_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count);

/* For slave device, read the data specified in slaves reg_addr.
 * The received data is available in ReceiveBuffer
 *
 * reg_addr: The register or command to send to the slave.
 *           Example: CMD_TYPE_0_SLAVE
 * count: The length of data to read
 *           Example: TYPE_0_LENGTH
 *  */
SPI_Mode SPI_Master_ReadReg(uint8_t reg_addr, uint8_t count);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);
void SendUCA0Data(uint8_t val);

void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}


SPI_Mode SPI_Master_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;

    //Copy register data to TransmitBuffer
    CopyArray(reg_data, TransmitBuffer, count);

    TXByteCtr = count;
    RXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    SLAVE_CS_OUT &= ~(SLAVE_CS_PIN);
    SendUCA0Data(TransmitRegAddr);

    __bis_SR_register(CPUOFF + GIE);              // Enter LPM0 w/ interrupts

    SLAVE_CS_OUT |= SLAVE_CS_PIN;
    return MasterMode;
}

SPI_Mode SPI_Master_ReadReg(uint8_t reg_addr, uint8_t count)
{
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;
    RXByteCtr = count;
    TXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    SLAVE_CS_OUT &= ~(SLAVE_CS_PIN);
    SendUCA0Data(TransmitRegAddr);

    __bis_SR_register(CPUOFF + GIE);              // Enter LPM0 w/ interrupts

    SLAVE_CS_OUT |= SLAVE_CS_PIN;
    return MasterMode;
}


void SendUCA0Data(uint8_t val)
{
    while (!(UCA0IFG & UCTXIFG));              // USCI_A0 TX buffer ready?
    UCA0TXBUF = val;
}


//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************

void initClockTo16MHz()
{
    UCSCTL3 |= SELREF_2;                      // Set DCO FLL reference = REFO
    UCSCTL4 |= SELA_2;                        // Set ACLK = REFO
    __bis_SR_register(SCG0);                  // Disable the FLL control loop
    UCSCTL0 = 0x0000;                         // Set lowest possible DCOx, MODx
    UCSCTL1 = DCORSEL_5;                      // Select DCO range 16MHz operation
    UCSCTL2 = FLLD_0 + 487;                   // Set DCO Multiplier for 16MHz
                                              // (N + 1) * FLLRef = Fdco
                                              // (487 + 1) * 32768 = 16MHz
                                              // Set FLL Div = fDCOCLK
    __bic_SR_register(SCG0);                  // Enable the FLL control loop

    // Worst-case settling time for the DCO when the DCO range bits have been
    // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx
    // UG for optimization.
    // 32 x 32 x 16 MHz / 32,768 Hz = 500000 = MCLK cycles for DCO to settle
    __delay_cycles(500000);//
    // Loop until XT1,XT2 & DCO fault flag is cleared
    do
    {
        UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags
        SFRIFG1 &= ~OFIFG;                          // Clear fault flags
    }while (SFRIFG1&OFIFG);                         // Test oscillator fault flag
}

uint16_t setVCoreUp(uint8_t level){
    uint32_t PMMRIE_backup, SVSMHCTL_backup, SVSMLCTL_backup;

    //The code flow for increasing the Vcore has been altered to work around
    //the erratum FLASH37.
    //Please refer to the Errata sheet to know if a specific device is affected
    //DO NOT ALTER THIS FUNCTION

    //Open PMM registers for write access
    PMMCTL0_H = 0xA5;

    //Disable dedicated Interrupts
    //Backup all registers
    PMMRIE_backup = PMMRIE;
    PMMRIE &= ~(SVMHVLRPE | SVSHPE | SVMLVLRPE |
                SVSLPE | SVMHVLRIE | SVMHIE |
                SVSMHDLYIE | SVMLVLRIE | SVMLIE |
                SVSMLDLYIE
                );
    SVSMHCTL_backup = SVSMHCTL;
    SVSMLCTL_backup = SVSMLCTL;

    //Clear flags
    PMMIFG = 0;

    //Set SVM highside to new level and check if a VCore increase is possible
    SVSMHCTL = SVMHE | SVSHE | (SVSMHRRL0 * level);

    //Wait until SVM highside is settled
    while((PMMIFG & SVSMHDLYIFG) == 0)
    {
        ;
    }

    //Clear flag
    PMMIFG &= ~SVSMHDLYIFG;

    //Check if a VCore increase is possible
    if((PMMIFG & SVMHIFG) == SVMHIFG)
    {
        //-> Vcc is too low for a Vcore increase
        //recover the previous settings
        PMMIFG &= ~SVSMHDLYIFG;
        SVSMHCTL = SVSMHCTL_backup;

        //Wait until SVM highside is settled
        while((PMMIFG & SVSMHDLYIFG) == 0)
        {
            ;
        }

        //Clear all Flags
        PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
                     SVMLVLRIFG | SVMLIFG |
                     SVSMLDLYIFG
                     );

        //Restore PMM interrupt enable register
        PMMRIE = PMMRIE_backup;
        //Lock PMM registers for write access
        PMMCTL0_H = 0x00;
        //return: voltage not set
        return false;
    }

    //Set also SVS highside to new level
    //Vcc is high enough for a Vcore increase
    SVSMHCTL |= (SVSHRVL0 * level);

    //Wait until SVM highside is settled
    while((PMMIFG & SVSMHDLYIFG) == 0)
    {
        ;
    }

    //Clear flag
    PMMIFG &= ~SVSMHDLYIFG;

    //Set VCore to new level
    PMMCTL0_L = PMMCOREV0 * level;

    //Set SVM, SVS low side to new level
    SVSMLCTL = SVMLE | (SVSMLRRL0 * level) |
               SVSLE | (SVSLRVL0 * level);

    //Wait until SVM, SVS low side is settled
    while((PMMIFG & SVSMLDLYIFG) == 0)
    {
        ;
    }

    //Clear flag
    PMMIFG &= ~SVSMLDLYIFG;
    //SVS, SVM core and high side are now set to protect for the new core level

    //Restore Low side settings
    //Clear all other bits _except_ level settings
    SVSMLCTL &= (SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 +
                 SVSMLRRL1 + SVSMLRRL2
                 );

    //Clear level settings in the backup register,keep all other bits
    SVSMLCTL_backup &=
        ~(SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 + SVSMLRRL1 + SVSMLRRL2);

    //Restore low-side SVS monitor settings
    SVSMLCTL |= SVSMLCTL_backup;

    //Restore High side settings
    //Clear all other bits except level settings
    SVSMHCTL &= (SVSHRVL0 + SVSHRVL1 +
                 SVSMHRRL0 + SVSMHRRL1 +
                 SVSMHRRL2
                 );

    //Clear level settings in the backup register,keep all other bits
    SVSMHCTL_backup &=
        ~(SVSHRVL0 + SVSHRVL1 + SVSMHRRL0 + SVSMHRRL1 + SVSMHRRL2);

    //Restore backup
    SVSMHCTL |= SVSMHCTL_backup;

    //Wait until high side, low side settled
    while(((PMMIFG & SVSMLDLYIFG) == 0) &&
          ((PMMIFG & SVSMHDLYIFG) == 0))
    {
        ;
    }

    //Clear all Flags
    PMMIFG &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
                SVMLVLRIFG | SVMLIFG | SVSMLDLYIFG
                );

    //Restore PMM interrupt enable register
    PMMRIE = PMMRIE_backup;

    //Lock PMM registers for write access
    PMMCTL0_H = 0x00;

    return true;
}

bool increaseVCoreToLevel2()
{
    uint8_t level = 2;
    uint8_t actlevel;
    bool status = true;

    //Set Mask for Max. level
    level &= PMMCOREV_3;

    //Get actual VCore
    actlevel = PMMCTL0 & PMMCOREV_3;

    //step by step increase or decrease
    while((level != actlevel) && (status == true))
    {
        if(level > actlevel)
        {
            status = setVCoreUp(++actlevel);
        }
    }

    return (status);
}

void initGPIO()
{
  //LEDs
  P1OUT = 0x00;                             // P1 setup for LED & reset output
  P1DIR |= BIT0 + BIT5;

  P4DIR |= BIT7;
  P4OUT &= ~(BIT7);

  //SPI Pins
  P3SEL |= BIT3 + BIT4;                     // P3.3,4 option select
  P2SEL |= BIT7;                            // P2.7 option select

  //Button to initiate transfer
  P1DIR &= ~BIT1;                           // Set P1.1 to inpput direction
  P1REN |= BIT1;                            // Enable P1.1 internal resistance
  P1OUT |= BIT1;                            // Set P1.1 as pull-Up resistance
  P1IES |= BIT1;                            // P1.1 Hi/Lo edge
  P1IFG &= ~BIT1;                           // P1.1 IFG cleared
  P1IE |= BIT1;                             // P1.1 interrupt enabled
}

void initSPI()
{
  //Clock Polarity: The inactive state is high
  //MSB First, 8-bit, Master, 3-pin mode, Synchronous
  UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
  UCA0CTL0 |= UCCKPL + UCMSB + UCMST + UCSYNC;
  UCA0CTL1 |= UCSSEL_2;                     // SMCLK
  UCA0BR0 |= 0x20;                          // /2
  UCA0BR1 = 0;                              //
  UCA0MCTL = 0;                             // No modulation must be cleared for SPI
  UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
  UCA0IE |= UCRXIE;                          // Enable USCI0 RX interrupt

  SLAVE_CS_DIR |= SLAVE_CS_PIN;
  SLAVE_CS_OUT |= SLAVE_CS_PIN;
}


//******************************************************************************
// Main ************************************************************************
// Send and receive three messages containing the example commands *************
//******************************************************************************


int main(void) {
    WDTCTL = WDTPW | WDTHOLD;	// Stop watchdog timer

    increaseVCoreToLevel2();
    initClockTo16MHz();
	initGPIO();
	initSPI();

	P1OUT &= ~BIT5;                           // Now with SPI signals initialized,
	__delay_cycles(100000);
	P1OUT |= BIT5;                            // reset slave
	__delay_cycles(100000);                   // Wait for slave to initialize

	P1OUT |= BIT0;
	__bis_SR_register(LPM0_bits + GIE);       // CPU off, enable interrupts
	SPI_Master_ReadReg(CMD_TYPE_2_SLAVE, TYPE_2_LENGTH);
	CopyArray(ReceiveBuffer, SlaveType2, TYPE_2_LENGTH);

	SPI_Master_ReadReg(CMD_TYPE_1_SLAVE, TYPE_1_LENGTH);
	CopyArray(ReceiveBuffer, SlaveType1, TYPE_1_LENGTH);

	SPI_Master_ReadReg(CMD_TYPE_0_SLAVE, TYPE_0_LENGTH);
	CopyArray(ReceiveBuffer, SlaveType0, TYPE_0_LENGTH);

	SPI_Master_WriteReg(CMD_TYPE_2_MASTER, MasterType2, TYPE_2_LENGTH);
	SPI_Master_WriteReg(CMD_TYPE_1_MASTER, MasterType1, TYPE_1_LENGTH);
	SPI_Master_WriteReg(CMD_TYPE_0_MASTER, MasterType0, TYPE_0_LENGTH);
	__bis_SR_register(LPM0_bits + GIE);
    __no_operation();

	return 0;
}


//******************************************************************************
// SPI Interrupt ***************************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
  uint8_t uca0_rx_val = 0;
  switch(__even_in_range(UCA0IV,4))
  {
    case 0:break;                             // Vector 0 - no interrupt
    case 2:                                   // Vector 2 - RXIFG
        uca0_rx_val = UCA0RXBUF;
        switch (MasterMode)
        {
            case TX_REG_ADDRESS_MODE:
                if (RXByteCtr)
                {
                    MasterMode = RX_DATA_MODE;   // Need to start receiving now
                    //Send Dummy To Start
                    __delay_cycles(2000000);
                    SendUCA0Data(DUMMY);
                }
                else
                {
                    MasterMode = TX_DATA_MODE;        // Continue to transmision with the data in Transmit Buffer
                    //Send First
                    SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                    TXByteCtr--;
                }
                break;

            case TX_DATA_MODE:
                if (TXByteCtr)
                {
                  SendUCA0Data(TransmitBuffer[TransmitIndex++]);
                  TXByteCtr--;
                }
                else
                {
                  //Done with transmission
                  MasterMode = IDLE_MODE;
                  __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
                }
                break;

            case RX_DATA_MODE:
                if (RXByteCtr)
                {
                    ReceiveBuffer[ReceiveIndex++] = uca0_rx_val;
                    //Transmit a dummy
                    RXByteCtr--;
                }
                if (RXByteCtr == 0)
                {
                    MasterMode = IDLE_MODE;
                    __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
                }
                else
                {
                    SendUCA0Data(DUMMY);
                }
                break;

            default:
                __no_operation();
                break;
        }
        __delay_cycles(1000);
        break;
    case 4:break;                             // Vector 4 - TXIFG
    default: break;
  }
}


//******************************************************************************
// PORT1 Interrupt *************************************************************
// Interrupt occurs on button press and initiates the SPI data transfer ********
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=PORT1_VECTOR
__interrupt void Port_1(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(PORT1_VECTOR))) Port_1 (void)
#else
#error Compiler not supported!
#endif
{
  P4OUT ^= BIT7;                            // P1.0 = toggle
  P1IFG &= ~BIT1;                          // P1.1 IFG cleared
  P1IE &= ~BIT1;
  __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
}
ET 代码 CI dessous pour l'esclave:
MSP430F243x_eusci_spi_standard_slave.c
//******************************************************************************
//   MSP430FR243x Demo - eUSCI_A1, 4-Wire SPI Slave multiple-byte RX/TX
//
//   Description: SPI slave communicates with SPI master sending and receiving
//   3 different messages of different length. SPI slave will enter LPM0
//   while waiting for the messages to be sent/received using SPI interrupt.
//
//   ACLK = NA, MCLK = DCO = 16MHz, SMCLK = MCLK / 2 = 8MHz
//
//
//                    MSP430FR2433
//                 -----------------
//            /|\ |              RST|<- Master's GPIO (To reset slave)
//             |  |                 |
//             ---|RST          P2.6|<- Data In (UCA1SIMO)
//                |                 |
//                |             P2.5|-> Data Out (UCA1SOMI)
//                |                 |
//                |             P2.4|<- Serial Clock In (UCA1CLK)
//                |                 |
//                |             P3.1|<- Master's GPIO (UCA1STE)
//
//   James Evans
//   Texas Instruments Inc.
//   May 2021
//   Built with CCS v10.3
//******************************************************************************

#include <msp430.h> 
#include <stdint.h>

//******************************************************************************
// Pin Config ******************************************************************
//******************************************************************************

#define LED_OUT                 P1OUT
#define LED_DIR                 P1DIR
#define LED0_PIN                BIT0


//******************************************************************************
// Example Commands ************************************************************
//******************************************************************************

#define DUMMY                   0xFF

/* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
 * The slave will send example SlaveTypeX buffers in response.
 *
 * CMD_TYPE_X_MASTER are example commands the master sends to the slave.
 * The slave will initialize itself to receive MasterTypeX example buffers.
 * */

#define CMD_TYPE_0_SLAVE        0
#define CMD_TYPE_1_SLAVE        1
#define CMD_TYPE_2_SLAVE        2

#define CMD_TYPE_0_MASTER       3
#define CMD_TYPE_1_MASTER       4
#define CMD_TYPE_2_MASTER       5

#define TYPE_0_LENGTH           1
#define TYPE_1_LENGTH           2
#define TYPE_2_LENGTH           6

#define MAX_BUFFER_SIZE         20

/* MasterTypeX are example buffers initialized in the master, they will be
 * sent by the master to the slave.
 * SlaveTypeX are example buffers initialized in the slave, they will be
 * sent by the slave to the master.
 * */

uint8_t MasterType2 [TYPE_2_LENGTH] = {0};
uint8_t MasterType1 [TYPE_1_LENGTH] = {0, 0};
uint8_t MasterType0 [TYPE_0_LENGTH] = {0};

uint8_t SlaveType2 [TYPE_2_LENGTH]  = {'A', 'B', 'C', 'D', '1', '2'};
uint8_t SlaveType1 [TYPE_1_LENGTH]  = {0x15, 0x16};
uint8_t SlaveType0 [TYPE_0_LENGTH]  = {12};


//******************************************************************************
// General SPI State Machine ***************************************************
//******************************************************************************

typedef enum SPI_ModeEnum{
    IDLE_MODE,
    TX_REG_ADDRESS_MODE,
    RX_REG_ADDRESS_MODE,
    TX_DATA_MODE,
    RX_DATA_MODE,
    TIMEOUT_MODE
} SPI_Mode;

/* Used to track the state of the software state machine*/
SPI_Mode SlaveMode = RX_REG_ADDRESS_MODE;

/* The Register Address/Command to use*/
uint8_t ReceiveRegAddr = 0;

/* ReceiveBuffer: Buffer used to receive data in the ISR
 * RXByteCtr: Number of bytes left to receive
 * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
 * TransmitBuffer: Buffer used to transmit data in the ISR
 * TXByteCtr: Number of bytes left to transfer
 * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
 * */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;

/* Initialized the software state machine according to the received cmd
 *
 * cmd: The command/register address received
 * */
void SPI_Slave_ProcessCMD(uint8_t cmd);

/* The transaction between the slave and master is completed. Uses cmd
 * to do post transaction operations. (Place data from ReceiveBuffer
 * to the corresponding buffer based in the last received cmd)
 *
 * cmd: The command/register address corresponding to the completed
 * transaction
 */
void SPI_Slave_TransactionDone(uint8_t cmd);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);
void SendUCA1Data(uint8_t val);

void SendUCA1Data(uint8_t val)
{
    while (!(UCA1IFG & UCTXIFG));           // USCI_A1 TX buffer ready?
    UCA1TXBUF = val;
}

void SPI_Slave_ProcessCMD(uint8_t cmd)
{
    ReceiveIndex = 0;
    TransmitIndex = 0;
    RXByteCtr = 0;
    TXByteCtr = 0;

    switch (cmd)
    {
        // Send slave device ID (this device's ID)
        case (CMD_TYPE_0_SLAVE):
            SlaveMode = TX_DATA_MODE;
            TXByteCtr = TYPE_0_LENGTH;
            // Fill out the TransmitBuffer
            CopyArray(SlaveType0, TransmitBuffer, TYPE_0_LENGTH);
            // Send next byte
            SendUCA1Data(TransmitBuffer[TransmitIndex++]);
            TXByteCtr--;
            break;

        // Send slave device time (this device's time)
        case (CMD_TYPE_1_SLAVE):
            SlaveMode = TX_DATA_MODE;
            TXByteCtr = TYPE_1_LENGTH;
            // Fill out the TransmitBuffer
            CopyArray(SlaveType1, TransmitBuffer, TYPE_1_LENGTH);
            // Send next byte
            SendUCA1Data(TransmitBuffer[TransmitIndex++]);
            TXByteCtr--;
            break;

        // Send slave device location (this device's location)
        case (CMD_TYPE_2_SLAVE):
            SlaveMode = TX_DATA_MODE;
            TXByteCtr = TYPE_2_LENGTH;
            // Fill out the TransmitBuffer
            CopyArray(SlaveType2, TransmitBuffer, TYPE_2_LENGTH);
            // Send next byte
            SendUCA1Data(TransmitBuffer[TransmitIndex++]);
            TXByteCtr--;
            break;

        case (CMD_TYPE_0_MASTER):
            SlaveMode = RX_DATA_MODE;
            RXByteCtr = TYPE_0_LENGTH;
            break;

        case (CMD_TYPE_1_MASTER):
            SlaveMode = RX_DATA_MODE;
            RXByteCtr = TYPE_1_LENGTH;
            break;

        case (CMD_TYPE_2_MASTER):
            SlaveMode = RX_DATA_MODE;
            RXByteCtr = TYPE_2_LENGTH;
            break;

        default:
            __no_operation();
            break;
    }
}

void SPI_Slave_TransactionDone(uint8_t cmd)
{
    switch (cmd)
    {
        // Slave device ID was sent (this device's ID)
        case (CMD_TYPE_0_SLAVE):
            break;

        // Slave device time was sent (this device's time)
        case (CMD_TYPE_1_SLAVE):
            break;

        // Slave device location was sent (this device's location)
        case (CMD_TYPE_2_SLAVE):
            break;

        case (CMD_TYPE_0_MASTER):
            CopyArray(ReceiveBuffer, MasterType0, TYPE_0_LENGTH);
            break;

        case (CMD_TYPE_1_MASTER):
            CopyArray(ReceiveBuffer, MasterType1, TYPE_1_LENGTH);
            break;

        case (CMD_TYPE_2_MASTER):
            CopyArray(ReceiveBuffer, MasterType2, TYPE_2_LENGTH);
            break;

        default:
            __no_operation();
            break;
    }
}

void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}


//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************

void initSPI()
{
    // Clock polarity select: inactive state is high, MSB first
    // 8-bit data, Synchronous, Slave mode, 4-pin SPI
    UCA1CTLW0 = UCSWRST;                    // **Put eUSCI module in reset**
    UCA1CTLW0 |= UCCKPL | UCMSB | UCSYNC |
                 UCMODE_2;
    UCA1CTLW0 &= ~UCSWRST;                  // **Initialize eUSCI module**
    UCA1IE |= UCRXIE;                       // Enable eUSCI0 RX interrupt
}

void initGPIO()
{
    // Configure LEDs
    LED_OUT &= ~LED0_PIN;
    LED_DIR |= LED0_PIN;

    // Configure eUSCI pins
    P2SEL0 |= BIT4 | BIT5 | BIT6;
    P2SEL1 &= ~(BIT4 | BIT5 | BIT6);
    P3SEL0 |= BIT1;
    P3SEL1 &= ~BIT1;

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;
}

void initClockTo16MHz()
{
    // Configure one FRAM waitstate as required by the device datasheet for MCLK
    // operation beyond 8MHz _before_ configuring the clock system.
    FRCTL0 = FRCTLPW | NWAITS_1;

    __bis_SR_register(SCG0);    // Disable FLL
    CSCTL3 |= SELREF__REFOCLK;  // Set REFO as FLL reference source
    CSCTL0 = 0;                 // Clear DCO and MOD registers
    CSCTL1 &= ~(DCORSEL_7);     // Clear DCO frequency select bits first
    CSCTL1 |= DCORSEL_5;        // Set DCO = 16MHz
    CSCTL2 = FLLD_0 + 487;      // set to fDCOCLKDIV = (FLLN + 1)*(fFLLREFCLK/n)
                                //                   = (487  + 1)*(32.768 kHz/1)
                                //                   = 16MHz

    __delay_cycles(3);
    __bic_SR_register(SCG0);                    // Enable FLL
    while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));  // FLL locked

    CSCTL5 |= DIVM_0 | DIVS_1;                  // MCLK = DCOCLK = 16MHz,
                                                // SMCLK = MCLK/2 = 8MHz
}


//******************************************************************************
// Main ************************************************************************
// Enters LPM0 and waits for SPI interrupts. The data sent from the master is  *
// then interpreted and the device will respond accordingly                    *
//******************************************************************************

int main(void)
{
    // Stop watchdog timer
    WDTCTL = WDTPW | WDTHOLD;

    // Initialize device
    initClockTo16MHz();
    initGPIO();
    initSPI();

    // Enter LPM0 w/interrupts enabled
    __bis_SR_register(LPM0_bits + GIE);
    __no_operation();
    return 0;
}


//******************************************************************************
// SPI Interrupt ***************************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A1_VECTOR))) USCI_A1_ISR (void)
#else
#error Compiler not supported!
#endif
{
    uint8_t uca1_rx_val = 0;
    switch(__even_in_range(UCA1IV, USCI_SPI_UCTXIFG))
    {
        case USCI_NONE: break;
        case USCI_SPI_UCRXIFG:
            uca1_rx_val = UCA1RXBUF;
            UCA1IFG &= ~UCRXIFG;
            switch (SlaveMode)
            {
                case (RX_REG_ADDRESS_MODE):
                    ReceiveRegAddr = uca1_rx_val;
                    SPI_Slave_ProcessCMD(ReceiveRegAddr);
                    break;
                case (RX_DATA_MODE):
                    // Store received byte
                    ReceiveBuffer[ReceiveIndex++] = uca1_rx_val;
                    RXByteCtr--;
                    if (RXByteCtr == 0)
                    {
                        // Done with reception
                        SlaveMode = RX_REG_ADDRESS_MODE;
                        SPI_Slave_TransactionDone(ReceiveRegAddr);
                    }
                    break;
                case (TX_DATA_MODE):
                    if (TXByteCtr > 0)
                    {
                        // Send additional byte
                        SendUCA1Data(TransmitBuffer[TransmitIndex++]);
                        TXByteCtr--;
                    }
                    if (TXByteCtr == 0)
                    {
                        // Done with transmission
                        SlaveMode = RX_REG_ADDRESS_MODE;
                        SPI_Slave_TransactionDone(ReceiveRegAddr);
                    }
                    break;
                default:
                    __no_operation();
                    break;
                }
            break;
        case USCI_SPI_UCTXIFG:
            break;
        default: break;
    }
}
reçu è re a bien effectuer et savoir quels ont ont les donn é es qui ont transmise et reçu è s é t é t é t é t é t é t é t é t é t é t é et souvernir é t é t é t é s é t é t é t é t é t é t é s
感谢 Vos Retours
Code composer Studio 的 Je travaille
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bonjour Maxime、

    Je vous r é ponds en anglais, je ne parles pas assez bien en Français è ne。

    如果您想检查数据包的内容、您可以直接使用逻辑分析仪(如果您有)观察导线、或者在代码中使用断点来查看接收到的数据的内容。 例如、您可以在 CCS 中使用调试器放置断点并检查 ReceiveBuffer 的内容。

    此致、

    Evan

    P.S. 论坛将关闭至第2次会议、因此我们将无法在会议结束前作出响应。 感谢您的耐心!