This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR2355:如何发送16位寄存器地址以进行 I2C 事务读取

Guru**** 2538955 points
Other Parts Discussed in Thread: MSP430FR2355

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1009174/msp430fr2355-how-to-send-16-bit-register-addresses-for-reads-on-i2c-transactions

器件型号:MSP430FR2355
主题中讨论的其他器件:MSPWARE

我一直在使用 MSP430FR2355从几个不同的传感器收集一些数据、并且使用 MSPWare 的标准主代码开始我正在使用的代码。 该代码仅允许8位器件寄存器地址、但我需要具有发送16位寄存器/命令、然后从传感器接收数据的功能。 我已经尝试了几种不同的实现来修改存在的代码、但是 I2C 总线在发送一个寄存器字节后会停止(SCL 低电平和 SDA 高电平)。 因此、TXBUF 中断永远不会再次触发、我一直在等待中断发生、或者我过早从读取函数返回。 您如何建议修改此代码的正确过程? 理想情况下、我希望发送1字节和2字节寄存器地址、因为我所使用的不同传感器具有基于2字节命令的事务处理和1字节寄存器读取事务。

下面随附的是我主要 i2c 功能所基于的代码。

#include <msp430.h> 
#include <stdint.h>
#include <stdbool.h>

//******************************************************************************
// Pin Config ******************************************************************
//******************************************************************************

#define LED0_OUT    P1OUT
#define LED0_DIR    P1DIR
#define LED0_PIN    BIT0

#define LED1_OUT    P6OUT
#define LED1_DIR    P6DIR
#define LED1_PIN    BIT6

#define MAX_BUFFER_SIZE     20

//******************************************************************************
// General I2C State Machine ***************************************************
//******************************************************************************

typedef enum I2C_ModeEnum{
    IDLE_MODE,
    NACK_MODE,
    TX_REG_ADDRESS_MODE,
    RX_REG_ADDRESS_MODE,
    TX_DATA_MODE,
    RX_DATA_MODE,
    SWITCH_TO_RX_MODE,
    SWITHC_TO_TX_MODE,
    TIMEOUT_MODE
} I2C_Mode;


/* Used to track the state of the software state machine*/
I2C_Mode MasterMode = IDLE_MODE;

/* The Register Address/Command to use*/
uint8_t TransmitRegAddr = 0;

/* ReceiveBuffer: Buffer used to receive data in the ISR
 * RXByteCtr: Number of bytes left to receive
 * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
 * TransmitBuffer: Buffer used to transmit data in the ISR
 * TXByteCtr: Number of bytes left to transfer
 * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
 * */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;



/* I2C Write and Read Functions */

/* For slave device with dev_addr, writes the data specified in *reg_data
 *
 * dev_addr: The slave device address.
 *           Example: SLAVE_ADDR
 * reg_addr: The register or command to send to the slave.
 *           Example: CMD_TYPE_0_MASTER
 * *reg_data: The buffer to write
 *           Example: MasterType0
 * count: The length of *reg_data
 *           Example: TYPE_0_LENGTH
 *  */
I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count);

/* For slave device with dev_addr, read the data specified in slaves reg_addr.
 * The received data is available in ReceiveBuffer
 *
 * dev_addr: The slave device address.
 *           Example: SLAVE_ADDR
 * reg_addr: The register or command to send to the slave.
 *           Example: CMD_TYPE_0_SLAVE
 * count: The length of data to read
 *           Example: TYPE_0_LENGTH
 *  */
I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);


I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count)
{
    /* Initialize state machine */
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;
    RXByteCtr = count;
    TXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    /* Initialize slave address and interrupts */
    UCB0I2CSA = dev_addr;
    UCB0IFG &= ~(UCTXIFG + UCRXIFG);       // Clear any pending interrupts
    UCB0IE &= ~UCRXIE;                       // Disable RX interrupt
    UCB0IE |= UCTXIE;                        // Enable TX interrupt

    UCB0CTLW0 |= UCTR + UCTXSTT;             // I2C TX, start condition
    __bis_SR_register(LPM0_bits + GIE);              // Enter LPM0 w/ interrupts

    return MasterMode;

}


I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
    /* Initialize state machine */
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;

    //Copy register data to TransmitBuffer
    CopyArray(reg_data, TransmitBuffer, count);

    TXByteCtr = count;
    RXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    /* Initialize slave address and interrupts */
    UCB0I2CSA = dev_addr;
    UCB0IFG &= ~(UCTXIFG + UCRXIFG);       // Clear any pending interrupts
    UCB0IE &= ~UCRXIE;                       // Disable RX interrupt
    UCB0IE |= UCTXIE;                        // Enable TX interrupt

    UCB0CTLW0 |= UCTR + UCTXSTT;             // I2C TX, start condition
    __bis_SR_register(LPM0_bits + GIE);              // Enter LPM0 w/ interrupts

    return MasterMode;
}

void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}


//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************


void initGPIO()
{
    //LEDs
    LED0_OUT &= ~LED0_PIN;
    LED0_DIR |= LED0_PIN;

    LED1_OUT &= ~LED1_PIN;
    LED1_DIR |= LED1_PIN;

    // I2C pins
    P1SEL0 |= BIT2 | BIT3;
    P1SEL1 &= ~(BIT2 | BIT3);

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;
}

void initClockTo16MHz()
{
    // Configure one FRAM waitstate as required by the device datasheet for MCLK
    // operation beyond 8MHz _before_ configuring the clock system.
    FRCTL0 = FRCTLPW | NWAITS_1;

    // Clock System Setup
    __bis_SR_register(SCG0);                           // disable FLL
    CSCTL3 |= SELREF__REFOCLK;                         // Set REFO as FLL reference source
    CSCTL0 = 0;                                        // clear DCO and MOD registers
    CSCTL1 &= ~(DCORSEL_7);                            // Clear DCO frequency select bits first
    CSCTL1 |= DCORSEL_5;                               // Set DCO = 16MHz
    CSCTL2 = FLLD_0 + 487;                             // DCOCLKDIV = 16MHz
    __delay_cycles(3);
    __bic_SR_register(SCG0);                           // enable FLL
    while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1));         // FLL locked
}

void initI2C()
{
    UCB0CTLW0 = UCSWRST;                      // Enable SW reset
    UCB0CTLW0 |= UCMODE_3 | UCMST | UCSSEL__SMCLK | UCSYNC; // I2C master mode, SMCLK
    UCB0BRW = 160;                            // fSCL = SMCLK/160 = ~100kHz
    UCB0I2CSA = 0x00;                         // Slave Address
    UCB0CTLW0 &= ~UCSWRST;                    // Clear SW reset, resume operation
    UCB0IE |= UCNACKIE;
}


//******************************************************************************
// Main ************************************************************************
// Send and receive three messages containing the example commands *************
//******************************************************************************

int main(void) {
    WDTCTL = WDTPW | WDTHOLD;	// Stop watchdog timer
    initClockTo16MHz();
    initGPIO();
    initI2C();
    
    while(1) {
        // specific functionality here
    }

    __bis_SR_register(LPM0_bits + GIE);
	return 0;
}


//******************************************************************************
// I2C Interrupt ***************************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B0_VECTOR
__interrupt void USCI_B0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_B0_ISR (void)
#else
#error Compiler not supported!
#endif
{
  //Must read from UCB0RXBUF
  uint8_t rx_val = 0;
  switch(__even_in_range(UCB0IV, USCI_I2C_UCBIT9IFG))
  {
    case USCI_NONE:          break;         // Vector 0: No interrupts
    case USCI_I2C_UCALIFG:   break;         // Vector 2: ALIFG
    case USCI_I2C_UCNACKIFG:                // Vector 4: NACKIFG
      break;
    case USCI_I2C_UCSTTIFG:  break;         // Vector 6: STTIFG
    case USCI_I2C_UCSTPIFG:  break;         // Vector 8: STPIFG
    case USCI_I2C_UCRXIFG3:  break;         // Vector 10: RXIFG3
    case USCI_I2C_UCTXIFG3:  break;         // Vector 12: TXIFG3
    case USCI_I2C_UCRXIFG2:  break;         // Vector 14: RXIFG2
    case USCI_I2C_UCTXIFG2:  break;         // Vector 16: TXIFG2
    case USCI_I2C_UCRXIFG1:  break;         // Vector 18: RXIFG1
    case USCI_I2C_UCTXIFG1:  break;         // Vector 20: TXIFG1
    case USCI_I2C_UCRXIFG0:                 // Vector 22: RXIFG0
        rx_val = UCB0RXBUF;
        if (RXByteCtr)
        {
          ReceiveBuffer[ReceiveIndex++] = rx_val;
          RXByteCtr--;
        }

        if (RXByteCtr == 1)
        {
          UCB0CTLW0 |= UCTXSTP;
        }
        else if (RXByteCtr == 0)
        {
          UCB0IE &= ~UCRXIE;
          MasterMode = IDLE_MODE;
          __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
        }
        break;
    case USCI_I2C_UCTXIFG0:                 // Vector 24: TXIFG0
        switch (MasterMode)
        {
          case TX_REG_ADDRESS_MODE:
              UCB0TXBUF = TransmitRegAddr;
              if (RXByteCtr)
                  MasterMode = SWITCH_TO_RX_MODE;   // Need to start receiving now
              else
                  MasterMode = TX_DATA_MODE;        // Continue to transmision with the data in Transmit Buffer
              break;

          case SWITCH_TO_RX_MODE:
              UCB0IE |= UCRXIE;              // Enable RX interrupt
              UCB0IE &= ~UCTXIE;             // Disable TX interrupt
              UCB0CTLW0 &= ~UCTR;            // Switch to receiver
              MasterMode = RX_DATA_MODE;    // State state is to receive data
              UCB0CTLW0 |= UCTXSTT;          // Send repeated start
              if (RXByteCtr == 1)
              {
                  //Must send stop since this is the N-1 byte
                  while((UCB0CTLW0 & UCTXSTT));
                  UCB0CTLW0 |= UCTXSTP;      // Send stop condition
              }
              break;

          case TX_DATA_MODE:
              if (TXByteCtr)
              {
                  UCB0TXBUF = TransmitBuffer[TransmitIndex++];
                  TXByteCtr--;
              }
              else
              {
                  //Done with transmission
                  UCB0CTLW0 |= UCTXSTP;     // Send stop condition
                  MasterMode = IDLE_MODE;
                  UCB0IE &= ~UCTXIE;                       // disable TX interrupt
                  __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
              }
              break;

          default:
              __no_operation();
              break;
        }
        break;
    default: break;
  }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这应该非常简单。 您所需要的只是状态机中的一个额外状态。 在新的发送16位地址状态下开始。 在 ISR 中、这会发送地址的第一个字节并将下一个状态设置为字节地址状态、以便它可以发送地址的第二个字节并照常继续。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我第二天尝试了此修复、一旦它超过 TX_REG_ADDRESS_MODE 状态、总线就会停止。 但是、我认为问题可能出在上拉。 I2C 接口是否需要外部10K 上拉电阻器而不是内部30K 上拉电阻器、因为我在设计中没有尝试过外部上拉电阻器?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    上拉电阻器值取决于寄生总线电容和所需的边沿速度。 (开漏输出强度也是如此。) 互联网上有大量的资源来描述这一点。

    如果您获得一个到从器件地址的 ACK、内部上拉电阻器可能是可以的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    使用您所述的状态机(我已经发布了一些代码段)、TX 中断根本不会触发、即使是使用内部上拉电阻器也是如此。 我目前没有在示波器上、因此我无法验证线路在执行什么操作、但我知道中断没有执行。

    ...
    I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint16_t reg_addr, bool long_addr, uint8_t *reg_data, uint8_t count)
    {
        /* Initialize state machine */
        if (long_addr) { // long_addr indicates a 2 byte addr/command
            MasterMode = TX_REG_ADDRESS_MODE_MSB;
        } else {
            MasterMode = TX_REG_ADDRESS_MODE_LSB;
        }
        TransmitRegAddr_MSB = (uint8_t)reg_addr >> 8;
        TransmitRegAddr_LSB = (uint8_t)reg_addr;
    ...
    
    ...
    case USCI_I2C_UCTXIFG0:                 // Vector 24: TXIFG0
            switch (MasterMode)
            {
              case TX_REG_ADDRESS_MODE_MSB:
                  UCB0TXBUF = TransmitRegAddr_MSB;
                  MasterMode = TX_REG_ADDRESS_MODE_LSB;
                  break;
    
              case TX_REG_ADDRESS_MODE_LSB:
                  UCB0TXBUF = TransmitRegAddr_LSB;
                  if (RXByteCtr)
                      MasterMode = SWITCH_TO_RX_MODE;   // Need to start receiving now
                  else
                      MasterMode = TX_DATA_MODE;        // Continue to transmision with the data in Transmit Buffer
                  break;
    ...