This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5994:借助适用于 MSP430FR5994的 GCC 编译器移植 Compute Through Power Loss Fram 实用程序

Guru**** 2535130 points
Other Parts Discussed in Thread: MSP430FR5994

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/991321/msp430fr5994-help-in-porting-compute-through-power-loss-fram-utility-with-gcc-compiler-for-msp430fr5994

器件型号:MSP430FR5994

我正在尝试使用适用于 MSP430FR5994的 GNU v8.3.0.16编译器移植 Compute Through Power Loss FRAM 实用程序。

  通过此主题、我了解 到需要从 TI 编译器移植到 GCC 的两个组件是链接器文件(将除堆栈之外的所有 RAM 数据放入 FRAM 中)和低级汇编例程。 我更新了低级汇编文件、并使用5994的默认链接器、

我能够从 Resource Explorer 编译示例代码(用于检查点的内部 ADC 监控)、但代码看起来不起作用。 GPIO 切换本身并不重要。  

通过 此线程 ,我能够重新解决 问题,并尝试修改链接器文件(适用于5994器件),甚至是看门狗计时器问题,但出于某种原因,它不会使用更新的链接器文件进行编译。 (我这样比较了示例代码中的链接器文件,该示例代码使用 TI 编译器进行编译)

我在 这里附加了项目 e2e.ti.com/.../ctpl_5F00_with_5F00_gcc_5F00_debug.zip -它带有默认链接器。

未编译的更新链接器文件就是这样   

/* ============================================================================ */
/* Copyright (c) 2015, Texas Instruments Incorporated                           */
/*  All rights reserved.                                                        */
/*                                                                              */
/*  Redistribution and use in source and binary forms, with or without          */
/*  modification, are permitted provided that the following conditions          */
/*  are met:                                                                    */
/*                                                                              */
/*  *  Redistributions of source code must retain the above copyright           */
/*     notice, this list of conditions and the following disclaimer.            */
/*                                                                              */
/*  *  Redistributions in binary form must reproduce the above copyright        */
/*     notice, this list of conditions and the following disclaimer in the      */
/*     documentation and/or other materials provided with the distribution.     */
/*                                                                              */
/*  *  Neither the name of Texas Instruments Incorporated nor the names of      */
/*     its contributors may be used to endorse or promote products derived      */
/*     from this software without specific prior written permission.            */
/*                                                                              */
/*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" */
/*  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,       */
/*  THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR      */
/*  PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR            */
/*  CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,       */
/*  EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,         */
/*  PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; */
/*  OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,    */
/*  WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR     */
/*  OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,              */
/*  EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.                          */
/* ============================================================================ */

/* This file supports MSP430FR5994 devices. */
/* Default linker script, for normal executables */

/* 1.207 */

OUTPUT_ARCH(msp430)
ENTRY(_start)

MEMORY {
  TINYRAM          : ORIGIN = 0xA, LENGTH = 0x0016
  BSL              : ORIGIN = 0x1000, LENGTH = 0x0800
  RAM              : ORIGIN = 0x1C00, LENGTH = 0x1000
  LEARAM           : ORIGIN = 0x2C00, LENGTH = 0x0EC8
  LEASTACK         : ORIGIN = 0x3AC8, LENGTH = 0x0138
  INFOMEM          : ORIGIN = 0x1800, LENGTH = 0x0200
  INFOD            : ORIGIN = 0x1800, LENGTH = 0x0080
  INFOC            : ORIGIN = 0x1880, LENGTH = 0x0080
  INFOB            : ORIGIN = 0x1900, LENGTH = 0x0080
  INFOA            : ORIGIN = 0x1980, LENGTH = 0x0080
  FRAM	           : ORIGIN = 0x4000, LENGTH = 0xBF80 /* END=0xFF7F, size 49024 */
  FRAM2	           : ORIGIN = 0x10000, LENGTH = 0x34000
  HIFRAM (rxw)     : ORIGIN = 0x00010000, LENGTH = 0x00033FFF
  JTAGSIGNATURE    : ORIGIN = 0xFF80, LENGTH = 0x0004
  BSLSIGNATURE     : ORIGIN = 0xFF84, LENGTH = 0x0004
  IPESIGNATURE     : ORIGIN = 0xFF88, LENGTH = 0x0008
  VECT0           : ORIGIN = 0xFF90, LENGTH = 0x0002
  VECT1           : ORIGIN = 0xFF92, LENGTH = 0x0002
  VECT2           : ORIGIN = 0xFF94, LENGTH = 0x0002
  VECT3           : ORIGIN = 0xFF96, LENGTH = 0x0002
  VECT4           : ORIGIN = 0xFF98, LENGTH = 0x0002
  VECT5           : ORIGIN = 0xFF9A, LENGTH = 0x0002
  VECT6           : ORIGIN = 0xFF9C, LENGTH = 0x0002
  VECT7           : ORIGIN = 0xFF9E, LENGTH = 0x0002
  VECT8           : ORIGIN = 0xFFA0, LENGTH = 0x0002
  VECT9           : ORIGIN = 0xFFA2, LENGTH = 0x0002
  VECT10           : ORIGIN = 0xFFA4, LENGTH = 0x0002
  VECT11           : ORIGIN = 0xFFA6, LENGTH = 0x0002
  VECT12           : ORIGIN = 0xFFA8, LENGTH = 0x0002
  VECT13           : ORIGIN = 0xFFAA, LENGTH = 0x0002
  VECT14           : ORIGIN = 0xFFAC, LENGTH = 0x0002
  VECT15           : ORIGIN = 0xFFAE, LENGTH = 0x0002
  VECT16           : ORIGIN = 0xFFB0, LENGTH = 0x0002
  VECT17           : ORIGIN = 0xFFB2, LENGTH = 0x0002
  VECT18           : ORIGIN = 0xFFB4, LENGTH = 0x0002
  VECT19           : ORIGIN = 0xFFB6, LENGTH = 0x0002
  VECT20           : ORIGIN = 0xFFB8, LENGTH = 0x0002
  VECT21           : ORIGIN = 0xFFBA, LENGTH = 0x0002
  VECT22           : ORIGIN = 0xFFBC, LENGTH = 0x0002
  VECT23           : ORIGIN = 0xFFBE, LENGTH = 0x0002
  VECT24           : ORIGIN = 0xFFC0, LENGTH = 0x0002
  VECT25           : ORIGIN = 0xFFC2, LENGTH = 0x0002
  VECT26           : ORIGIN = 0xFFC4, LENGTH = 0x0002
  VECT27           : ORIGIN = 0xFFC6, LENGTH = 0x0002
  VECT28           : ORIGIN = 0xFFC8, LENGTH = 0x0002
  VECT29           : ORIGIN = 0xFFCA, LENGTH = 0x0002
  VECT30           : ORIGIN = 0xFFCC, LENGTH = 0x0002
  VECT31           : ORIGIN = 0xFFCE, LENGTH = 0x0002
  VECT32           : ORIGIN = 0xFFD0, LENGTH = 0x0002
  VECT33           : ORIGIN = 0xFFD2, LENGTH = 0x0002
  VECT34           : ORIGIN = 0xFFD4, LENGTH = 0x0002
  VECT35           : ORIGIN = 0xFFD6, LENGTH = 0x0002
  VECT36           : ORIGIN = 0xFFD8, LENGTH = 0x0002
  VECT37           : ORIGIN = 0xFFDA, LENGTH = 0x0002
  VECT38           : ORIGIN = 0xFFDC, LENGTH = 0x0002
  VECT39           : ORIGIN = 0xFFDE, LENGTH = 0x0002
  VECT40           : ORIGIN = 0xFFE0, LENGTH = 0x0002
  VECT41           : ORIGIN = 0xFFE2, LENGTH = 0x0002
  VECT42           : ORIGIN = 0xFFE4, LENGTH = 0x0002
  VECT43           : ORIGIN = 0xFFE6, LENGTH = 0x0002
  VECT44           : ORIGIN = 0xFFE8, LENGTH = 0x0002
  VECT45           : ORIGIN = 0xFFEA, LENGTH = 0x0002
  VECT46           : ORIGIN = 0xFFEC, LENGTH = 0x0002
  VECT47           : ORIGIN = 0xFFEE, LENGTH = 0x0002
  VECT48           : ORIGIN = 0xFFF0, LENGTH = 0x0002
  VECT49           : ORIGIN = 0xFFF2, LENGTH = 0x0002
  VECT50           : ORIGIN = 0xFFF4, LENGTH = 0x0002
  VECT51           : ORIGIN = 0xFFF6, LENGTH = 0x0002
  VECT52           : ORIGIN = 0xFFF8, LENGTH = 0x0002
  VECT53           : ORIGIN = 0xFFFA, LENGTH = 0x0002
  VECT54           : ORIGIN = 0xFFFC, LENGTH = 0x0002
  RESETVEC         : ORIGIN = 0xFFFE, LENGTH = 0x0002
}

SECTIONS
{
  .leaRAM             : {} > LEARAM
  .jtagsignature      : {} > JTAGSIGNATURE
  .bslsignature       : {} > BSLSIGNATURE
  .ipe :
  {
    KEEP (*(.ipesignature))
    KEEP (*(.jtagpassword))
  } > IPESIGNATURE

  __interrupt_vector_0   : { KEEP (*(__interrupt_vector_0  )) } > VECT0
  __interrupt_vector_1   : { KEEP (*(__interrupt_vector_1  )) } > VECT1
  __interrupt_vector_2   : { KEEP (*(__interrupt_vector_2  )) } > VECT2
  __interrupt_vector_3   : { KEEP (*(__interrupt_vector_3  )) } > VECT3
  __interrupt_vector_4   : { KEEP (*(__interrupt_vector_4  )) } > VECT4
  __interrupt_vector_5   : { KEEP (*(__interrupt_vector_5  )) } > VECT5
  __interrupt_vector_6   : { KEEP (*(__interrupt_vector_6  )) } > VECT6
  __interrupt_vector_7   : { KEEP (*(__interrupt_vector_7  )) } > VECT7
  __interrupt_vector_8   : { KEEP (*(__interrupt_vector_8  )) } > VECT8
  __interrupt_vector_9   : { KEEP (*(__interrupt_vector_9  )) } > VECT9
  __interrupt_vector_10   : { KEEP (*(__interrupt_vector_10  )) } > VECT10
  __interrupt_vector_11   : { KEEP (*(__interrupt_vector_11  )) } > VECT11
  __interrupt_vector_12   : { KEEP (*(__interrupt_vector_12  )) } > VECT12
  __interrupt_vector_13   : { KEEP (*(__interrupt_vector_13  )) } > VECT13
  __interrupt_vector_14   : { KEEP (*(__interrupt_vector_14  )) } > VECT14
  __interrupt_vector_15   : { KEEP (*(__interrupt_vector_15  )) } > VECT15
  __interrupt_vector_16   : { KEEP (*(__interrupt_vector_16  )) } > VECT16
  __interrupt_vector_17   : { KEEP (*(__interrupt_vector_17  )) } > VECT17
  __interrupt_vector_18  : { KEEP (*(__interrupt_vector_18)) KEEP (*(__interrupt_vector_lea)) } > VECT18
  __interrupt_vector_19  : { KEEP (*(__interrupt_vector_19)) KEEP (*(__interrupt_vector_port8)) } > VECT19
  __interrupt_vector_20  : { KEEP (*(__interrupt_vector_20)) KEEP (*(__interrupt_vector_port7)) } > VECT20
  __interrupt_vector_21  : { KEEP (*(__interrupt_vector_21)) KEEP (*(__interrupt_vector_eusci_b3)) } > VECT21
  __interrupt_vector_22  : { KEEP (*(__interrupt_vector_22)) KEEP (*(__interrupt_vector_eusci_b2)) } > VECT22
  __interrupt_vector_23  : { KEEP (*(__interrupt_vector_23)) KEEP (*(__interrupt_vector_eusci_b1)) } > VECT23
  __interrupt_vector_24  : { KEEP (*(__interrupt_vector_24)) KEEP (*(__interrupt_vector_eusci_a3)) } > VECT24
  __interrupt_vector_25  : { KEEP (*(__interrupt_vector_25)) KEEP (*(__interrupt_vector_eusci_a2)) } > VECT25
  __interrupt_vector_26  : { KEEP (*(__interrupt_vector_26)) KEEP (*(__interrupt_vector_port6)) } > VECT26
  __interrupt_vector_27  : { KEEP (*(__interrupt_vector_27)) KEEP (*(__interrupt_vector_port5)) } > VECT27
  __interrupt_vector_28  : { KEEP (*(__interrupt_vector_28)) KEEP (*(__interrupt_vector_timer4_a1)) } > VECT28
  __interrupt_vector_29  : { KEEP (*(__interrupt_vector_29)) KEEP (*(__interrupt_vector_timer4_a0)) } > VECT29
  __interrupt_vector_30  : { KEEP (*(__interrupt_vector_30)) KEEP (*(__interrupt_vector_aes256)) } > VECT30
  __interrupt_vector_31  : { KEEP (*(__interrupt_vector_31)) KEEP (*(__interrupt_vector_rtc_c)) } > VECT31
  __interrupt_vector_32  : { KEEP (*(__interrupt_vector_32)) KEEP (*(__interrupt_vector_port4)) } > VECT32
  __interrupt_vector_33  : { KEEP (*(__interrupt_vector_33)) KEEP (*(__interrupt_vector_port3)) } > VECT33
  __interrupt_vector_34  : { KEEP (*(__interrupt_vector_34)) KEEP (*(__interrupt_vector_timer3_a1)) } > VECT34
  __interrupt_vector_35  : { KEEP (*(__interrupt_vector_35)) KEEP (*(__interrupt_vector_timer3_a0)) } > VECT35
  __interrupt_vector_36  : { KEEP (*(__interrupt_vector_36)) KEEP (*(__interrupt_vector_port2)) } > VECT36
  __interrupt_vector_37  : { KEEP (*(__interrupt_vector_37)) KEEP (*(__interrupt_vector_timer2_a1)) } > VECT37
  __interrupt_vector_38  : { KEEP (*(__interrupt_vector_38)) KEEP (*(__interrupt_vector_timer2_a0)) } > VECT38
  __interrupt_vector_39  : { KEEP (*(__interrupt_vector_39)) KEEP (*(__interrupt_vector_port1)) } > VECT39
  __interrupt_vector_40  : { KEEP (*(__interrupt_vector_40)) KEEP (*(__interrupt_vector_timer1_a1)) } > VECT40
  __interrupt_vector_41  : { KEEP (*(__interrupt_vector_41)) KEEP (*(__interrupt_vector_timer1_a0)) } > VECT41
  __interrupt_vector_42  : { KEEP (*(__interrupt_vector_42)) KEEP (*(__interrupt_vector_dma)) } > VECT42
  __interrupt_vector_43  : { KEEP (*(__interrupt_vector_43)) KEEP (*(__interrupt_vector_eusci_a1)) } > VECT43
  __interrupt_vector_44  : { KEEP (*(__interrupt_vector_44)) KEEP (*(__interrupt_vector_timer0_a1)) } > VECT44
  __interrupt_vector_45  : { KEEP (*(__interrupt_vector_45)) KEEP (*(__interrupt_vector_timer0_a0)) } > VECT45
  __interrupt_vector_46  : { KEEP (*(__interrupt_vector_46)) KEEP (*(__interrupt_vector_adc12_b)) } > VECT46
  __interrupt_vector_47  : { KEEP (*(__interrupt_vector_47)) KEEP (*(__interrupt_vector_eusci_b0)) } > VECT47
  __interrupt_vector_48  : { KEEP (*(__interrupt_vector_48)) KEEP (*(__interrupt_vector_eusci_a0)) } > VECT48
  __interrupt_vector_49  : { KEEP (*(__interrupt_vector_49)) KEEP (*(__interrupt_vector_wdt)) } > VECT49
  __interrupt_vector_50  : { KEEP (*(__interrupt_vector_50)) KEEP (*(__interrupt_vector_timer0_b1)) } > VECT50
  __interrupt_vector_51  : { KEEP (*(__interrupt_vector_51)) KEEP (*(__interrupt_vector_timer0_b0)) } > VECT51
  __interrupt_vector_52  : { KEEP (*(__interrupt_vector_52)) KEEP (*(__interrupt_vector_comp_e)) } > VECT52
  __interrupt_vector_53  : { KEEP (*(__interrupt_vector_53)) KEEP (*(__interrupt_vector_unmi)) } > VECT53
  __interrupt_vector_54  : { KEEP (*(__interrupt_vector_54)) KEEP (*(__interrupt_vector_sysnmi)) } > VECT54
  __reset_vector         : { KEEP (*(__interrupt_vector_55)) KEEP (*(__interrupt_vector_reset)) KEEP (*(.resetvec)) } > RESETVEC

  .lower.rodata :
  {
    . = ALIGN(2);
    *(.lower.rodata.* .lower.rodata)
  } > ROM

  .rodata :
  {
    . = ALIGN(2);
    *(.plt)
    *(.rodata .rodata.* .gnu.linkonce.r.* .const .const:*)
    *(.rodata1)
    *(.lower.rodata.* .lower.rodata)
	/* Note: By default we do not have this line:

         *(.either.rodata.*) *(.either.rodata)

       defined here, or anywhere else in this script.  This is deliberate.
       The algorithm in the linker that automatically places rodata into
       either the .rodata or the .upper.rodata sections relies upon the
       fact that the .either.rodata section is not defined, and that the
       .upper.rodata section is defined.  If the .upper.rodata is not
       defined in this script then the line above should be restored so that
       code compiled with -mdata-region=either enabled will still work.

       The same reasoning applies to the absence of definitions for the
       .either.text, .either.data and .either.bss sections as well.  */
	*(.eh_frame_hdr)
    KEEP (*(.eh_frame))
    KEEP (*(.gcc_except_table)) *(.gcc_except_table.*)
    PROVIDE (__preinit_array_start = .);
    KEEP (*(.preinit_array))
    PROVIDE (__preinit_array_end = .);
    PROVIDE (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array))
    PROVIDE (__init_array_end = .);
    PROVIDE (__fini_array_start = .);
    KEEP (*(.fini_array))
    KEEP (*(SORT(.fini_array.*)))
    PROVIDE (__fini_array_end = .);

  /* Note: Separate .rodata section for sections which are
     read only but which older linkers treat as read-write.
     This prevents older linkers from marking the entire .rodata
     section as read-write.  */
  /*.rodata2 : {
    . = ALIGN(2);
    *(.eh_frame_hdr)
    KEEP (*(.eh_frame))*/

    /* gcc uses crtbegin.o to find the start of the constructors, so
       we make sure it is first.  Because this is a wildcard, it
       doesn't matter if the user does not actually link against
       crtbegin.o; the linker won't look for a file to match a
       wildcard.  The wildcard also means that it doesn't matter which
       directory crtbegin.o is in.  */
    KEEP (*crtbegin*.o(.ctors))

    /* We don't want to include the .ctor section from from the
       crtend.o file until after the sorted ctors.  The .ctor section
       from the crtend file contains the end of ctors marker and it
       must be last */
    KEEP (*(EXCLUDE_FILE (*crtend*.o ) .ctors))
    KEEP (*(SORT(.ctors.*)))
    KEEP (*(.ctors))

    KEEP (*crtbegin*.o(.dtors))
    KEEP (*(EXCLUDE_FILE (*crtend*.o ) .dtors))
    KEEP (*(SORT(.dtors.*)))
    KEEP (*(.dtors))
  } > ROM
  
  /* This section contains data that is not initialised during load
     or application reset. */
  /*.persistent :
  {
    . = ALIGN(2);
    PROVIDE (__persistent_start = .);
    *(.persistent)
    . = ALIGN(2);
    PROVIDE (__persistent_end = .);
  } > ROM
  */
  .upper.rodata :
  {
    /* Note: If this section is not defined then please add:

           *(.either.rodata.*) *(.either.rodata)

       to the definition of the .rodata section above.  This
       will allow code compiled with -mdata-region=either to
       work properly.  */
    *(.upper.rodata.* .upper.rodata)
  } > HIFRAM

  .tinyram : {} > TINYRAM

  .lower.data :
  {
    . = ALIGN(2);
    PROVIDE (__datastart = .);
    *(.lower.data.* .lower.data)
  } > RAM AT> ROM

  .data :
  {
    . = ALIGN(2);
    PROVIDE (__datastart = .);

    KEEP (*(.jcr))
    *(.data.rel.ro.local) *(.data.rel.ro*)
    *(.dynamic)

    *(.data .data.* .gnu.linkonce.d.*)
    KEEP (*(.gnu.linkonce.d.*personality*))
    SORT(CONSTRUCTORS)
    *(.data1)
    *(.got.plt) *(.got)

    /* We want the small data sections together, so single-instruction offsets
       can access them all, and initialized data all before uninitialized, so
       we can shorten the on-disk segment size.  */
    . = ALIGN(2);
    *(.sdata .sdata.* .gnu.linkonce.s.* D_2 D_1)

    /* See the note in .rodata section about why we do not have this line here:

        *(.either.data.* .either.data)
    */
    . = ALIGN(2);
    *(.lower.data.* .lower.data)
    . = ALIGN(2);

    _edata = .;
    PROVIDE (edata = .);
    PROVIDE (__dataend = .);
  } > RAM AT> ROM

  /* Note that crt0 assumes this is a multiple of two; all the
     start/stop symbols are also assumed word-aligned.  */
  PROVIDE(__romdatastart = LOADADDR(.data));
  PROVIDE (__romdatacopysize = SIZEOF(.data));

  .upper.data :
  {
    __upper_data_init = LOADADDR (.upper.data);
    /* Status word.  */
    SHORT(1);
    __high_datastart = .;
    *(.upper.data.* .upper.data)
    __high_dataend = .;
  } > HIFRAM AT> ROM

  __rom_highdatacopysize = SIZEOF(.upper.data) - 2;
  __rom_highdatastart = LOADADDR(.upper.data) + 2;

  .lower.bss :
  {
    . = ALIGN(2);
    PROVIDE (__bssstart = .);
    *(.lower.bss.* .lower.bss)
  } > RAM

  .bss :
  {
    . = ALIGN(2);
    PROVIDE (__bssstart = .);
    *(.dynbss)
    *(.sbss .sbss.*)
    *(.bss .bss.* .gnu.linkonce.b.*)
    *(.lower.bss.* .lower.bss)
    /* See the note in .rodata section about why we do not have this line here:

        *(.either.bss.* .either.bss)
    */
    . = ALIGN(2);
    *(COMMON)
    PROVIDE (__bssend = .);
  } > RAM
  PROVIDE (__bsssize = SIZEOF(.lower.bss) + SIZEOF(.bss));
  /* This section contains data that is not initialised during load
     or application reset.  */
  .noinit (NOLOAD) :
  {
    . = ALIGN(2);
    PROVIDE (__noinit_start = .);
    *(.noinit)
    . = ALIGN(2);
    PROVIDE (__noinit_end = .);
  } > RAM

  .upper.bss :
  {
    /* Note - if this section is not going to be defined then please
       add this line back into the definition of the .bss section above:

         *(.either.bss.* .either.bss)
    */
    . = ALIGN(2);
    __high_bssstart = .;
    *(.upper.bss.* .upper.bss)
    . = ALIGN(2);
    __high_bssend = .;
  } > HIFRAM
  __high_bsssize = SIZEOF(.upper.bss);

 .ctpl (ORIGIN (FRAM)):
  {
    . = ALIGN(2);
    PROVIDE (__ctpl = .);
    *(.ctpl)
    . = ALIGN(2);
    PROVIDE (__ctpl_end = .);
  } > FRAM = 0x0

  /* We create this section so that "end" will always be in the
     RAM region (matching .stack below), even if the .bss
     section is empty.  */
 /* .heap (NOLOAD) :
  {
    . = ALIGN(2);
    __heap_start__ = .;
    _end = __heap_start__;
    PROVIDE (end = .); 
    KEEP (*(.heap))
    _end = .;
    PROVIDE (end = .);
    /* This word is here so that the section is not empty, and thus
       not discarded by the linker.  The actual value does not matter
       and is ignored.  */
  /*  LONG(0);
    __heap_end__ = .;
    __HeapLimit = __heap_end__;
  } > RAM
  */
  /* WARNING: Do not place anything in RAM here.
     The heap section must be the last section in RAM and the stack
     section must be placed at the very end of the RAM region.  */
  .stack (ORIGIN (RAM) + LENGTH(RAM)) :
  {
    PROVIDE (__stack = .);
    *(.stack)
  }

  .lower.text :
  {
    . = ALIGN(2);
    *(.lower.text.* .lower.text)
  } > ROM

  .text :
  {
    PROVIDE (_start = .);

    . = ALIGN(2);
    KEEP (*(SORT(.crt_*)))

    . = ALIGN(2);
    KEEP (*(.lowtext))

    . = ALIGN(2);

    *(.lower.text.* .lower.text)

    . = ALIGN(2);
    *(.text .stub .text.* .gnu.linkonce.t.* .text:*)
    /* See the note in .rodata section about why we do not have this line here:

        *(.either.text.* .either.text)

    */

    KEEP (*(.text.*personality*))
    /* .gnu.warning sections are handled specially by elf32.em.  */
    *(.gnu.warning)
    *(.interp .hash .dynsym .dynstr .gnu.version*)
    PROVIDE (__etext = .);
    PROVIDE (_etext = .);
    PROVIDE (etext = .);
    . = ALIGN(2);
    KEEP (*(.init))
    KEEP (*(.fini))
    KEEP (*(.tm_clone_table))
  } > ROM

  .upper.text :
  {
    /* Note - if this section is not going to be included in the script
       then please add this line back into the definition of the .text
       section above:

         *(.either.text.* .either.text)
    */
    . = ALIGN(2);
    *(.upper.text.* .upper.text)
  } > HIFRAM

  /* MSP430 INFO FLASH MEMORY SEGMENTS */
  .infoD  : {} > INFOD
  .infoC  : {} > INFOC
  .infoB  : {} > INFOB
  .infoA  : {} > INFOA


  /* The rest are all not normally part of the runtime image.  */

  .MSP430.attributes 0 :
  {
    KEEP (*(.MSP430.attributes))
    KEEP (*(.gnu.attributes))
    KEEP (*(__TI_build_attributes))
  }

  /* Stabs debugging sections.  */
  .stab          0 : { *(.stab) }
  .stabstr       0 : { *(.stabstr) }
  .stab.excl     0 : { *(.stab.excl) }
  .stab.exclstr  0 : { *(.stab.exclstr) }
  .stab.index    0 : { *(.stab.index) }
  .stab.indexstr 0 : { *(.stab.indexstr) }
  .comment       0 : { *(.comment) }
  /* DWARF debug sections.
     Symbols in the DWARF debugging sections are relative to the beginning
     of the section so we begin them at 0.  */
  /* DWARF 1.  */
  .debug          0 : { *(.debug) }
  .line           0 : { *(.line) }
  /* GNU DWARF 1 extensions.  */
  .debug_srcinfo  0 : { *(.debug_srcinfo) }
  .debug_sfnames  0 : { *(.debug_sfnames) }
  /* DWARF 1.1 and DWARF 2.  */
  .debug_aranges  0 : { *(.debug_aranges) }
  .debug_pubnames 0 : { *(.debug_pubnames) }
  /* DWARF 2.  */
  .debug_info     0 : { *(.debug_info .gnu.linkonce.wi.*) }
  .debug_abbrev   0 : { *(.debug_abbrev) }
  .debug_line     0 : { *(.debug_line .debug_line.* .debug_line_end ) }
  .debug_frame    0 : { *(.debug_frame) }
  .debug_str      0 : { *(.debug_str) }
  .debug_loc      0 : { *(.debug_loc) }
  .debug_macinfo  0 : { *(.debug_macinfo) }
  /* SGI/MIPS DWARF 2 extensions.  */
  .debug_weaknames 0 : { *(.debug_weaknames) }
  .debug_funcnames 0 : { *(.debug_funcnames) }
  .debug_typenames 0 : { *(.debug_typenames) }
  .debug_varnames  0 : { *(.debug_varnames) }
  /* DWARF 3 */
  .debug_pubtypes 0 : { *(.debug_pubtypes) }
  .debug_ranges   0 : { *(.debug_ranges) }
  /* DWARF Extension.  */
  .debug_macro    0 : { *(.debug_macro) }

  /DISCARD/ : { *(.note.GNU-stack) }
}

/****************************************************************************/
/* Include peripherals memory map                                           */
/****************************************************************************/

INCLUDE msp430fr5994_symbols.ld

如果有任何帮助,将不胜感激。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    《MSP430 GCC 工具链 用户指南 》应为本练习提供了很好的资源。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 James 的回复。 我已经成功编译了低级汇编文件、但您能否让我深入了解链接器文件必须进行的特定更改、以便成功地将 ctpl 导入以与 GCC 配合使用。 抱歉、我对链接器脚本有点陌生。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您修改后的链接器脚本引用了符号"ROM"、该符号未定义。 (通常用于闪存部件。) 原始版本使用"FRAM"。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    在这一点上进行扩展、下面是脚本的一部分:

      .lower.data :
      {
        . = ALIGN(2);
        PROVIDE (__datastart = .);
        *(.lower.data.* .lower.data)
      } > RAM AT> FRAM
    
    

    这样做的原因是、虽然变量在 RAM 中有效、但它们的初始值存储在 FRAM 中。 启动例程复制初始值。

    您需要的似乎是">FRAM at > FRAM。 这种冗余的方法会浪费空间、但禁用初始值的副本需要深入到启动代码中。 本手册(slau646)介绍了如何将函数插入初始化序列以禁用看门狗、但对替换或禁用现有例程没有任何说明。

    您可能还需要将 BSS 从 RAM 更改为 FRAM、因为未初始化的变量存在于那里。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢 David、让我尝试一下您的建议、看看它。 因此,您是否建议使用 gcc 项目获得的默认链接器文件,并将其修改 为使 >FRAM at>FRAM 禁用初始值的复制并 将 BSS 从 RAM 更改为 FRAM

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我想堆应该放置在 FRAM 上、堆应该保留在 RAM 中吗?  如下面的代码片段中所示。 我还应该将 FRAM 拆分为两个空间(用于读取和写入)、然后如何 将其与 ctpl 库链接?

    .heap (NOLOAD) :
      {
        . = ALIGN(2);
        __heap_start__ = .;
        _end = __heap_start__;
        PROVIDE (end = .); 
        KEEP (*(.heap))
        _end = .;
        PROVIDE (end = .);
        /* This word is here so that the section is not empty, and thus
           not discarded by the linker.  The actual value does not matter
           and is ignored.  */
        LONG(0);
        __heap_end__ = .;
        __HeapLimit = __heap_end__;
      } > ROM
      /* WARNING: Do not place anything in RAM here.
         The heap section must be the last section in RAM and the stack
         section must be placed at the very end of the RAM region.  */
      .stack (ORIGIN (RAM) + LENGTH(RAM)) :
      {
        PROVIDE (__stack = .);
        *(.stack)
      }
    
      .lower.text :
      {
        . = ALIGN(2);
        *(.lower.text.* .lower.text)
      } > RAM

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    同时、我在低级汇编文件中使用以下代码片段、但编译器始终会向我提供一个错误消息: ./fram-utilities/ctpl/ctpl_low_level.s:126:错误:在立即表达式'#_bis_SR_register (((0x0080)+(0x0040)+(0x0020)+(0x0010)))'末尾处添加额外字符'((((((0x0080)+(0x0020)+(0x0010))))))+)。

    ctpl_enterLpm:
        benchmark                                   ; Toggle the CTPL benchmark pin
        lpmDebug                                    ; Optional LPMx.5 debug mode*
        mov.b   #PMMPW_H,&PMMCTL0_H                 ; Set LPMx.5 bit
        mov.b   #PMMREGOFF,&PMMCTL0_L               ; Set LPMx.5 bit
        bis.w   #LPM4, SR                            /*# Enter LPMx.5 mode*/
        nop

    有人能帮我解决这个问题、以及为什么会发生这种情况?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否在该汇编语言文件中的某个位置定义了__STDC__? 5994.h 文件使用该符号在适用于汇编器或 C 的 LPM4定义之间进行选择。您可以获得 C 版本。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢 David 提供的信息。 否、我尚未在汇编文件中定义__ STDC_宏。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我在 e2e.ti.com/.../ctpl_5F00_with_5F00_gcc.zip 上附上了我的总体实施情况。 您能帮我调试这个、看看我是否完全错了?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    它是在某个地方定义的。 如果无法跟踪其中的位置、则可以使用 LPM4的 C 版本、即 LPM4_BITS。