请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:MSP430FR6989 工具/软件:Code Composer Studio
你(们)好
是否有办法加快 LCD 上的滚动速度?
此致
Graham
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Code Composer Studio
你(们)好
是否有办法加快 LCD 上的滚动速度?
此致
Graham
格雷厄姆
在 hal_lcd.c 的第172行中、在显示下一个字符之前存在延迟。 要提高速度、请减小此延迟。 下面的代码段中显示了这种情况。
void displayScrollText (char * msg) { int length = strlen (msg); int oldmode = mode; int i; INT s = 5; 字符缓冲区[6]=" "; (i=0;<length+7; i++) { if (mode!= oldmode) 中断; int t; 对于(t=0;t<6;t++) Buffer[t]='; int j; 对于(j=0;j = 0)&&((s+j)< 6) Buffer[s+j]= msg[j]; } S--; showChar (buffer[0]、pos1); showChar (buffer[1]、pos2); showChar (buffer[2]、pos3); showChar (buffer[3]、pos4); showChar (buffer[4]、pos5); showChar (buffer[5]、pos6); __DELAY_CYCLES (200000); }