This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR2355:低功耗模式消耗过多功率

Guru**** 2771175 points

Other Parts Discussed in Thread: MSP430FR2355

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1175203/msp430fr2355-low-power-mode-consuming-excessive-power

器件型号:MSP430FR2355

您好论坛、

 我已经编写了一些简单的代码来将 MSP430fr2355置于 LPM4模式、但我在3V 时的测量值大约为60uA。这似乎比我预期的要高很多、我是否在代码中遗漏了明显的东西?  

int main(void)
{
    //////////////////////////////Set up the ports and variables///////////////////////////////////////////


    //Stop watchdog timer
    WDTCTL = WDTPW | WDTHOLD;                   // Stop watchdog timer

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;

    ///PORT 6 SET UP
    P6DIR = P6DIR | 0b11111111;                 //Set port 6 to all outputs
    P6OUT = P6OUT & 0b00000000;                 // P6 all outputs off


    ///PORT 4 SET UP  // Configure Pins for I2C//////////////
    P4DIR = 0b11111111;
    P4OUT = 0b11000000;
    P4SEL0 |= BIT6 | BIT7;                      // I2C pins
    P4SEL1 &= 0b00111111;                       // I2C pins

    ///PORT 5 SET UP
    P5DIR = 0b11111111;                         //Port 5 all outputs - remember that port 5.1 and 5.2 have been disconnected and redirected to port 1
    //P5REN = 0b11111110;
    P5OUT = 0b00000000;

    ///PORT 3 SET UP
    P3DIR = 0b11111111;                         //Set as all outputs and
    P3OUT = 0b00000000;                         //Set all pins low

    ///PORT 2 SET UP
    P2SEL0 |= 0b11000000;                      // Configure 6 and 7 for external clock.
    P2SEL1 |= 0b11000000;
    P2DIR = 0b11101111;                        // 6 and 7 are used for clk, 4 is used for interrupt
    P2OUT = 0b00100000;
    P2IE |=  0b10000;                          // P2.4 interrupt enabled
    P2IES |= 0b00000;                          // P2.4 Hi/lo edge
    P2IFG &=~0b10000;                          // P2.4 IFG cleared


    ///PORT 1 SET UP
    //P1SEL0 |= 0b1;                              // Configure ADC A1 pin 0
    //P1SEL1 |= 0b1;
    P1DIR =  0b11111000;                          //Port 1 set as inputs and outputs remember that ports 1.1 and 1.2 have been connected to max interrupts
    P1IE |=  0b00000110;                          // interrupt enabled
    P1IES |= 0b00000000;                          // Lo/Hi edge
    P1IFG &= 0b00000000;                          // IFG cleared
    //P1OUT = 0b00000000;
    PM5CTL0 &= ~LOCKLPM5;                         // Disable the GPIO power-on default high-impedance mode to activate previously configured port settings


    // Source = 32kHz crystal, divided by 1024
  //  RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1024 | RTCIE;

    //////////////////////////Set clock to 8MHZ///////////////////////////////////
    PM5CTL0 &= ~LOCKLPM5;                    // Disable the GPIO power-on default high-impedance mode to activate 1previously configured port settings
    __bis_SR_register(SCG0);                 // disable FLL
    CSCTL3 |= SELREF__XT1CLK;               // Set REFO as FLL reference source
    CSCTL1 = DCOFTRIMEN_1 | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_3;// DCOFTRIM=3, DCO Range = 8MHz
    CSCTL2 = FLLD_0 + 243;                  // DCODIV = 8MHz this is F3 in hex
    __delay_cycles(3);
    __bic_SR_register(SCG0);                // enable FLL
    Software_Trim();                        // Software Trim to get the best DCOFTRIM value
    CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                                  // default DCODIV as MCLK and SMCLK source





    PMMCTL0 = PMMPW |PMMREGOFF;             // This should enable the PCMTL0 password and also turn off the internal regulator.
    _low_power_mode_4();                    //Should enter LPM4
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    忘记我的问题! 我断开了 Tektronix MDO3024示波器上的逻辑分析仪探针与 I2Clines 的连接、并移除了 JTAG 编程连接器、电流降至1.2uA。 但是、如果有人想知道如何实现这种功耗-代码起作用-它很丑、有些人讨厌二进制、有点讨厌、但它起作用了!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好 Richard、

    感谢您的更新。 很高兴听到您的解决方案。 如果您 有任何其他问题、请随时打开另一个主题。  

    此致、
    Brandon Fisher

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    找到容易解决的东西的乐趣!