This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR6879:如果主器件在启动器件之前发送数据,则作为从器件的 SPI 会发出错误消息。

Guru**** 2539500 points
Other Parts Discussed in Thread: MSP430FR6879

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/568875/msp430fr6879-spi-as-slave-gives-error-if-the-master-sends-data-before-starting-the-device

器件型号:MSP430FR6879

我在从模式下使用 msp430fr6879与另一个 用作主控 的电路通信,  

如果我仅在从设备上的交换机之后打开主设备,则可以正常工作。

但是,如果我先给主设备上电,然后再给从设备上电,我接收到的数据就会被破坏。
任何领导都将不胜感激。

下面、我添加了初始化

SPI_SLVTO_BOS_INIT ()

 P1SEL1 &=~(BIT4 | BIT6 | BIT4);                    

//配置从器件选择和 clk

P1SEL0 |= BIT4 | BIT6 | BIT7;

//配置 SOMI 和 MISO

 UCB0CTLW0 = UCSWRST;
 UCB0CTLW0 |= UCSYNC | UCMSB |UCCKPL;
 UCB0CTLW0 &=~UCSWRST;
 UCB0IE |= UCRXIE;

 }

其次、我还在主 while 循环中包含了溢出标志处理程序

if ((UCB0STATW 和 UCOE)=UCOE)

 RxBUFF_ATG[MAX_RXBYTECOUNT]= UCB0RXBUF;

 

#include 
#include "string.h"
#include "spi_SendReceive.h"
#include "structure.h"

//--- SPI-BOS-Commons--------------------------------------------------
TANK_Config_struct bTankConfig;
Delivery;Delivery;
TANK_Table_struct bTankTable;
Time_struct bTimeData;
firmware_version bFirmWareVersion;
unsigned char bTankNo;
unsigned short int bTankCount;
//---------------

#define rxtxBuffSize 280

枚举 commStateS
{
ideal = 0、
WaitForAck、
WaitForReply、
receiving、
received、
ReadyToTransmit、
Transmit、
Initialize、
Busy
};

volatile unsigned int commState=0、txCount=0、rxCount=0、index=0、forVar;
unsigned long int crc、sum;

volatile unsigned char *txPtr;
volatile unsigned char dummy1;
unsigned char rxBuff[rxtxBuffSize]、txBuff[rxtxBuffSize]、receivedCmd、crcData[4];
char crcMatch;

#define txnStartAddress 0x1F000 //0x1C7FF
#define txnCountAddress 0x1EFFF //0x1C7FE
#define txnMaxSize261/// inbytes
unsigned char txnCount、arnIndex、retVar、busyShaved;

long modbusCRCAddition (unsigned char * arr、int bSize);
void readString (unsigned char * arr、int size、int unsigned char * arr);
void writeChart * getArr (long char * arsize、
int);void writeChart *、int size (unsigned char *、int)
void writeNumberHEX (unsigned char * arr、int size、unsigned long int value);
unsigned long int readNumber (unsigned char * arr、int size);
unsigned long int readNumberHEX (unsigned char * arr、int size);

void BOS_DataParsing (void);
void getTankNumber (void);// CMD = 4(void
)= 4 (void)/GetCMD= 4 (void);void 配置(void)/FCMD/(void)
// CMD = 2
void GetDeliveryData (void);// CMD = 3
void setTankCount (void);// CMD = 6
void setLEDStatus (void);// CMD = 7
void setTankTablePoint (void);// CMD = 8
void getRTCData (void);// CMD = 9 void (
void)
;CMD = 10 (void) TransactionIndex
(void);// CMD = 10 (void)// CMD = 12
void readTransactionIndex (void);// CMD = 13
void readTransactionCount (void);// CMD = 14
void clearAllTransaction (void);// CMD = 15
void readSPIFirmwareVersion (void);// CMD = 16

void writeFRAMTnx (long add、unsigned int
char、unsigned int)、unsigned int long char、unsigned int、unsigned int 长度(unsigned int)

void BOS_Intialization (void)
{
commState = ideal;
__no_operation();
}

void BOS_ReceiveSendFunction (void)
{
if (commState=received)
{
rxCount=index+1;
CRC = modbusCRCAddition (rxBuff+1、rxCount-6);
writeNumberHEX (crcData、4、 crc);
crcMatch=0;
if (crcData[0]=rxBuff[rxCount-5])
if (crcData[1]=rxBuff[rxCount-4])
if (crcData[2]=rxBuff[rxCount-3])
if (crcData[3]=rxBuff[rxCount-4]) if (crcData[2]=rxCount=rxBuf=rxBuy=xe2]=rxBuy=xe;crUCB0Xe=


xe= r= r= xBuy= xe;cr1



) if

) if (cr&trab=cr&trab=cr= r= r= rx 1);cr&trab=cr&trab=r= r= rx
}
否则、如果(commState=ReadyToTransmit)
{
if (txCount < rxtxBuffSize-6)
{
txBuff[0]= 0x02;
CRC = modbusCRCAddition (txBuff+1、txCount);
writeNumberHEX (crcData、4、 crc);

txBuff[txCount+1]=crcData[0];
txBuff[txCount+2]=crcData[1];
txBuff[txCount+3]=crcData[2];
txBuff[txCount+4]=crcData[3];
txBuff[txCount+5]=0x03;
txCount=txCount+6;
txPtR=&txBuff[0];
commState=Transmit;
}
其他
commState=ideal;
伪= UCB0RXBUF;
UCB0IE |=UCRXIE;
}
__no_operation();
}

void BOS_Operations (void)
{
if (commState=WaitForAck)
{
retVar=0;
if (receivedCmd=1)
retVar=b_setTankConfiguration ();
否则 if (receivedCmd=4)
retVar=b_setTankyAck ();
否则 if (receivedCmd=5)
retVar=b_setTankyAck

();elt (receivedCmd=6);elt (retedCankyar = 6);elt (receivedCmd=6)
否则、如果(receivedCmd=7)
retVar=b_setLEDStatus();
否则(receivedCmd=8)
retVar=b_setTankTableData();
否则(receivedCmd=10)
retVar=b_setRTCData();
如果(receivedCankTableData=18)
;stoperHandlers

(receivedCmd=18);retedHandlers (=b);startHandlers (=18);els=b = ver= vredCmd);

writeNumber (txBuff+1、2、(unsigned long int) receivedCmd);
if (retVar=1)
txBuff[3]='1';
否则
txBuff[3]='0';
txCount=3;
commState=ReadyToTransmit;
}
否则 if (commState=WaitForReply)
{
retVar=0;
if (receivedCmd=3)
retVar=b_getDeliveryData();
否则 if (receivedCmd=9)
retVar=b_getRTCData();
否则 if (receivedCmd=16)
b_readDeliveryVersion();

if (retvar=b_getRTCData=b+3)eedC16=eed()










;if (receivedCfeedC16=1eCd=1eC16=1eC16=eCfeed();receivedCfeed();receivedCfeed()



commState=ReadyToTransmit;
}
否则 if (commState=Busy)
{
if (busyShared=0)
{
if (receivedCmd=9)
b_getRTCData();
否则 if (receivedCmd=10)
b_setRTCData();
}
否则 if (busyShared=1)
{
if (receivedCmd=9)
getRTCData();
否则 if (receivedCmd=10)
{
writeNumber (txBuff+1、2、(unsigned long int) receivedCmd);
txBuff[3]='1';
txCount=3;
}
commState=ReadyToTransmit;
}
否则 if (busyShayred=2)
{
writeNumber (txBuff+1、2、(unsigned long int) receivedCmd);
txBuff[3]='0';
txCount=3;
commState=ReadyToTransmit;
}
}


void BOS_DataPars()
{
receivedCmd = readNumber (rxBuff+1,2);
switch (receivedCmd)
{
案例1:
FillTankConfiguration();
commState=WaitForAck;
break;
案例2:
GetTankStatus();
commState=ReadyToTransmit;
break;
case 3:
getTankNumber();
commState=WaitForReply;
break;
case 4:
getTankNumber();
commState=WaitForAck;
break;
case 5:
getTankNumber();
commState=WaitForAck;
break;
判例6:
setTankCount();
commState=WaitForAck;
break;
判例7:
setLEDStatus();
commState=WaitForAck;
break;
case 8:
setTankTablePoint();
commState=WaitForAck;
break;
case 9:
busyShayred=0;
commState=Busy;
break;
case 10:
busyShared=0;
setRTCData();
commState=Busy;
break;
case 11:
addTransactionIndex();
commState=ReadyToTransmit;
break;
case 12:
updateTransactionIndex();
commState=ReadyToTransmit;
break;
case 13:
readTransactionIndex();
commState=ReadyToTransmit;break
;
判例14:
readTransactionCount();
commState=ReadyToTransmit;
break;
判例15:
clearAllTransaction();
commState=ReadyToTransmit;
break;
case 16:
commState=WaitForReply;
break;
case 17:
commState=WaitForAck;
break;
判例18:
commState=WaitForAck;
break;
默认:
break;
}
}//---------------

NVRAM 操作-------------------------------------------------------

void TransactionIndex()
{
if (rxCount>=(261+10))
{
readFRAMTnx (TxnCountAddress,&txnCount, 1);
if (txnCount >70)
{
txnCount=0;
writeFRAMTnx (TxnCountAddress,&txnCount, 1);
if (txnCount+)<rxBuqeCount=0(txnCount=0;txnCount+4)





;writeCRC+3r&txnCount=(rxBunCount=(xx+4);rnCount+4);rxDCMD=(rxCnCount+3r&r&r&nCount=(r&r&r&r&nCount=(rnCount);r&rnCRCnCount+4);r&r&r&r&
rxBuff[rxCount-5]=crcData[0];
rxBuff[rxCount-4]=crcData[1];
rxBuff[rxCount-3]=crcData[2];
rxBuff[rxCount-2]=crcData[3];

writeFRAMTnx ((txnIndex*(MaxStart+nSize) rxBuff+5、txnMaxSize+4);

txnCount=txnIndex+1;
writeFRAMTnx (txnCountAddress、&txnCount、 1);

txBuff[1]=0x31;
txBuff[2]=0x31;
txBuff[3]='1';
txCount=3;
}
}

{
txBuff[1]=0x31;
txBuff[2]=0x31;
writBuff[3]='0';
txCount=3;
}


void updateTransactionIndex (

){if (rxCount >=(261+10)))}
{
readFRAMTnx (txCountAddress、txnNumber、1&1xx)、



rxCount+4 (rx





)
、rxCount+N);rnCount (rx (rx)、rxCnCnCount (rnCnCnCnCnCnCn);rx (rx (rx)、rnCn)、rnCn (rq1)、rnCount (rnCn)、rx (rnCn)、rnCn)、rnCn (rq1)
rxBuff[rxCount-5]=crcData[0];
rxBuff[rxCount-4]=crcData[1];
rxBuff[rxCount-3]=crcData[2];
rxBuff[rxCount-2]=crcData[3];

writeFRAMTnx ((txnIndex*(MaxStart+nSize) rxBuff+5、txnMaxSize+4);

txBuff[1]=0x31;
txBuff[2]=0x32;
txBuff[3]='1';
txCount=3;
}

}否则
{
txBuff[1]=0x31;
txBuff[2]=0x32;
txBuff[3]='0';
txCount=3;
}


}void readTransactionIndex ()
{
readFRAMTnx (readCountAddress、&CounnCount、1);
if (txnCount>3





、txN);txCount (txnCount = 1
);txnCount (txnCount);txnCount (txnCount = 3、txnCount);txnCount = txnCount;txnCount;txnCount = txnCount) 70)
{
txnCount=0;
writeFRAMTnx (txnCountAddress、&txnCount、1);
txBuff[3]=0x30;
txBuff[4]=0x30;
}
否则
writeNumber (txBuff+3、2、(unsigned long int) txnCount);

txCount=4;
}

void clearAllTransaction()
{
txnCount=0;
writeFRAMTnx (txnCountAddress,&txnCount,1);

txBuff[1]=0x31;
txBuff[2]=0x35;
txBuff[3]='1';
txCount=3;
}

void writeFRAMTnx (unsigned long int add、unsigned char * buff、unsigned int length)
{
unsigned int loopVar=0;
for (



unsigned var=0;loopVar<length;unsigned var++)__loopar (unsigned var + int、unsigned vale+);loopvar + val=0;loopvar (unsigned val=val=vale+、loopvale+);enchar (enchar + v=v=val=val=ve+)(unsigned val=ve


5000)
bTankConfig.Probeoffset =(-1)*(tempvar - 5000);
否则
bTankConfig.Probeoffset = tempvar;

tempvar = readNumber (rxBuff+31、4);
if (tempvar > 5000)
bTankConfig.zero_water =(-1)*(txvar - 5000);
else = readNumber (rxBuff+31、4);if (tempedtfar = 0xbankConfig = 0x3



)、btbankConfig = 0xbfuff =


0x3;tidfu20[toff+3](tbfuff = 0xbtbfu.eOff_2);btidfuff = 0xbank3 (tid.t

2、(unsigned long int) tankstatus_struct[bTankNo-1].TAnkNo);
writeNumber (txBuff+5、1、(unsigned long int) tankstatus_struct[bTankNo-1].probe_status);
writeNumber (txBuff+6、2、(unsigned long int) tankstatus_struct[bTankNo-1].alarm_value.Astatus);
writeNumber (txBuff+8、8、 (unsigned long int) tankstatus_struct[bTankNo-1].Product_volume);
writeNumber (txBuff+16、6、(unsigned long int) tankstatus_struct[bTankNo-1].product_height);
writeNumber (txBuff+22、 4、(unsigned long int) tankstatus_struct[bTankNo-1].TEMP);
writeNumber (txBuff+26、6、(unsigned long int) tankstatus_struct[bTankNo-1].water 卷);
writeNumber (txBuff+32、6、(unsigned long int) tankstatus_struct[bTankNo-1].Water 高度);
writeNumber (txBuff+38、8、 (unsigned long int) tankstatus_struct[bTankNo-1].TCVOLUME;
writeNumber (txBuff+46、1、(unsigned long int) tankstatus_struct[bTankNo-1].on_delivery);

txCount=46;
}

void GetDeliveryData()
{txBuff[1]=0x30
;
txBuff[2]=0x33;

writeNumber (txBuff+3、2、(unsigned long int)bTankDeliveration.tank_no);
writeNumber (txBuff+5、1、(unsigned long int) bTankDelivery 交付结果计数);
writeNumberHEX (txBuff+6、2、 (unsigned long int) bTankDelivery。StartTime.year);
writeNumberHEX (txBuff+8、2、(unsigned long int) bTankDelivery。StartTime.Month);
writeNumberHEX (txBuff+10、 2、(unsigned long int) bTankDeliveration.StartTime.dayofmonth);
writeNumberHEX (txBuff+12、2、(unsigned long int) bTankDeliveration.StartTime.hour);
writeNumberHEX (txBuff+14、2、(unsigned long int) bTankDelivery .StartTime.min);
writeNumberHEX (txBuff+16、2、 (unsigned long int) bTankDelivery.Starttime.sec);
writeNumber (txBuff+18、8、(unsigned long int) bTankDelivery .StartVolume);
writeNumber (txBuff+26、 6、(unsigned long int) bTankDelivery .StartHeight);
writeNumber (txBuff+32、4、(unsigned long int) bTankDelivery .StartTemp);
writeNumberHEX (txBuff+36、2、(unsigned long int) bTankDelivery .EndTime.year);
writeNumberHEX (txBuff+38、2、 (unsigned long int) bTankDeliveration.EndTime.Month);
writeNumberHEX (txBuff+40、2、(unsigned long int) bTankDeliveration.EndTime.dayofmonth);
writeNumberHEX (txBuff+42、 2、(unsigned long int) bTankDelivery .EndTime.Hour);
writeNumberHEX (txBuff+44、2、(unsigned long int) bTankDelivery .EndTime.min);
writeNumberHEX (txBuff+46、2、(unsigned long int) bTankDelivery.EndTime.sec);
writeNumber (txBuff+48、8、 (unsigned long int) bTankDelivery。ENDVOLUME);
writeNumber (txBuff+56、6、(unsigned long int) bTankDelivery。EndHeight);
writeNumber (txBuff+62、 4、(unsigned long int) bTankDeliveration.Endtemp);

txCount=65;
}

void getTankNumber()
{
bTankNo = readNumber (rxBuff+3、2);
}

void setTankCount()
{
bTankCount = readNumber (rxBuff+3、5);





}void setLEDStatus(rxBuff+3+)= rbTankCount+3+ tid=rbToxTankCount+3

;rbToxTankNumber+3



(rbToxF=readTankOff+3、rbToxBuff3);}nbToxTankPoint+3 (rbToxTank0=rbToxTankOff_3;} 6);
bTankTable.volume_value = readNumber (rxBuff+14、8);
}

void getRTCData ()
{
txBuff[1]=0x30;
txBuff[2]=0x39;
txBuff[3]=0x31;
txBuff[4]=0x32;
writeNumberHEX (txBuff+5、txBuff+5 2、(unsigned long int) bTimeData.year);
writeNumberHEX (txBuff+7、2、(unsigned long int) bTimeData.Month);
writeNumberHEX (txBuff+9、2、(unsigned long int) bTimeData.dayofmonth);
writeNumberHEX (txBuff+11、2、 (unsigned long int) bTimeData.Hour);
writeNumberHEX (txBuff+13、2、(unsigned long int) bTimeData.min);
writeNumberHEX (txBuff+15、 2、(unsigned long int) bTimeData.sec);

txCount=16;
}

void setRTCData()
{
//bTimeData.year = readNumber (rxBuff+3、2);
bTimeData.year = readNumberHEX (rxBuff+5、2);
bTimeData.Month= readNumberHEX (rxBuff+7、 2);
bTimeData.dayofmonth = readNumberHEX (rxBuff+9、2);
bTimeData.Hour = readNumberHEX (rxBuff+11、2);
bTimeData.min = readNumberHEX (rxBuff+13、2);
bTimeData.sec = readNumberHEX (rxBuff+15、2);
}

void readSPIFirmwareVersion ()
{
txBuff[1]=0x31;
FirmBuff[2]=0x36;
writeNumber (txBuff+3、2)、blong long)
txBuff[5]='.';
writeNumber (txBuff+6、2、(unsigned long int) bFirmWareVersion.second);
txBuff[8]='.';
writeNumber (txBuff+9、2、(unsigned long int) bFirmWareVersion.third);

txCount=10;
}

void writeNumber (unsigned char * arr、int size、unsigned long int value)
{
for (forVar=0;forVar< size;forVar++)
{
unsigned arr[size-forVar-1、




unsigned var =

10;value = 0x30、unsigned v/int value}(void var = 10);void (void v/int value = 10) >(size-1-forVar)*4)& 0x0F)+ 0x30;
}


void writeCharArray (unsigned char * arr、unsigned char * arret、int size)
{
int i=0;
for (forVar = 0;forVar 0x40)?0x37:0x30)< 4)& 0xF0)|((arr[forVar+1]-((arr[forVar+1]> 0x40)?0x37:0x30)& 0x0F);}




无符号整型 int readberHEX (archar * arr * arr、0x30




)(unsigned int 大小


= 0x30);unsigned int (unsigned int r + 1)(unsigned int r (arr +)(arr = 0x30)(unsigned int)(alr + 1)(unsigned int (alr)、int (arr = 0)、unsigned int (arr)、int (alr = 0)、unsigned int (arr、int <size-1; ) forVar++)
sum =(sum +(arr[forVar]- 0x30)*10;
sum+=arr[size-1]- 0x30;
return sum;
}

void readString (unsigned char * arr、int size、unsigned char * getArr)
{
for (forVar=0;forVar<size;forVbus+



)}unsigned cr+




(unsigned char +)(unsigned cr +)(unsigned arge+)、unsigned arge+(unsigned char +)(unsigned cr +) r)(unsigned cr +)

int i;
for (i=0;i < bSize; i++)
{
CRCFull = CRCULL ^







^(unsigned long int)(arr[i]);int j;for (j=0;j<8;j++){CRCLSB = CRCULL & 0x0001;CRCFULL =(CRCULL >> 1)& 0x7FFF;if (CRCLSB=1)}CRCFULL =


1);(CRCFULL = 1)}(CRCFULL = 1)


/**中断服务例程
*
//

#if defined (__TI_Compiler_version__)|| Defined (__IAR_systems_ICC__)
#pragma vector=USCI_B0_vector
__interrupt void USCI_B0_ISR (void)
#Elif defined (__GISR__)
void __attribute__((((nuc1_b0_bvector

))#USCI_isr U0!
#endif
{
if (UCB0IFG & UCRXIFG)
{
//////dummy1 = UCB0RXBUF;
//if (0x00!= UCB0RXBUF_L)
//{
//dummy1 = UCB0RXBUF;
//if (dummy1 = 0x02)= UCB0XBUF



;~


// come= 0x0 = 0x0 = U0;//





= UCC0XBUF;//= 0x0 = U0 = U0 = 0x2;//= UCC0XBUF;= 0 = 0 = U0 = U0 = U0 = 0x2;//

}
否则 if (commState==Receiving)
{
if (index <(rxtxBuffSize-1))
index++;
if (0x03 =UCB0RXBUF_L)
{
P9OUT &=~BIT4;
commState=Received;
UCB0IE &=~UCRXIE;
}

else if (commState=Transmit)
= UCB0XBUF;
{=RXBUCFF=UCB0XBUD!= UCB0XF+





}




 

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好、Noble、

    在完全开启且 MSP 在字节传输过程中开始接收通信之前、主器件是否有可能向 MSP 发送数据?

    此致、
    Caleb Overbay
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    第一次-发布748 (!) 代码行太多了。 您只能发布相关代码。 下次请编写与您的问题、部件无关的代码。 我个人跳过了所有这些-因为你没有打扰,我也是如此

    您的问题很可能是从器件选择处理不当。 典型 SPI 编程错误:在从器件选择有效后、主器件立即开始传输、而不会暂停、这对于从器件处理从器件选择信号和初始化 SPI 外设而言是很可能的。 在从器件选择和传输之间向主器件代码添加一些延迟。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好、Noble、

    您是否仍然需要此方面的帮助、或者是否为您想要共享的解决方案提供了资金?

    此致、
    Caleb Overbay
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    是的、这是问题发生的时间。 还可以,问题已经解决了。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    您好、
    很抱歉朋友说这是748! 代码行,现在我将处理它。
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
    你好、我得到了我的答案
    感谢你提醒我的职责。

    首先、我的问题是这个
    当(SPI)主器件(其它器件)在从器件(MSP430)上电或准备好接收数据之前尝试发送数据时,我获得错误数据
    即使在保存起始接收代码后也是如此。
    因为数据会被移位,并在 i8n 之后保留,无论您尝试接收什么(即使您使用了 cs)。


    这就是我的问题得到解决的方式

    我将 SPI 的 CS 引脚作为中断引脚、在中断时、我重新初始化 SPI。
    这会清除 Rx 移位寄存器。 从而解决我的问题。