This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5994:使用中断和 DriverLib 发送 UART 数据

Guru**** 2386620 points
Other Parts Discussed in Thread: MSP430FR5994
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1233948/msp430fr5994-send-uart-data-using-interrupt-with-driverlib

器件型号:MSP430FR5994

您好!

我使用 MSP430FR5994有一段时间。

我知道如何使用中断来接收数据、并且通常使用主循环来 使用"EUSCI_A_UART_TRANSD输 数据"函数发送 UART 数据。

现在、为了 提高性能、我们希望使用 UART Tx 中断测试数据发送。

可以举个例子吗?

在 DriverLib 示例中、我看到示例通过中断进行接收、而不是发送。

谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、通常您必须翻滚自己的脸。 下面是我写的一个大脑死区,可以通过添加循环缓冲器改进:

    /*
     * Program to control two pass transistors, one to charge the caps and one to dump it.
     *
     * Ports used:
     * Port J: Pins 2 &3 - Crystal
     * Port 1: Pin 0: Red LED
     * Port 1: Pins 2&3 Back Channel UART
     * Port4: Pin 0 Control to Charge Caps
     * Port 3: Pin 0 : Control to Dump Caps
     *
     *
     */
    /* DriverLib Includes */
    #include <ti/devices/msp432p4xx/driverlib/driverlib.h>
    
    /* Standard Includes */
    #include <stdint.h>
    #include <stdbool.h>
    #include <string.h>
    #include <stdio.h>
    #include <stdlib.h>
    
    void executeCommand(char *cmd);
    int getData(char *cmd, char *name);
    void waitForSerial(void);
    void Delay(int msec);
    
    /* UART Configuration Parameter. These are the configuration parameters to
     * make the eUSCI A UART module to operate with a 115200 baud rate. These
     * values were calculated using the online calculator that TI provides
     * at:
     * software-dl.ti.com/.../index.html
     */
    const eUSCI_UART_ConfigV1 uartConfig =
    {
     EUSCI_A_UART_CLOCKSOURCE_SMCLK,          // SMCLK Clock Source
     156,                                      // BRDIV =
     4,                                       // UCxBRF =
     0,                                      // UCxBRS =
     EUSCI_A_UART_NO_PARITY,                  // No Parity
     EUSCI_A_UART_LSB_FIRST,                  // LSB First
     EUSCI_A_UART_ONE_STOP_BIT,               // One stop bit
     EUSCI_A_UART_MODE,                       // UART mode
     EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION  // Oversampling
    };
    
    /* Other Rates
     *  9600
     *  BRDIV: 156
     *  UCXBRF: 4
     *  UCXBRS: 0
     *  Oversample: 1
     *
     *  38400
     *  BRDIV: 39
     *  UCXBRF: 1
     *  UCXBRS: 0
     *  Oversample: 1
     *
     *  115200
     *  BRDIV: 13
     *  UCXBRF: 1
     *  UCXBRS: 37
     *  Oversample: 1
     *
     */
    
    char TXData[256];
    volatile int TXIdx = -1; // No transmission
    
    
    uint8_t RXData;
    uint8_t RXIdx = 0;
    char RXLine[64];
    
    // Systick timer
    volatile unsigned int Tick;
    
    int main(void)
    {
        int index;
    
        /* Halting the Watchdog */
        MAP_WDT_A_holdTimer();
    
        //![Simple CS Config]
        /* Configuring pins for peripheral/crystal usage and LED for output */
        MAP_GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_PJ,
                                                        GPIO_PIN3 | GPIO_PIN2, GPIO_PRIMARY_MODULE_FUNCTION);
    
        MAP_GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
                                                       GPIO_PIN2 | GPIO_PIN3, GPIO_PRIMARY_MODULE_FUNCTION); // UART
    
        MAP_GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0); // Main Red LED
        MAP_GPIO_setAsOutputPin(GPIO_PORT_P3, GPIO_PIN0); // Dump
        MAP_GPIO_setAsOutputPin(GPIO_PORT_P4, GPIO_PIN0); // Capacitor Charging
    
        MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0); // Follows the gate drive
        MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0);
        MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P4, GPIO_PIN0);
    
        /* Just in case the user wants to use the getACLK, getMCLK, etc. functions,
         * let's set the clock frequency in the code. 
         */
        CS_setExternalClockSourceFrequency(32000,48000000);
    
        /* Starting HFXT in non-bypass mode without a timeout. Before we start
         * we have to change VCORE to 1 to support the 48MHz frequency */
        MAP_PCM_setCoreVoltageLevel(PCM_VCORE1);
        MAP_FlashCtl_setWaitState(FLASH_BANK0, 1);
        MAP_FlashCtl_setWaitState(FLASH_BANK1, 1);
        CS_startHFXT(false);
    
        /* Initializing MCLK to HFXT (effectively 48MHz) */
        MAP_CS_initClockSignal(CS_MCLK, CS_HFXTCLK_SELECT, CS_CLOCK_DIVIDER_1);
        // The UART is limited to 24 MHz...
        MAP_CS_initClockSignal(CS_SMCLK, CS_HFXTCLK_SELECT, CS_CLOCK_DIVIDER_2);
    
        // Configure SysTick
        MAP_SysTick_enableModule();
        // 48M = 1 sec, 4.8M = 100ms, 480000 = 10ms...
        MAP_SysTick_setPeriod(48000); // Every 1 msec
        MAP_SysTick_enableInterrupt();
    
        /* Configuring UART Module */
        MAP_UART_initModule(EUSCI_A0_BASE, &uartConfig);
    
        /* Enable UART module */
        MAP_UART_enableModule(EUSCI_A0_BASE);
    
        /* Enabling interrupts */
        MAP_UART_enableInterrupt(EUSCI_A0_BASE, EUSCI_A_UART_RECEIVE_INTERRUPT|EUSCI_A_UART_TRANSMIT_INTERRUPT);
    
        /* Enabling interrupts */
        MAP_Interrupt_enableInterrupt(INT_EUSCIA0);
    
        /* Enabling MASTER interrupts */
        MAP_Interrupt_enableMaster();
    
        //debug
        strcpy(TXData, "Hello, World!\n\r");
        TXIdx = 0;
    
        while (1)
        {
            
    
            if (RXData != 0) {
                if ((RXData == '\r') || (RXData == '\n')) {
                    RXLine[RXIdx] = '\0';
    
                    RXData = 0;
    
                    executeCommand(RXLine);
    
                    RXIdx = 0;
                    MAP_GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0);
    
                } else {
    
                    RXLine[RXIdx++] = RXData;
    
                    waitForSerial();
                    TXData[0] = RXData;
                    TXData[1] = '\0';
    
                    TXIdx = 0;
                    RXData = 0;
    
                }
    
            }
            
            if (TXIdx == 0)
            {
                // Start the transmission
                MAP_UART_transmitData(EUSCI_A0_BASE, TXData[TXIdx++]);
            }
    
        } // while()
    }
    
    
    
    /* EUSCI A0 UART ISR */
    void EUSCIA0_IRQHandler(void)
    {
        uint32_t status = MAP_UART_getEnabledInterruptStatus(EUSCI_A0_BASE);
    
        MAP_UART_clearInterruptFlag(EUSCI_A0_BASE, status);
    
        if(status & EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG)
        {
            RXData = MAP_UART_receiveData(EUSCI_A0_BASE);
    
    
        } else if (status & EUSCI_A_UART_TRANSMIT_INTERRUPT_FLAG) {
            // Ready to transmit the next byte
            if (TXIdx == -1) return;
    
            if (TXData[TXIdx] == '\0')
            {
                // Done transmitting
                TXIdx = -1;
    
            } else {
                MAP_UART_transmitData(EUSCI_A0_BASE, TXData[TXIdx++]);
    
            }
        }
    
    }
    
    
    void waitForSerial(void)
    {
        // Wait for TXIdx to go to -1...
        while (TXIdx != -1);
    
    }
    
    void SysTick_Handler(void)
    {
        Tick++;
    }
    
    void Delay(int msec) {
        // Busy wait msec ms
        int starttime = Tick;
    
        while((Tick - starttime) < msec);
    }

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Ron:

    抱歉迟到了响应、实际上代码示例中的应用程序使用了 RX 中断。

    可以尝试启用 TX 中断、然后尝试使用该中断进行传输。  当新数据被写入 UCAxTXBUF 时、UCTXIFG 被置位。

      UCA3IE |= UCRXIE;             //启用 USCI_A3 RX 中断

    -> UCA3IE |= UCRXIE | UCTXIE;    //启用 USCI_A3 RX 和 TX 中断

    如果您在使用 TX 中断时遇到任何问题、欢迎回复线程。

    B.R.

    Sal.