This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5969:MSP 低功耗微控制器论坛

Guru**** 2616675 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1277238/msp430fr5969-msp-low-power-microcontroller-forum

器件型号:MSP430FR5969

MSP430新手上路。 我正在尝试进入 LPM4.5。 在该代码中、当 UART 上接收到特定字符时、器件需要进入 LPM4.5。  

我看到的电流消耗为0.3mA。

//#include "main.h"
#include <stdio.h>
#include <string.h>
#include "driverlib.h"
#include <msp430.h>

extern int mode;
extern int pingHost;

uint8_t RXData = 0;                               // UART Receive byte
uint8_t sleep  = 0;
void Init_GPIO(void);
void Init_Clock(void);
void Init_UART(void);


//-----------------------------------------------------------------------------
int _system_pre_init(void)
{
    // Stop Watchdog timer
    WDTCTL = WDTPW | WDTHOLD;    // Stop WDT
    return 1;
}

/*
 * main.c
 */
int main(void) {

    Init_Clock();
    Init_GPIO();
    Init_UART();

    int i =0;
    while (1)
    {
        if (sleep)
        {
            EUSCI_A_UART_disable(EUSCI_A0_BASE);

            P1OUT = 0;
            P2OUT = 0;
            P3OUT = 0;
            P4OUT = 0;

            P1SEL0 = 0;
            P1SEL1 = 0;

            P2SEL0 = 0;
            P2SEL1 = 0;

            P3SEL0 = 0;
            P3SEL1 = 0;

            P4SEL0 = 0;
            P4SEL1 = 0;

            PMMCTL0_H = PMMPW_H;                // Open PMM Registers for write
            PMMCTL0_L &= ~(SVSHE);              // Disable high-side SVS
            PMMCTL0_L |= PMMREGOFF;             // and set PMMREGOFF
            PMMCTL0_H = 0;                      // Lock PMM Registers

            sleep = 0;

            // Enter LPM4 Note that this operation does not return. The LPM4.5
            __bis_SR_register(GIE);
            __bis_SR_register(LPM4_bits);



        }

        printf("test %d\n", i++);
        __delay_cycles(9000000);
    }
}

int fputc(int _c, register FILE *_fp)
{
    EUSCI_A_UART_transmitData(EUSCI_A0_BASE, _c);

    return((unsigned char)_c);
}

int fputs(const char *_ptr, register FILE *_fp)
{
    unsigned int i, len;

    len = strlen(_ptr);

    for(i=0 ; i<len ; i++)
    {
        fputc(_ptr[i], _fp);
    }

    return len;
}
/*
 * GPIO Initialization
 */
void Init_GPIO()
{
    // Set all GPIO pins to output low for low power
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setOutputLowOnPin(GPIO_PORT_P4, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setOutputLowOnPin(GPIO_PORT_PJ, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);

    GPIO_setAsOutputPin(GPIO_PORT_P1, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setAsOutputPin(GPIO_PORT_P2, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setAsOutputPin(GPIO_PORT_P3, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setAsOutputPin(GPIO_PORT_P4, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);
    GPIO_setAsOutputPin(GPIO_PORT_PJ, GPIO_PIN0|GPIO_PIN1|GPIO_PIN2|GPIO_PIN3|GPIO_PIN4|GPIO_PIN5|GPIO_PIN6|GPIO_PIN7);

    // Configure P2.0 - UCA0TXD and P2.1 - UCA0RXD
    //  GPIO_setOutputLowOnPin(GPIO_PORT_P2, GPIO_PIN0);
    //  GPIO_setAsOutputPin(GPIO_PORT_P2, GPIO_PIN0);
    //
    GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P2, GPIO_PIN0, GPIO_SECONDARY_MODULE_FUNCTION);
    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P2, GPIO_PIN1, GPIO_SECONDARY_MODULE_FUNCTION);

    // Set PJ.4 and PJ.5 as Primary Module Function Input, LFXT.
    GPIO_setAsPeripheralModuleFunctionInputPin(
            GPIO_PORT_PJ,
            GPIO_PIN4 + GPIO_PIN5,
            GPIO_PRIMARY_MODULE_FUNCTION
    );

    // Disable the GPIO power-on default high-impedance mode
    // to activate previously configured port settings
    PMM_unlockLPM5();
}

/*
 * Clock System Initialization
 */
void Init_Clock()
{
    // Set DCO frequency to 8 MHz
    CS_setDCOFreq(CS_DCORSEL_0, CS_DCOFSEL_6);
    //Set external clock frequency to 32.768 KHz
    CS_setExternalClockSource(32768, 0);
    //Set ACLK=LFXT
    CS_initClockSignal(CS_ACLK, CS_LFXTCLK_SELECT, CS_CLOCK_DIVIDER_1);
    // Set SMCLK = DCO with frequency divider of 1
    CS_initClockSignal(CS_SMCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);
    // Set MCLK = DCO with frequency divider of 1
    CS_initClockSignal(CS_MCLK, CS_DCOCLK_SELECT, CS_CLOCK_DIVIDER_1);
    //Start XT1 with no time out
    //    CS_turnOnLFXT(CS_LFXT_DRIVE_3);
}

/*
 * UART Communication Initialization
 */
void Init_UART()
{
    // Configure USCI_A0 on 115200
    EUSCI_A_UART_initParam param = {0};
    param.selectClockSource = EUSCI_A_UART_CLOCKSOURCE_SMCLK;
    param.clockPrescalar = 4;
    param.firstModReg = 5;
    param.secondModReg = 0x55;
    param.parity = EUSCI_A_UART_NO_PARITY;
    param.msborLsbFirst = EUSCI_A_UART_LSB_FIRST;
    param.numberofStopBits = EUSCI_A_UART_ONE_STOP_BIT;
    param.uartMode = EUSCI_A_UART_MODE;
    param.overSampling = EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION;

    if(STATUS_FAIL == EUSCI_A_UART_init(EUSCI_A0_BASE, &param))
        return;

    EUSCI_A_UART_enable(EUSCI_A0_BASE);

    EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE,
                                EUSCI_A_UART_RECEIVE_INTERRUPT);

    // Enable USCI_A0 RX interrupt
    EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE,
                                 EUSCI_A_UART_RECEIVE_INTERRUPT); // Enable interrupt

    // Enable globale interrupt
    __enable_interrupt();
}

/*
 * USCI_A0 Interrupt Service Routine that receives PC GUI's commands
 */
#pragma vector = USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
{
    switch (__even_in_range(UCA0IV, USCI_UART_UCTXCPTIFG)) {
    case USCI_NONE:
        break;
    case USCI_UART_UCRXIFG:
        RXData = EUSCI_A_UART_receiveData(EUSCI_A0_BASE);
        printf("%d",RXData);
        if (RXData == 0x31)
        {
            sleep = 1;
        }
        break;
    case USCI_UART_UCTXIFG:
        break;
    case USCI_UART_UCSTTIFG:
        break;
    case USCI_UART_UCTXCPTIFG:
        break;
    }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    > P2OUT = 0;

    这会将 P2.1驱动为低电平(相对于传入(主机) Tx 线)、后者空闲为高电平;这将导致总线冲突。 也许先尝试添加类似这样的内容:

    > P2DIR &=~BIT1; // P2.1 (UART Rx)作为输入