This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5994:用作从器件时卡在 LPM0中

Guru**** 2616675 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1288396/msp430fr5994-getting-stuck-in-lpm0-when-using-as-slave

器件型号:MSP430FR5994

我正尝试将 MCU 用作数字发现的从器件、数字发现向 MCU 发送命令0x08 (VOLTAGE_CMD)并在 VoltageBuffer 中接收数据进行响应。 然而,我的代码被卡在   main ()中的_ bis_SR_register(LPM0_bits + GIE)行,不能超过这个范围,即使命令是由数字发现发送. 我的代码基于 MSP430FR599x 演示- eUSCI_B2、I2C 从器件多字节 TX/RX 代码。 在我的下面的代码中、是否有任何突出的问题?

//******************************************************************************
//   MSP430FR599x Demo - eUSCI_B2, I2C Slave multiple byte TX/RX
//
//   Description: I2C master communicates to I2C slave sending and receiving
//   3 different messages of different length. (This is the slave code). The
//   slave will be in LPM0 mode, waiting for the master to initiate the
//   communication. The slave will send/receive bytes based on the master's
//   request. The slave will handle I2C bytes sent/received using the
//   I2C interrupt.
//   ACLK = NA, MCLK = SMCLK = DCO 16MHz.
//
//                                     /|\ /|\
//                   MSP430FR5994      4.7k |
//                 -----------------    |  4.7k
//            /|\ |             P7.1|---+---|-- I2C Clock (UCB1SCL)
//             |  |                 |       |
//             ---|RST          P7.0|-------+-- I2C Data (UCB1SDA)
//                |                 |
//                |                 |
//                |                 |
//                |                 |
//                |                 |
//                |                 |
//
//   Nima Eskandari and Ryan Meredith
//   Texas Instruments Inc.
//   November 2017
//   Built with CCS V7.3
//******************************************************************************

#include <msp430.h> 
#include <stdint.h>

//******************************************************************************
// Pin Config ******************************************************************
//******************************************************************************

#define LED_OUT     P1OUT
#define LED_DIR     P1DIR
#define LED0_PIN    BIT0
#define LED1_PIN    BIT1

//******************************************************************************
// Example Commands ************************************************************
//******************************************************************************

#define SLAVE_ADDR  0x0B

/* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
 * The slave will send example SlaveTypeX buffers in response.
 *
 * CMD_TYPE_X_MASTER are example commands the master sends to the slave.
 * The slave will initialize itself to receive MasterTypeX example buffers.
 * */

#define VOLTAGE_CMD      0x08


#define VOLTAGE_BUFFER_LENGTH   1


#define MAX_BUFFER_SIZE     20

/* MasterTypeX are example buffers initialized in the master, they will be
 * sent by the master to the slave.
 * SlaveTypeX are example buffers initialized in the slave, they will be
 * sent by the slave to the master.
 * */


uint8_t VoltageBuffer [VOLTAGE_BUFFER_LENGTH] = {8};

//******************************************************************************
// General I2C State Machine ***************************************************
//******************************************************************************

typedef enum I2C_ModeEnum{
    IDLE_MODE,
    NACK_MODE,
    TX_REG_ADDRESS_MODE,
    RX_REG_ADDRESS_MODE,
    TX_DATA_MODE,
    RX_DATA_MODE,
    SWITCH_TO_RX_MODE,
    SWITCH_TO_TX_MODE,
    TIMEOUT_MODE
} I2C_Mode;

/* Used to track the state of the software state machine*/
I2C_Mode SlaveMode = RX_REG_ADDRESS_MODE;

/* The Register Address/Command to use*/
uint8_t ReceiveRegAddr = 0;

/* ReceiveBuffer: Buffer used to receive data in the ISR
 * RXByteCtr: Number of bytes left to receive
 * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
 * TransmitBuffer: Buffer used to transmit data in the ISR
 * TXByteCtr: Number of bytes left to transfer
 * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
 * */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;


/* Initialized the software state machine according to the received cmd
 *
 * cmd: The command/register address received
 * */
void I2C_Slave_ProcessCMD(uint8_t cmd);

/* The transaction between the slave and master is completed. Uses cmd
 * to do post transaction operations. (Place data from ReceiveBuffer
 * to the corresponding buffer based in the last received cmd)
 *
 * cmd: The command/register address corresponding to the completed
 * transaction
 */
void I2C_Slave_TransactionDone(uint8_t cmd);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);

void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}

void I2C_Slave_ProcessCMD(uint8_t cmd)
{
    ReceiveIndex = 0;
    TransmitIndex = 0;
    RXByteCtr = 0;
    TXByteCtr = 0;

    switch (cmd)
    {
        case (VOLTAGE_CMD):
            SlaveMode = TX_DATA_MODE;
            TXByteCtr = VOLTAGE_BUFFER_LENGTH;
            //Fill out the TransmitBuffer
            CopyArray(VoltageBuffer, TransmitBuffer, VOLTAGE_BUFFER_LENGTH);
            UCB1IE &= ~UCRXIE;                       // Disable RX interrupt
            UCB1IE |= UCTXIE;                        // Enable TX interrupt
            break;
        default:
            __no_operation();
            break;
    }
}


void I2C_Slave_TransactionDone(uint8_t cmd)
{
    switch (cmd)
    {
        case (0x08):
            break;
        default:
            __no_operation();
            break;
    }
}




//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************

void initGPIO()
{
    //LEDs
    LED_DIR |= LED0_PIN | LED1_PIN;
    LED_OUT &= ~(LED0_PIN | LED1_PIN);         // P1 setup for LED & reset output

    // I2C pins
    P5SEL0 |= BIT0 | BIT1;
    P5SEL1 &= ~(BIT0 | BIT1);

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;
}

void initI2C()
{
    UCB1CTLW0 = UCSWRST;                      // Software reset enabled
    UCB1CTLW0 |= UCMODE_3 | UCSYNC;           // I2C mode, sync mode
    UCB1I2COA0 = SLAVE_ADDR | UCOAEN;        // Own Address and enable
    UCB1CTLW0 &= ~UCSWRST;                    // clear reset register
    UCB1IE |= UCRXIE + UCSTPIE;
}


void initClockTo16MHz()
{
    // Configure one FRAM waitstate as required by the device datasheet for MCLK
    // operation beyond 8MHz _before_ configuring the clock system.
    FRCTL0 = FRCTLPW | NWAITS_1;

    // Clock System Setup
    CSCTL0_H = CSKEY_H;                     // Unlock CS registers
    CSCTL1 = DCOFSEL_0;                     // Set DCO to 1MHz
    // Set SMCLK = MCLK = DCO, ACLK = LFXTCLK (VLOCLK if unavailable)
    CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK;
    // Per Device Errata set divider to 4 before changing frequency to
    // prevent out of spec operation from overshoot transient
    CSCTL3 = DIVA__4 | DIVS__4 | DIVM__4;   // Set all corresponding clk sources to divide by 4 for errata
    CSCTL1 = DCOFSEL_4 | DCORSEL;           // Set DCO to 16MHz
    // Delay by ~10us to let DCO settle. 60 cycles = 20 cycles buffer + (10us / (1/4MHz))
    __delay_cycles(60);
    CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1;   // Set all dividers to 1 for 16MHz operation
    CSCTL0_H = 0;                           // Lock CS registers
}

//******************************************************************************
// Main ************************************************************************
// Enters LPM0 and waits for I2C interrupts. The data sent from the master is  *
// then interpreted and the device will respond accordingly                    *
//******************************************************************************


int main(void) {
    WDTCTL = WDTPW | WDTHOLD;   // Stop watchdog timer

    initClockTo16MHz();
    initGPIO();
    initI2C();

    __bis_SR_register(LPM0_bits + GIE);
    return 0;
}

//******************************************************************************
// I2C Interrupt ***************************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B1_VECTOR
__interrupt void USCI_B1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B1_VECTOR))) USCI_B1_ISR (void)
#else
#error Compiler not supported!
#endif
{
  //Must read from UCB1RXBUF
  uint8_t rx_val = 0;
  switch(__even_in_range(UCB1IV, USCI_I2C_UCBIT9IFG))
  {
    case USCI_NONE:          break;         // Vector 0: No interrupts
    case USCI_I2C_UCALIFG:   break;         // Vector 2: ALIFG
    case USCI_I2C_UCNACKIFG:                // Vector 4: NACKIFG
      break;
    case USCI_I2C_UCSTTIFG:  break;         // Vector 6: STTIFG
    case USCI_I2C_UCSTPIFG:
        UCB1IFG &= ~(UCTXIFG0);
        break;         // Vector 8: STPIFG
    case USCI_I2C_UCRXIFG3:  break;         // Vector 10: RXIFG3
    case USCI_I2C_UCTXIFG3:  break;         // Vector 12: TXIFG3
    case USCI_I2C_UCRXIFG2:  break;         // Vector 14: RXIFG2
    case USCI_I2C_UCTXIFG2:  break;         // Vector 16: TXIFG2
    case USCI_I2C_UCRXIFG1:  break;         // Vector 18: RXIFG1
    case USCI_I2C_UCTXIFG1:  break;         // Vector 20: TXIFG1
    case USCI_I2C_UCRXIFG0:                 // Vector 22: RXIFG0
        rx_val = UCB1RXBUF;
        switch (SlaveMode)
        {
          case (RX_REG_ADDRESS_MODE):
              ReceiveRegAddr = rx_val;
              I2C_Slave_ProcessCMD(ReceiveRegAddr);
              break;
          case (RX_DATA_MODE):
              ReceiveBuffer[ReceiveIndex++] = rx_val;
              RXByteCtr--;
              if (RXByteCtr == 0)
              {
                  //Done Receiving MSG
                  SlaveMode = RX_REG_ADDRESS_MODE;
                  UCB1IE &= ~(UCTXIE);
                  UCB1IE |= UCRXIE;                          // Enable RX interrupt
                  I2C_Slave_TransactionDone(ReceiveRegAddr);
              }
              break;
          default:
              __no_operation();
              break;
        }
        break;
    case USCI_I2C_UCTXIFG0:                 // Vector 24: TXIFG0
        switch (SlaveMode)
        {
          case (TX_DATA_MODE):
              UCB1TXBUF = TransmitBuffer[TransmitIndex++];
              TXByteCtr--;
              if (TXByteCtr == 0)
              {
                  //Done Transmitting MSG
                  SlaveMode = RX_REG_ADDRESS_MODE;
                  UCB1IE &= ~(UCTXIE);
                  UCB1IE |= UCRXIE;                          // Enable RX interrupt
                  I2C_Slave_TransactionDone(ReceiveRegAddr);
              }
              break;
          default:
              __no_operation();
              break;
        }
        break;                      // Interrupt Vector: I2C Mode: UCTXIFG
    default: break;
  }
}

TIA!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我不会期望 main ()会经过 LPM0行(到 return 语句),因为没有唤醒;所有的工作都在后台完成。 关于在 ISR 中设置断点、本手册可能会提供更多信息。

    您在 Discovery 中使用的 I2C 地址是什么? 看一下它的文档、他们似乎认为 R/W 位是地址的一部分(并非如此)。 如果是这种情况、您可能需要使用地址(0x0B << 1)= 0x16。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bruce、您好!

    感谢您指出我应该在 Discovery 中使用地址0x16。 我在 ISR 中更改了这个设置并设置了断点、但似乎仍未进入它。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我能够通过在 Discovery 的数据和时钟线上启用内部10k 上拉电阻器来解决这个问题。 我最后还使用了原始地址0x0B 、因为发现会考虑 R/W 位、并在您选择读取或写入时相应地移动地址。