This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F5529:关于 MSP430F5510或 MSP430F5529进入 LMP4或 LPM4.5

Guru**** 2927270 points

Other Parts Discussed in Thread: MSP430F5529

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1289706/msp430f5529-about-msp430f5510-or-msp430f5529-enter-lmp4-or-lpm4-5

器件型号:MSP430F5529
主题中讨论的其他器件: MSP430WARE

我有关于 MSP430F5529低功耗的问题。 当我~MSP430F5529进入低功耗4.5状态时、MCU 电流流动为10 μ A 22uA、为什么不是0.1uA。

当 MCU,为3.3V 时、MCU 低功耗电流为22uA 当 MCU 电源为1.8V 时、MCU 低功耗电流为0.1uA。 你会告诉我为什么、谢谢。

      //This code is about MSP430F5510 enter LPM4.5
      
      //将所有IO口配置为普通IO口
      P1DIR = 0x00;P2DIR = 0x00;P3DIR = 0x00;P4DIR = 0x00;P5DIR = 0x00;P6DIR = 0x00;
      PJDIR = 0x00;
      P1SEL = 0x00;P2SEL = 0x00;P3SEL = 0x00;P4SEL = 0x00;P5SEL = 0x00;P6SEL = 0x00;

      // 端口配置为下拉
//        P1REN = 0x00;//disabled Pullup or pulldown
//        P2REN = 0x00;
//        P3REN = 0x00;
//        P4REN = 0x00;
//        P5REN = 0x00;
//        P6REN = 0x00;

        // 端口配置为上拉
       P1REN = 0xFF;//disabled Pullup or pulldown
       P2REN = 0xFF;
       P3REN = 0xFF;
       P4REN = 0xFF;
       P5REN = 0xFF;
       P6REN = 0xFF;

      GPIO_ExtInt_Init();

//      UCSCTL4=UCSCTL4&(~(SELS_7|SELM_7))|SELS_1|SELM_1;
     //将SMCLK和MCLK配置为VLOCLK

      UCSCTL8 &= ~MCLKREQEN;
      UCSCTL8 &= ~ACLKREQEN;
      UCSCTL8 &= ~SMCLKREQEN;
      UCSCTL8 &= ~MODOSCREQEN;


      /* UCSCTL4&(~(SELS_7|SELM_7))这一语句相当于先把SELS和SELM清零*/
//   UCSCTL4=UCSCTL4&(~(SELS_7|SELM_7|SELA_7))|SELS_1|SELM_1;
  //将SMCLK和MCLK配置为VLOCLK

      PMMCTL0_H = PMMPW_H;                // Open PMM Registers for write
      PMMCTL0_L |= PMMREGOFF;             // and set PMMREGOFF

       SVSMLCTL &= ~SVMLE;   //关闭SVML模块
      SVSMLCTL &= ~SVSLE;   //关闭SVS模块

      SVSMHCTL &= ~SVSHE;
      SVSMHCTL &= ~SVMHE;

      PM5CTL0 &= ~LOCKLPM5;       //清除LOCKLPM5,解除端口状态锁定 锁定所有端口状态,
                                  //   必须在此之前将所有端口的状态改变为最低功耗,锁定。

      PMMCTL0_H = 0;     // Lock PMM Registers

    
      __bis_SR_register(LPM4_bits + GIE);