This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR2532:无法向 MSP430FR2532 ULP CapTIvate 代码添加延迟

Guru**** 2924050 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1316914/msp430fr2532-trouble-adding-delay-to-msp430fr2532-ulp-captivate-code

器件型号:MSP430FR2532

大家好!

我很难在 LED2保持运行的时间上增加延迟。

在以下代码中、没有出现延迟、一切正常、我得到了所需的消耗量。

#include <msp430.h>                      // Generic MSP430 Device Include
#include "driverlib.h"                   // MSPWare Driver Library
#include "captivate.h"                   // CapTIvate Touch Software Library
#include "CAPT_App.h"                    // CapTIvate Application Code
#include "CAPT_BSP.h"                    // CapTIvate EVM Board Support Package

void main(void)
{
	//
	// Initialize the MCU
	// BSP_configureMCU() sets up the device IO and clocking
	// The global interrupt enable is set to allow peripherals
	// to wake the MCU.
	//
	WDTCTL = WDTPW | WDTHOLD;
	BSP_configureMCU();
	__bis_SR_register(GIE);

	//
	// Start the CapTIvate application
	//
	CAPT_appStart();

	//
	// Background Loop
	//
	while(1)
	{
		//
		// Run the captivate application handler.
		// Set LED1 while the app handler is running,
		// and set LED2 if proximity is detected
		// on any sensor.
		//
		LED1_ON;
		if(CAPT_appHandler()==true)
			LED2_ON;
		else
			LED2_OFF;
		LED1_OFF;
		
		//
		// This is a great place to add in any 
		// background application code.
		//
		__no_operation();

		//
		// End of background loop iteration
		// Go to sleep if there is nothing left to do
		//
		CAPT_appSleep();
		
	} // End background loop
} // End main()

工程会成功构建;

但是、当我添加如下延迟(第94行)时、项目不会生成;

/* --COPYRIGHT--,BSD
 * Copyright (c) 2017, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * --/COPYRIGHT--*/
//*****************************************************************************
// Development main.c for MSP430FR2633, MSP430FR2533, MSP430FR2632, and
// MSP430FR2532.
//
// This starter application initializes the CapTIvate touch library
// for the touch panel specified by CAPT_UserConfig.c/.h via a call to
// CAPT_appStart(), which initializes and calibrates all sensors in the
// application, and starts the CapTIvate interval timer.
//
// Then, the capacitive touch interface is driven by calling the CapTIvate
// application handler, CAPT_appHandler().  The application handler manages
// whether the user interface (UI) is running in full active scan mode, or
// in a low-power wake-on-proximity mode.
//
// The CapTIvate application handler will return true if proximity was
// detected on any of the sensors in the application, which is used here
// to control the state of LED2. LED1 is set while the background loop enters
// the handler, and is cleared when the background loop leaves the handler.
//
// \version 1.83.00.05
// Released on May 15, 2020
//
//*****************************************************************************

#include <msp430.h>                      // Generic MSP430 Device Include
#include "driverlib.h"                   // MSPWare Driver Library
#include "captivate.h"                   // CapTIvate Touch Software Library
#include "CAPT_App.h"                    // CapTIvate Application Code
#include "CAPT_BSP.h"                    // CapTIvate EVM Board Support Package

void main(void)
{
	//
	// Initialize the MCU
	// BSP_configureMCU() sets up the device IO and clocking
	// The global interrupt enable is set to allow peripherals
	// to wake the MCU.
	//
	WDTCTL = WDTPW | WDTHOLD;
	BSP_configureMCU();
	__bis_SR_register(GIE);

	//
	// Start the CapTIvate application
	//
	CAPT_appStart();

	//
	// Background Loop
	//
	while(1)
	{
		//
		// Run the captivate application handler.
		// Set LED1 while the app handler is running,
		// and set LED2 if proximity is detected
		// on any sensor.
		//
		LED1_ON;
		if(CAPT_appHandler()==true)
			LED2_ON;
		// Add delay for 5 seconds
		            delay(5000000); // 5 seconds delay
		else
			LED2_OFF;
		LED1_OFF;
		
		//
		// This is a great place to add in any 
		// background application code.
		//
		__no_operation();

		//
		// End of background loop iteration
		// Go to sleep if there is nothing left to do
		//
		CAPT_appSleep();
		
	} // End background loop
} // End main()

我在构建控制台中得到以下编译失败信息;

我们将感谢您提供任何支持/指导。 如果您需要任何进一步的信息、请告诉我。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    1)显然没有名为"delay()"的函数可用。 我怀疑您需要"__delay_cycles (5000000);"。

    2) 2)您需要将 LED2_ON 和延迟放在大括号中("{}")

        (
            LED2_ON;
            // Add delay for 5 seconds
            __delay_cycles(5000000); // 5 seconds delay
        }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢你。 傻我。 这起作用了!