This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F6779:使用驱动程序库示例时 UART 无法执行 RX

Guru**** 2536210 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1319520/msp430f6779-uart-not-able-to-rx-using-driver-lib-example

器件型号:MSP430F6779

我正在尝试回波示例、我能够发送、但无法接收。 RX 中断标志没有达到高电平而触发中断

/* --COPYRIGHT--,BSD
 * Copyright (c) 2017, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * --/COPYRIGHT--*/
//******************************************************************************
//!  EUSCI_A0 External Loopback test using EUSCI_A_UART_init API
//!
//!  Description: This demo connects TX to RX of the MSP430 UART
//!  The example code shows proper initialization of registers
//!  and interrupts to receive and transmit data.
//!
//!  ACLK = BRCLK = 32.768kHz, MCLK = SMCLK = DCO/8 = ~1MHz
//!
//!
//!            Tested on MSP430F67791A
//!             -----------------
//!       RST -|     P3.0/UCA0RXD|----|
//!            |                 |    |
//!            |                 |    |
//!            |     P3.1/UCA0TXD|----|
//!            |                 |
//!
//! This example uses the following peripherals and I/O signals.  You must
//! review these and change as needed for your own board:
//! - UART peripheral
//! - GPIO Port peripheral (for UART pins)
//! - UCA0TXD
//! - UCA0RXD
//!
//! This example uses the following interrupt handlers.  To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - USCI_A0_VECTOR.
//******************************************************************************
#include "driverlib.h"

uint16_t i;
uint8_t RXData = 0, TXData = 0;
uint8_t check = 0;

void main(void)
{
    // stop watchdog
    WDT_A_hold(WDT_A_BASE);

    //Set external clock frequency to 32.768 KHz
    UCS_setExternalClockSource(32768, 0);
    //Set ACLK=XT1
    UCS_initClockSignal(UCS_ACLK, UCS_XT1CLK_SELECT, UCS_CLOCK_DIVIDER_1);
    //Start XT1 with no time out
    UCS_turnOnLFXT1(UCS_XT1_DRIVE_0, UCS_XCAP_3);

    //Configure UART pins (UCA0TXD/UCA0SIMO, UCA0RXD/UCA0SOMI)
    //Set P3.0 and P3.1 as Module Function Input
    GPIO_setAsPeripheralModuleFunctionInputPin(
        GPIO_PORT_P3,
        GPIO_PIN0 + GPIO_PIN1
        );

    // Configure UART
    EUSCI_A_UART_initParam param = {0};
    param.selectClockSource = EUSCI_A_UART_CLOCKSOURCE_ACLK;
    param.clockPrescalar = 3;
    param.firstModReg = 0;
    param.secondModReg = 92;
    param.parity = EUSCI_A_UART_NO_PARITY;
    param.msborLsbFirst = EUSCI_A_UART_LSB_FIRST;
    param.numberofStopBits = EUSCI_A_UART_ONE_STOP_BIT;
    param.uartMode = EUSCI_A_UART_MODE;
    param.overSampling = EUSCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;

    if (STATUS_FAIL == EUSCI_A_UART_init(EUSCI_A0_BASE, &param)) {
        return;
    }

    EUSCI_A_UART_enable(EUSCI_A0_BASE);

    EUSCI_A_UART_clearInterrupt(EUSCI_A0_BASE,
                         EUSCI_A_UART_RECEIVE_INTERRUPT);

    // Enable USCI_A0 RX interrupt
    EUSCI_A_UART_enableInterrupt(EUSCI_A0_BASE,
          EUSCI_A_UART_RECEIVE_INTERRUPT);                     // Enable interrupt

    __enable_interrupt();
    while (1)
    {
        TXData = TXData+1;                      // Increment TX data
        // Load data onto buffer
        EUSCI_A_UART_transmitData(EUSCI_A0_BASE,
                           TXData);
        while(check != 1);
        check = 0;
    }
}
//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(USCI_A0_VECTOR)))
#endif
void EUSCI_A0_ISR(void)
{
  switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG))
  {
    case USCI_NONE: break;
    case USCI_UART_UCRXIFG:
       RXData = EUSCI_A_UART_receiveData(EUSCI_A0_BASE);
      if(!(RXData == TXData))                   // Check value
      {
        while(1);
      }
      check =1;
      break;
    case USCI_UART_UCTXIFG: break;
    case USCI_UART_UCSTTIFG: break;
    case USCI_UART_UCTXCPTIFG: break;
  }
}
  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是否在 P3.0和 P3.1之间安装了跳线? [见评论第44-47行]

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这不是回声示例、而是回送测试。 它无法识别任何键盘输入。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、安装了跳线、TX 运行正常、但我无法接收数据   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你是正确的,但即使回送应该工作,我没有提供任何键盘输入. 但是、您可以看到我正在传输数据、并放置了一根跳线以短接 Rx 和 TX 引脚、因此我应该接收任何我正在传输的数据、但我无法接收   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您是否在跳线上放置了示波器、以确保传输数据?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此外、check 应为 volatile。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我使用了另一个控制器来接收数据、并且能够正确接收数据。 甚至可以 使用逻辑分析仪检查数据   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如何判断 TX 正在工作? 我问,因为我刚注意到 UCS_turnOnLFXT1将永远旋转,如果你的32kHz 晶体有什么问题。

    在这种情况下、您永远不会将其转到 while (1)循环。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我使用了另一个控制器来接收数据、并且能够正确接收数据。 甚至已使用逻辑分析仪检查数据。

    更详细地使用断点、我可以看到代码正在到达传输函数

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果您使用过这个程序来发送到另一个 MCU 并接收回来的东西、我认为唯一的区别是跳线。 您是否有可供换用的备用电源?  

    您还没有提到您的平台。 EVM [根据 SLAA577G]似乎只有一对用于 P3.0/1的抽头点(TX_EN、RX_EN 跳线引脚)、这会从物理上断开电路的 DB-9部分、从而防止任何冲突。 您的跳线在哪里?