This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F6779A:关于 POR 在库 PMM_setVCoreUp 中被禁用

Guru**** 2604225 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1323453/msp430f6779a-about-the-por-is-disable-in-the-library-pmm_setvcoreup

器件型号:MSP430F6779A

库 PMM_setVCoreUp 中禁用 POR

我们使用下面的库。

uint16_t PMM_setVCoreUp ( uint8_t level){
    uint32_t PMMRIE_backup, SVSMHCTL_backup, SVSMLCTL_backup;

    //The code flow for increasing the Vcore has been altered to work around
    //the erratum FLASH37.
    //Please refer to the Errata sheet to know if a specific device is affected
    //DO NOT ALTER THIS FUNCTION

    //Open PMM registers for write access
    HWREG8(PMM_BASE + OFS_PMMCTL0_H) = 0xA5;

    //Disable dedicated Interrupts
    //Backup all registers
    PMMRIE_backup = HWREG16(PMM_BASE + OFS_PMMRIE);
    HWREG16(PMM_BASE + OFS_PMMRIE) &= ~(SVMHVLRPE | SVSHPE | SVMLVLRPE |
                                          SVSLPE | SVMHVLRIE | SVMHIE |
                                          SVSMHDLYIE | SVMLVLRIE | SVMLIE |
                                          SVSMLDLYIE
                                          );
    SVSMHCTL_backup = HWREG16(PMM_BASE + OFS_SVSMHCTL);
    SVSMLCTL_backup = HWREG16(PMM_BASE + OFS_SVSMLCTL);

    //Clear flags
    HWREG16(PMM_BASE + OFS_PMMIFG) = 0;

    //Set SVM highside to new level and check if a VCore increase is possible
    HWREG16(PMM_BASE + OFS_SVSMHCTL) = SVMHE | SVSHE | (SVSMHRRL0 * level);

    //Wait until SVM highside is settled
    while ((HWREG16(PMM_BASE + OFS_PMMIFG) & SVSMHDLYIFG) == 0) ;

    //Clear flag
    HWREG16(PMM_BASE + OFS_PMMIFG) &= ~SVSMHDLYIFG;

    //Check if a VCore increase is possible
    if ((HWREG16(PMM_BASE + OFS_PMMIFG) & SVMHIFG) == SVMHIFG){
        //-> Vcc is too low for a Vcore increase
        //recover the previous settings
        HWREG16(PMM_BASE + OFS_PMMIFG) &= ~SVSMHDLYIFG;
        HWREG16(PMM_BASE + OFS_SVSMHCTL) = SVSMHCTL_backup;

        //Wait until SVM highside is settled
        while ((HWREG16(PMM_BASE + OFS_PMMIFG) & SVSMHDLYIFG) == 0) ;

        //Clear all Flags
        HWREG16(PMM_BASE +
            OFS_PMMIFG) &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
                             SVMLVLRIFG | SVMLIFG |
                             SVSMLDLYIFG
                             );

        //Restore PMM interrupt enable register
        HWREG16(PMM_BASE + OFS_PMMRIE) = PMMRIE_backup;
        //Lock PMM registers for write access
        HWREG8(PMM_BASE + OFS_PMMCTL0_H) = 0x00;
        //return: voltage not set
        return ( STATUS_FAIL) ;
    }

    //Set also SVS highside to new level
    //Vcc is high enough for a Vcore increase
    HWREG16(PMM_BASE + OFS_SVSMHCTL) |= (SVSHRVL0 * level);

    //Wait until SVM highside is settled
    while ((HWREG16(PMM_BASE + OFS_PMMIFG) & SVSMHDLYIFG) == 0) ;

    //Clear flag
    HWREG16(PMM_BASE + OFS_PMMIFG) &= ~SVSMHDLYIFG;

    //Set VCore to new level
    HWREG8(PMM_BASE + OFS_PMMCTL0_L) = PMMCOREV0 * level;

    //Set SVM, SVS low side to new level
    HWREG16(PMM_BASE + OFS_SVSMLCTL) = SVMLE | (SVSMLRRL0 * level) |
                                         SVSLE | (SVSLRVL0 * level);

    //Wait until SVM, SVS low side is settled
    while ((HWREG16(PMM_BASE + OFS_PMMIFG) & SVSMLDLYIFG) == 0) ;

    //Clear flag
    HWREG16(PMM_BASE + OFS_PMMIFG) &= ~SVSMLDLYIFG;
    //SVS, SVM core and high side are now set to protect for the new core level

    //Restore Low side settings
    //Clear all other bits _except_ level settings
    HWREG16(PMM_BASE + OFS_SVSMLCTL) &= (SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 +
                                           SVSMLRRL1 + SVSMLRRL2
                                           );

    //Clear level settings in the backup register,keep all other bits
    SVSMLCTL_backup &=
        ~(SVSLRVL0 + SVSLRVL1 + SVSMLRRL0 + SVSMLRRL1 + SVSMLRRL2);

    //Restore low-side SVS monitor settings
    HWREG16(PMM_BASE + OFS_SVSMLCTL) |= SVSMLCTL_backup;

    //Restore High side settings
    //Clear all other bits except level settings
    HWREG16(PMM_BASE + OFS_SVSMHCTL) &= (SVSHRVL0 + SVSHRVL1 +
                                           SVSMHRRL0 + SVSMHRRL1 +
                                           SVSMHRRL2
                                           );

    //Clear level settings in the backup register,keep all other bits
    SVSMHCTL_backup &=
        ~(SVSHRVL0 + SVSHRVL1 + SVSMHRRL0 + SVSMHRRL1 + SVSMHRRL2);

    //Restore backup
    HWREG16(PMM_BASE + OFS_SVSMHCTL) |= SVSMHCTL_backup;

    //Wait until high side, low side settled
    while (((HWREG16(PMM_BASE + OFS_PMMIFG) & SVSMLDLYIFG) == 0) ||
           ((HWREG16(PMM_BASE + OFS_PMMIFG) & SVSMHDLYIFG) == 0)) ;

    //Clear all Flags
    HWREG16(PMM_BASE + OFS_PMMIFG) &= ~(SVMHVLRIFG | SVMHIFG | SVSMHDLYIFG |
                                          SVMLVLRIFG | SVMLIFG | SVSMLDLYIFG
                                          );

    //Restore PMM interrupt enable register
    HWREG16(PMM_BASE + OFS_PMMRIE) = PMMRIE_backup;

    //Lock PMM registers for write access
    HWREG8(PMM_BASE + OFS_PMMCTL0_H) = 0x00;

    return ( STATUS_SUCCESS) ;
}

我试着测量 SVSLPE 和 SVSHPE 禁用 POR 的时序为500微秒。
因此、如果此时的电压降、MCU 可以在最小电压范围内运行。

在设置 VCORE 期间禁用 POR 的作用是什么?
如果在此期间出现压降(MCU 可能超出工作范围)、会发生什么情况?
是否有软件解决方案可防止 PMM_setVCoreUp 中出现压降时出现意外行为?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Tink:

    禁用 SVS 中断/POR 设置是为了保证在 VCORE 稳定到新值并且您移动 SVS 和 SVM 的阈值时、不会意外地触发一个 POR。

    如果您的 VDD 降至所需量以下、它仍会触发 BOR。

    您的电源+大容量电容器和去耦电容器应有助于防止器件降至可接受的 VDD 水平以下。 您使用什么来为器件供电?

    此致、

    卢克