This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR5969:TimerA 以 SMCLK (16MHz)运行时的最大计时器周期是多少?

Guru**** 2463330 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1409771/msp430fr5969-what-is-the-maximum-timer-period-when-timera-is-operated-at-smclk-16mhz

器件型号:MSP430FR5969

工具与软件:

TimerAをSMCLK(16MHz)で動作させたときの最大タイマー周期はどれくらいになりますでしょうか。

また、TA0CCR0の設定に関して最小値をご教示お願い致します。μ A