This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430F5529:USB 串行通信可以在 Windows 上工作、但不能在 Ubuntu 上工作

Guru**** 2616675 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1408880/msp430f5529-usb-serial-communication-works-on-windows-but-not-on-ubuntu

器件型号:MSP430F5529

工具与软件:

您好!

我已经从 SimpleUsbBackChannel 项目开始开发了一个项目(我已附加 main.c)。 基本来说、代码通过 USB 发送一些数字。 我可以在 Windows 上使用 Putty 看到输出。 但是、如果我使用 Ubuntu、则无法看到串行输出。 我正在使用屏幕查看 Ubuntu 中的串行通信。

使用此项目从 Windows 更改为 Ubuntu 时、是否会出现任何问题?

谢谢!

Alberto

/* --COPYRIGHT--,BSD
 * Copyright (c) 2012, Texas Instruments Incorporated
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 * --/COPYRIGHT--*/
//******************************************************************************
//   MSP430F5529LP:  simpleUsbBackchannel example
//
//   Description: 	Demonstrates simple sending over USB, as well as the F5529's
//                  backchannel UART.
//
//   Texas Instruments Inc.
//   August 2013
//******************************************************************************

// Basic MSP430 and driverLib #includes
#include "msp430.h"
#include "string.h"
#include "stdio.h"
#include "driverlib/MSP430F5xx_6xx/wdt_a.h"
#include "driverlib/MSP430F5xx_6xx/ucs.h"
#include "driverlib/MSP430F5xx_6xx/pmm.h"
#include "driverlib/MSP430F5xx_6xx/sfr.h"

// USB API #includes
#include "USB_config/descriptors.h"
#include "USB_API/USB_Common/device.h"
#include "USB_API/USB_Common/types.h"
#include "USB_API/USB_Common/usb.h"

#include "USB_app/usbConstructs.h"

// Application #includes
#include "BCUart.h"           // Include the backchannel UART "library"
#include "hal.h"              // Modify hal.h to select your hardware


/* You have a choice between implementing this as a CDC USB device, or a HID-
 * Datapipe device.  With CDC, the USB device presents a COM port on the host;
 * you interact with it with a terminal application, like Hyperterminal or
 * Docklight.  With HID-Datapipe, you interact with it using the Java HID Demo
 * App available within the MSP430 USB Developers Package.
 *
 * By default, this app uses CDC.  The HID calls are included, but commented
 * out.
 *
 * See the F5529 LaunchPad User's Guide for simple instructions to convert
 * this demo to HID-Datapipe.  For deeper information on CDC and HID-Datapipe,
 * see the USB API Programmer's Guide in the USB Developers Package.
 */


// Global variables
WORD rxByteCount;                        // Momentarily stores the number of bytes received
BYTE buf_bcuartToUsb[BC_RXBUF_SIZE];     // Same size as the UART's rcv buffer
BYTE buf_usbToBcuart[128];               // This can be any size


void main(void)
{
	WDTCTL = WDTPW + WDTHOLD;		// Halt the dog

    // MSP430 USB requires a Vcore setting of at least 2.  2 is high enough
	// for 8MHz MCLK, below.
    PMM_setVCore(PMM_CORE_LEVEL_2);

    //initPorts();           // Config all the GPIOS for low-power (output low)
    initClocks(8000000);   // Config clocks. MCLK=SMCLK=FLL=8MHz; ACLK=REFO=32kHz
    bcUartInit();          // Init the back-channel UART
    USB_setup(TRUE,TRUE);  // Init USB; if a USB host (PC) is present, connect

    P1DIR |= BIT3;              // P1.3 output
    P1OUT &= ~BIT3;             // P1.3 LOW

    P4DIR |= (BIT7 | BIT1);     // P4.1 & P4.7 output
    P4OUT &= ~(BIT7 | BIT1);    // p4.1 & P4.7 LOW

    // P1IES |= (BIT2);            // Rising Edge 0 -> 1
    P1IFG &= (~BIT2);           // Clear interrupt flag for P1.2

    int array[100];
    unsigned int i = 0;

    __enable_interrupt();  // Enable interrupts globally

    while(1)
    {
        P1OUT |= BIT3;      // Indicate start (trigger)

        for (i = 0; i < 100 ; i++)
        {
            array[i] = i + 1;
        }

        char buffer[4];
        for (i = 0; i < 100; i++)
        {
            sprintf(buffer, "%d ", array[i]); // Convert number to chain of characters
            cdcSendDataInBackground((BYTE*)buffer, strlen(buffer), CDC0_INTFNUM, 0); // Send counter value via USB
        }

        memset(array, 0, sizeof(array)); // Sets all positions of the array to 0

        __delay_cycles(1000000);

    }
    return 0;
}



  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    MCU 是否被识别? 您是否已安装驱动程序?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、可以识别。 这是我验证它的方式:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我的 Mac 上的屏幕工作正常。 枚举了两个端口、您是否选择了正确的端口?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、我选择了正确的这个、ttyACM0。 我无法通过屏幕打开另一个(tty0)、因此它肯定是 ttyACM0。

    注:我使用的是 Ubuntu 虚拟机。 SimpleUsbBackChannel 会创建一个额外的端口、即我正在虚拟机中使用的端口。 不过、请务必确保我还会筛选与 MSP430相关的其他端口、但不像预期的那样显示任何内容。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这似乎是一个 Ubuntu 问题。 它是否需要特定的硬件流控制配置? Windows 将忽略它、USB 应该无关紧要。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    据我所知、它不需要任何特定的硬件配置。 我是否应该在 Ubuntu 中配置除波特率以外的其他内容、停止奇偶校验...?