This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM3404MR/NOPB

Guru**** 2454880 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/other-wireless-group/other-wireless/f/other-wireless-technologies-forum/1118331/lm3404mr-nopb

在12V输入时、能快速启动带动9V / 3W的LED负载,不会出现启动时LED闪烁的情况,这个正常,

但是在输入14V或更高时,启动时输出不稳定,导致LED闪烁,有时甚至无法带动9V μ 3W负载。μ A

在低温-5℃时、输入12V / 14V都无法启动,无法使得LED点亮

在低温-5℃时、输入12V / 14V都无法启动,无法使得LED点亮,这是目前的主要问题点,我们在输入部分直接通过DC SUPPLIY 供电给IC(PIN8& GND),

此IC 仍然不能工作 μ A