This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] CC1352P:使用 CC1352P-2开发套件。 我希望通过 UART 将无线接收的数据发送到 PC

Guru**** 2813665 points

Other Parts Discussed in Thread: CC1352P

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/other-wireless-group/other-wireless/f/other-wireless-technologies-forum/1008066/cc1352p-use-cc1352p-2-development-kit-i-want-sent-the-data-received-by-wireless-to-pc-by-uart

器件型号:CC1352P

我使用了一个接收器,将两个示例项目 uart2callback_CC1352P_2_LAUNCHXL_tirtos_ccs 和 rfPacketRx_CC1352P_2_LAUNCHXL_tirtos_ccs 组合在一起。

我想通过 UART 端口将接收到的数据发送到 PC 进行显示。 我使用另一个无线发生器通过 rfListenBeforeTalk CC1352P_2_LAUNCHXL_tirtos_ccs 发送数据、

接收器可以在 debugge 状态下接收数据、但 UART 不会将数据发送到 PC、 调试必须停止一次、数据被发送。当数据正在运行时、接收器无法接收数据。 。

如何解决此问题?  

它是我编写的源代码。

/***** Function definitions *****/

void *mainThread(void *arg0)
{
    RF_Params rfParams;
    RF_Params_init(&rfParams);
    const char        echoPrompt[] = "Echoing characters:\r\n";
//
    UART2_Params      uartParams;
    int32_t           semStatus;
    uint32_t          status = UART2_STATUS_SUCCESS;
    uint8_t            bknumUart;
    /* Open LED pins */
    ledPinHandle = PIN_open(&ledPinState, pinTable);
    if (ledPinHandle == NULL)
    {
        while(1);
    }

    if( RFQueue_defineQueue(&dataQueue,
                            rxDataEntryBuffer,
                            sizeof(rxDataEntryBuffer),
                            NUM_DATA_ENTRIES,
                            MAX_LENGTH + NUM_APPENDED_BYTES))
    {
        /* Failed to allocate space for all data entries */
        while(1);
    }

    /* Modify CMD_PROP_RX command for application needs */
    /* Set the Data Entity queue for received data */
    RF_cmdPropRx.pQueue = &dataQueue;
    /* Discard ignored packets from Rx queue */
    RF_cmdPropRx.rxConf.bAutoFlushIgnored = 1;
    /* Discard packets with CRC error from Rx queue */
    RF_cmdPropRx.rxConf.bAutoFlushCrcErr = 1;
    /* Implement packet length filtering to avoid PROP_ERROR_RXBUF */
    RF_cmdPropRx.maxPktLen = MAX_LENGTH;
    RF_cmdPropRx.pktConf.bRepeatOk = 1;
    RF_cmdPropRx.pktConf.bRepeatNok = 1;

    /* Request access to the radio */
#if defined(DeviceFamily_CC26X0R2)
    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioSetup, &rfParams);
#else
    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
#endif// DeviceFamily_CC26X0R2

    /* Set the frequency */
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);

    /* Enter RX mode and stay forever in RX */
    RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRx,
                                               RF_PriorityNormal, &callback,
                                               RF_EventRxEntryDone);

    switch(terminationReason)
    {
        case RF_EventLastCmdDone:
            // A stand-alone radio operation command or the last radio
            // operation command in a chain finished.
            break;
        case RF_EventCmdCancelled:
            // Command cancelled before it was started; it can be caused
            // by RF_cancelCmd() or RF_flushCmd().
            break;
        case RF_EventCmdAborted:
            // Abrupt command termination caused by RF_cancelCmd() or
            // RF_flushCmd().
            break;
        case RF_EventCmdStopped:
            // Graceful command termination caused by RF_cancelCmd() or
            // RF_flushCmd().
            break;
        default:
            // Uncaught error event
            while(1);
    }

    uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropRx)->status;
    switch(cmdStatus)
    {
        case PROP_DONE_OK:
            // Packet received with CRC OK
            break;
        case PROP_DONE_RXERR:
            // Packet received with CRC error
            break;
        case PROP_DONE_RXTIMEOUT:
            // Observed end trigger while in sync search
            break;
        case PROP_DONE_BREAK:
            // Observed end trigger while receiving packet when the command is
            // configured with endType set to 1
            break;
        case PROP_DONE_ENDED:
            // Received packet after having observed the end trigger; if the
            // command is configured with endType set to 0, the end trigger
            // will not terminate an ongoing reception
            break;
        case PROP_DONE_STOPPED:
            // received CMD_STOP after command started and, if sync found,
            // packet is received
            break;
        case PROP_DONE_ABORT:
            // Received CMD_ABORT after command started
            break;
        case PROP_ERROR_RXBUF:
            // No RX buffer large enough for the received data available at
            // the start of a packet
            break;
        case PROP_ERROR_RXFULL:
            // Out of RX buffer space during reception in a partial read
            break;
        case PROP_ERROR_PAR:
            // Observed illegal parameter
            break;
        case PROP_ERROR_NO_SETUP:
            // Command sent without setting up the radio in a supported
            // mode using CMD_PROP_RADIO_SETUP or CMD_RADIO_SETUP
            break;
        case PROP_ERROR_NO_FS:
            // Command sent without the synthesizer being programmed
            break;
        case PROP_ERROR_RXOVF:
            // RX overflow observed during operation
            break;
        default:
            // Uncaught error event - these could come from the
            // pool of states defined in rf_mailbox.h
            while(1);
    }
    /* Create semaphore */
        semStatus = sem_init(&sem, 0, 0);

        if (semStatus != 0) {
            /* Error creating semaphore */
            while (1);
        }

        /* Create a UART in CALLBACK read mode */
        UART2_Params_init(&uartParams);
        uartParams.readMode = UART2_Mode_CALLBACK;
        uartParams.readCallback = callbackFxn;
        uartParams.baudRate = 2000000;

        uart = UART2_open(CONFIG_UART2_0, &uartParams);

        if (uart == NULL) {
            /* UART2_open() failed */
            while (1);
        }

        /* Pass NULL for bytesWritten since it's not used in this example */
        UART2_write(uart, echoPrompt, sizeof(echoPrompt), NULL);

        numBytesRead = 0;

         /* Pass NULL for bytesRead since it's not used in this example */
       //  status = UART2_readTimeout(uart, &input,1, NULL,1);

         if (status != UART2_STATUS_SUCCESS) {
             /* UART2_read() failed */
             while (1);
         }
    while(1){
        /* Do not write until read callback executes */
   //      sem_wait(&sem);

         if (numUart > 0) {
             bknumUart   = numUart;
             numUart     = 0;
  //           status = UART2_write(uart, input, 100, NULL);
             UART_polling(bknumUart);
             bknumUart = 0;
             if (status != UART2_STATUS_SUCCESS) {
                 /* UART2_write() failed */
                 while (1);
             }
         }
         while(rfnum > 0){
             UART2_write(uart, &rfrxpacket[rfrp], 1, NULL);
             rfnum--;

             rfrp++;
             if(rfrp >= MAX_BUFF_LENGTH){
                 rfrp   = 0;
             }
         }


    }
}

void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
{
    int i;
    if (e & RF_EventRxEntryDone)
    {
        /* Toggle pin to indicate RX */
        PIN_setOutputValue(ledPinHandle, CONFIG_PIN_RLED,
                           !PIN_getOutputValue(CONFIG_PIN_RLED));

        /* Get current unhandled data entry */
        currentDataEntry = RFQueue_getDataEntry();

        /* Handle the packet data, located at &currentDataEntry->data:
         * - Length is the first byte with the current configuration
         * - Data starts from the second byte */
        packetLength      = *(uint8_t*)(&currentDataEntry->data);
        packetDataPointer = (uint8_t*)(&currentDataEntry->data + 1);

        /* Copy the payload + the status byte to the packet variable */
        for(i= 0;i< packetLength + 1 ; i++){
            rfrxpacket[rfwp] = *(packetDataPointer + i);
            rfwp++;
            rfnum++;
            if(rfwp >= MAX_BUFF_LENGTH){
                rfwp    = 0;
            }
        }

        RFQueue_nextEntry();

    }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Xiaohong、

    您似乎有一些小错误、例如在下面、您已注释出状态、但尚未注释出关联的 while 循环。

             /* Pass NULL for bytesRead since it's not used in this example */
           //  status = UART2_readTimeout(uart, &input,1, NULL,1);
    
             if (status != UART2_STATUS_SUCCESS) {
                 /* UART2_read() failed */
                 while (1);
             }

    我认为一个很好的调试步骤是运行程序、按暂停并查看程序计数器的位置(查看正在执行的代码)。 您可以使用断点来查看何时执行哪个代码。

    您能更详细地解释一下您的代码架构吗? 哪个任务/线程发生了什么情况、谁正在发送和等待信号量等?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您回答问题。

    我搜索了停止点。 这种情况   

    /*等待信号量*/
    SemaphoreP_pend (&h->state.semSync、100);

    我可以简单地更改它吗?  这是否意味着 等待100秒?

    =>?

    SemaphoreP_pend (&h->state.semSync、1);

     

    如果没有收到无线数据、我首先要向 PC 发送什么数据、我该怎么办?

    目前的情况是,我一直在等待。

    /*等待信号量*/

    SemaphoreP_pend (&h->state.semSync、100);

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Xiaohong、

    您可以在 以下位置读取 Semaphore_pend()的文档:https://dev.ti.com/tirex/explore/content/simplelink_cc13x2_26x2_sdk_5_10_00_48/docs/tirtos/sysbios/docs/cdoc/index.html 

    如您所见、此 API 将等待一个信标被布置或超时已过期。 超时在系统节拍中定义。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我不知道如何使用半海。

    我 修改了源代码。  它可以在我停止调试后发送数据。

    我在 PC 中看到的数据 仅像这样两次。

    首先发送"回显字符:\r\n"  

    paket 是数据0~1D

    无法连续和自动接收数据

    base 为 rfPacketRx_CC1352P_2_LAUNCHXL_tirtos_ccs。 我添加了 UART。

    我 通过 rfPacketTx_CC1352P_2_LAUNCHXL_tirtos_ccs 每秒发送一次射频数据。  

    rfPacketRx.c

    /***** Includes *****/
    /* Standard C Libraries */
    #include <stdlib.h>
    
    /* TI Drivers */
    #include <ti/drivers/rf/RF.h>
    #include <ti/drivers/PIN.h>
    
    /* Driverlib Header files */
    #include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)
    
    /* Board Header files */
    #include "ti_drivers_config.h"
    
    /* Application Header files */
    #include "RFQueue.h"
    #include <ti_radio_config.h>
    #include <semaphore.h>
    
    #include <ti/drivers/GPIO.h>
    #include <ti/drivers/UART2.h>
    #include <application.h>
    
    
    /***** Defines *****/
    
    /* Packet RX Configuration */
    //#define DATA_ENTRY_HEADER_SIZE 8 /* Constant header size of a Generic Data Entry */
    //#define MAX_LENGTH 30 /* Max length byte the radio will accept */
    //#define NUM_DATA_ENTRIES 2 /* NOTE: Only two data entries supported at the moment */
    //#define NUM_APPENDED_BYTES 2 /* The Data Entries data field will contain:
    // * 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1)
    // * Max 30 payload bytes
    // * 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */
    
    
    
    /***** Prototypes *****/
    static void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e);
    
    /***** Variable declarations *****/
    static RF_Object rfObject;
    static RF_Handle rfHandle;
    
    /* Pin driver handle */
    static PIN_Handle ledPinHandle;
    static PIN_State ledPinState;
    
    /* Buffer which contains all Data Entries for receiving data.
    * Pragmas are needed to make sure this buffer is 4 byte aligned (requirement from the RF Core) */
    #if defined(__TI_COMPILER_VERSION__)
    #pragma DATA_ALIGN (rxDataEntryBuffer, 4);
    static uint8_t
    rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
    MAX_LENGTH,
    NUM_APPENDED_BYTES)];
    #elif defined(__IAR_SYSTEMS_ICC__)
    #pragma data_alignment = 4
    static uint8_t
    rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
    MAX_LENGTH,
    NUM_APPENDED_BYTES)];
    #elif defined(__GNUC__)
    static uint8_t
    rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
    MAX_LENGTH,
    NUM_APPENDED_BYTES)]
    __attribute__((aligned(4)));
    #else
    #error This compiler is not supported.
    #endif
    
    /* Receive dataQueue for RF Core to fill in data */
    static dataQueue_t dataQueue;
    static rfc_dataEntryGeneral_t* currentDataEntry;
    static uint8_t packetLength;
    static uint8_t* packetDataPointer;
    
    
    static uint8_t packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1]; /* The length byte is stored in a separate variable */
    static uint8_t rfLength;
    
    static sem_t semrf;
    
    
    extern UART2_Handle uart;
    extern void callbackFxn(UART2_Handle handle, void *buffer, size_t count,
    void *userArg, int_fast16_t status);
    /*
    * Application LED pin configuration table:
    * - All LEDs board LEDs are off.
    */
    PIN_Config pinTable[] =
    {
    CONFIG_PIN_RLED | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
    };
    
    /***** Function definitions *****/
    
    void *rfThread(void *arg0)
    {
    
    RF_Params rfParams;
    RF_Params_init(&rfParams);
    UART2_Params uartParams;
    int32_t semStatus;
    uint32_t status = UART2_STATUS_SUCCESS;
    const char echoPrompt[] = "Echoing characters:\r\n";
    
    /* Create semaphore */
    semStatus = sem_init(&semrf, 0, 0);
    
    /* Open LED pins */
    /* ledPinHandle = PIN_open(&ledPinState, pinTable);
    if (ledPinHandle == NULL)
    {
    while(1);
    }
    */
    if( RFQueue_defineQueue(&dataQueue,
    rxDataEntryBuffer,
    sizeof(rxDataEntryBuffer),
    NUM_DATA_ENTRIES,
    MAX_LENGTH + NUM_APPENDED_BYTES))
    {
    /* Failed to allocate space for all data entries */
    while(1);
    }
    
    /* Modify CMD_PROP_RX command for application needs */
    /* Set the Data Entity queue for received data */
    RF_cmdPropRx.pQueue = &dataQueue;
    /* Discard ignored packets from Rx queue */
    RF_cmdPropRx.rxConf.bAutoFlushIgnored = 1;
    /* Discard packets with CRC error from Rx queue */
    RF_cmdPropRx.rxConf.bAutoFlushCrcErr = 1;
    /* Implement packet length filtering to avoid PROP_ERROR_RXBUF */
    RF_cmdPropRx.maxPktLen = MAX_LENGTH;
    RF_cmdPropRx.pktConf.bRepeatOk = 1;
    RF_cmdPropRx.pktConf.bRepeatNok = 1;
    
    /* Request access to the radio */
    #if defined(DeviceFamily_CC26X0R2)
    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioSetup, &rfParams);
    #else
    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
    #endif// DeviceFamily_CC26X0R2
    
    /* Set the frequency */
    RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
    
    /* Enter RX mode and stay forever in RX */
    RF_EventMask terminationReason = RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRx,
    RF_PriorityNormal, &callback,
    RF_EventRxEntryDone);
    
    switch(terminationReason)
    {
    case RF_EventLastCmdDone:
    // A stand-alone radio operation command or the last radio
    // operation command in a chain finished.
    break;
    case RF_EventCmdCancelled:
    // Command cancelled before it was started; it can be caused
    // by RF_cancelCmd() or RF_flushCmd().
    break;
    case RF_EventCmdAborted:
    // Abrupt command termination caused by RF_cancelCmd() or
    // RF_flushCmd().
    break;
    case RF_EventCmdStopped:
    // Graceful command termination caused by RF_cancelCmd() or
    // RF_flushCmd().
    break;
    default:
    // Uncaught error event
    while(1);
    }
    
    uint32_t cmdStatus = ((volatile RF_Op*)&RF_cmdPropRx)->status;
    switch(cmdStatus)
    {
    case PROP_DONE_OK:
    // Packet received with CRC OK
    break;
    case PROP_DONE_RXERR:
    // Packet received with CRC error
    break;
    case PROP_DONE_RXTIMEOUT:
    // Observed end trigger while in sync search
    break;
    case PROP_DONE_BREAK:
    // Observed end trigger while receiving packet when the command is
    // configured with endType set to 1
    break;
    case PROP_DONE_ENDED:
    // Received packet after having observed the end trigger; if the
    // command is configured with endType set to 0, the end trigger
    // will not terminate an ongoing reception
    break;
    case PROP_DONE_STOPPED:
    // received CMD_STOP after command started and, if sync found,
    // packet is received
    break;
    case PROP_DONE_ABORT:
    // Received CMD_ABORT after command started
    break;
    case PROP_ERROR_RXBUF:
    // No RX buffer large enough for the received data available at
    // the start of a packet
    break;
    case PROP_ERROR_RXFULL:
    // Out of RX buffer space during reception in a partial read
    break;
    case PROP_ERROR_PAR:
    // Observed illegal parameter
    break;
    case PROP_ERROR_NO_SETUP:
    // Command sent without setting up the radio in a supported
    // mode using CMD_PROP_RADIO_SETUP or CMD_RADIO_SETUP
    break;
    case PROP_ERROR_NO_FS:
    // Command sent without the synthesizer being programmed
    break;
    case PROP_ERROR_RXOVF:
    // RX overflow observed during operation
    break;
    default:
    // Uncaught error event - these could come from the
    // pool of states defined in rf_mailbox.h
    while(1);
    }
    /* Create a UART in CALLBACK read mode */
    UART2_Params_init(&uartParams);
    uartParams.readMode = UART2_Mode_CALLBACK;
    uartParams.readCallback = callbackFxn;
    uartParams.baudRate = 2000000;
    
    uart = UART2_open(CONFIG_UART2_0, &uartParams);
    
    if (uart == NULL) {
    /* UART2_open() failed */
    while (1);
    }
    
    /* Pass NULL for bytesWritten since it's not used in this example */
    UART2_write(uart, echoPrompt, sizeof(echoPrompt), NULL);
    while(1){
    sem_wait(&semrf);
    // sem_post(&sem);
    
    UART2_write(uart, &packet, packetLength, NULL);
    }
    }
    
    void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
    {
    if (e & RF_EventRxEntryDone)
    {
    /* Toggle pin to indicate RX */
    PIN_setOutputValue(ledPinHandle, CONFIG_PIN_RLED,
    !PIN_getOutputValue(CONFIG_PIN_RLED));
    
    /* Get current unhandled data entry */
    currentDataEntry = RFQueue_getDataEntry();
    
    /* Handle the packet data, located at &currentDataEntry->data:
    * - Length is the first byte with the current configuration
    * - Data starts from the second byte */
    packetLength = *(uint8_t*)(&currentDataEntry->data);
    packetDataPointer = (uint8_t*)(&currentDataEntry->data + 1);
    
    /* Copy the payload + the status byte to the packet variable */
    memcpy(packet, packetDataPointer, (packetLength + 1));
    rfLength = packetLength + 1;
    
    sem_post(&semrf);
    
    RFQueue_nextEntry();
    }
    }
    
    
    
    
    
    
    
    
    
    

    main_tirtos.c

    /*
     * application.h
     *
     *  Created on: 2021/06/15
     *      Author: ZOU
     */
    
    #ifndef APPLICATION_H_
    #define APPLICATION_H_
    
    /* Packet RX Configuration */
    #define DATA_ENTRY_HEADER_SIZE 8  /* Constant header size of a Generic Data Entry */
    #define MAX_LENGTH             30 /* Max length byte the radio will accept */
    #define NUM_DATA_ENTRIES       2  /* NOTE: Only two data entries supported at the moment */
    #define NUM_APPENDED_BYTES     2  /* The Data Entries data field will contain:
                                       * 1 Header byte (RF_cmdPropRx.rxConf.bIncludeHdr = 0x1)
                                       * Max 30 payload bytes
                                       * 1 status byte (RF_cmdPropRx.rxConf.bAppendStatus = 0x1) */
    
    
    static uint8_t packet[MAX_LENGTH + NUM_APPENDED_BYTES - 1]; /* The length byte is stored in a separate variable */
    static uint8_t  rfLength;
    
    static sem_t sem;
    
    
    #endif /* APPLICATION_H_ */
    

    extern void *rfThread(void *arg0);
    extern void *uartThread(void *arg0);
    
    /* Stack size in bytes */
    #define THREADSTACKSIZE    2096
    
    /*
     *  ======== main ========
     */
    int main(void)
    {
        pthread_t           thread;
        pthread_attr_t      attrs;
        struct sched_param  priParam;
        int                 retc;
        int                 detachState;
    
        /* Call driver init functions */
        Board_initGeneral();
    
        /* Set priority and stack size attributes */
        pthread_attr_init(&attrs);
        priParam.sched_priority = 1;
    
        detachState = PTHREAD_CREATE_DETACHED;
        retc = pthread_attr_setdetachstate(&attrs, detachState);
        if (retc != 0) {
            /* pthread_attr_setdetachstate() failed */
            while (1);
        }
    
        pthread_attr_setschedparam(&attrs, &priParam);
    
        retc |= pthread_attr_setstacksize(&attrs, THREADSTACKSIZE);
        if (retc != 0) {
            /* pthread_attr_setstacksize() failed */
            while (1);
        }
    
        retc = pthread_create(&thread, &attrs, rfThread, NULL);
        if (retc != 0) {
            /* pthread_create() failed */
            while (1);
        }
    
    //    priParam.sched_priority = 2;
    //    pthread_attr_setschedparam(&attrs, &priParam);
    //    retc = pthread_create(&thread, &attrs, uartThread, NULL);
    //    if (retc != 0) {
            /* pthread_create() failed */
    //        while (1);
    //    }
    

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Xihong、

    当您说启动和停止调试时、您意味着启动和停止调试会话吗? 您是否记得在启动调试会话后按"Play"?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当 在 rfPacketRx.c 的第250和278行中设置断点时、UART 可以发送数据。 如果未设置、则不会发送任何数据。

    e2e.ti.com/.../b4167b1dd784cbdb4ac70312ea2b1a83.mp4

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Xiaohong、

    我关于调试这种问题的提示是、我想退一步、简要了解一下您正在运行的代码。 由于除非您设置断点、否则不会发送数据、因此似乎有人会阻止它?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    无线接收中断。后、似乎无法进入主 while 循环

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Xihong、

    好的、射频 RX 是如何构建的? 它是否在某处旋转、使 PC 不会返回主循环?