This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TRF7960A:TRF7960A 特定于 MIFARE

Guru**** 2558250 points
Other Parts Discussed in Thread: TRF7960A, TRF7970A

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/other-wireless-group/other-wireless/f/other-wireless-technologies-forum/1361748/trf7960a-mifare-specific-of-trf7960a

器件型号:TRF7960A
主题中讨论的其他器件: TRF7970A

您好!

您能否告诉我 TRF7960A 是否支持以下功能?

・ISO/IEC14443A MIFARE 1K 4K
・ISO/IEC14443A MIFARE UL AES
・ISO/IEC14443A MIFARE Plus
・ISO/IEC14443A MIFARE DESFire

谢谢。

科诺