This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TRF7970A:TRF7970AEVM

Guru**** 2555630 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/wireless-connectivity/other-wireless-group/other-wireless/f/other-wireless-technologies-forum/1404471/trf7970a-trf7970aevm

器件型号:TRF7970A

工具与软件:

您好、先生、

您知道如何通过 MATLAB 与 TRF7970AEVM 通信吗? 我知道我应该发送什么命令、但芯片完全没有响应。

clear all;
clc;
ports = serialportlist;
% Set up serial communication (assuming UART interface)
s = serialport(ports, 115200, "Timeout", 3);  % Modify COM port as needed

% Function to send command to TRF7970A and read the response
function response = sendCommand(s, cmd)
    write(s, cmd,"uint8");
    pause(0.1);  % Small delay to allow processing time
    response = read(s, 32, "uint8");  % Adjust read length as needed
end

% 1. Send a simple command to test the response
% Example: Send a command to read a TRF7970A register
simpleCmd = [0x01 0x08  0x00 0x03 0x04 0xFF 0x00 0x00];  % Example: Idle command
response = sendCommand(s, simpleCmd);

% Display the response for debugging
disp('Simple command response:');
disp(response);