This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ25895:无法以合理的成本提供60uF SMT 电容器、可以使用3个22uF 吗?

Guru**** 2731945 points

Other Parts Discussed in Thread: BQ25895

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1486511/bq25895-unable-to-source-60uf-smt-capacitor-at-reasonable-cost-ok-to-use-3x-22uf

器件型号:BQ25895

工具与软件:

您好!

我正在为基于 BQ25895的设计收集器件信息、并计划在3.1A 条件下使用完整的5V 电压(PMID 提供了该电压)、但是数据表指定了一个60uF 的电容器、我无法以合理的成本买到该电容器。 可以用3个22uF 0805电容器代替它吗?或者这会导致任何可疑行为吗?