This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ2.4075万:原理图检查

Guru**** 1125150 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1097395/bq24075-schematic-check

部件号:BQ2.4075万

你(们)好  

您是否可以帮助检查以下BQ2.4075万示意图以及是否需要调整?

设计要求

电源电压= 5 V

 

快速充电电流约为500 mA;=> RISET:17.8K欧姆

 

输入电流限制=1A;=> RISET:1.6K欧姆

 

安全计时器持续时间,快速充电=6小时;=> RTRM:45.3K欧姆

 

TS蓄电池温度感应=请勿使用;=>低拉10K欧姆