This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ24073:BQ24073输出电流?

Guru**** 2511415 points
Other Parts Discussed in Thread: BQ24073

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1026363/bq24073-bq24073-output-current

器件型号:BQ24073

在 BQ24073数据表8页[8.3推荐运行条件]中、

 输入电流,IN 引脚:1.5A

 -电流,OUT 引脚:4.5A

 -电流,BAT 针脚(放电):4.5A

 -电流,BAT 针脚(充电):1.5A

如果 同时描述了[电流、输出引脚:4.5A]和[电流、输出引脚:4.5A],则电池和适配器是否都可以使用4.5A 负载?

输入电流(1.5A)包括系统负载和电池充电电流。

如何使用高达4.5A 的输出电流?

然后、将输入电流(ILIM)设置为1.5A 后、我是否可以使用500mA 的充电电流和4A 的负载电流?

谢谢你。