请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TLV61048大家好、团队、
您能不能为 具有带磁滞、Vin 和 Vout 去耦合的 UVLO 的直流/直流转换器推荐最佳器件
输入电压:3.0至4.2- 1节锂离子电池,输出电压12V,输出电流>0.2A?
提前感谢。
此致、
Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.