请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS61196 您好!
TPS61196能否达到400mA 并满足以下规格?
输入=24VDC
输出= 36V/400mA * 6通道 LED (需要电流平衡)
必须具有调光功能(45ms 打开/45ms 关闭)
当驱动器异常时、需要引脚发送一个错误信号 (例如 OVP.OTP.OCP.OPEN...)
总功率86.4W
此致
摇滚
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.