从上电(施加 VDD)开始、SMBus 接口何时可用于接受主器件访问?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最后一个问题:我不确定 ADDR[1:0]到底是如何工作的。
根据数据表、ADDR1设置10s 位、而 ADDR0设置1s 位。 例如、如果 ADDR1上的下拉电阻为127K、ADDR0上的下拉电阻为38.3K、则 I2C 从器件地址将为63。 正确吗? 63是十进制还是十六进制? 它是7位地址还是8位地址?
然后、如果您查看数据表中的参考设计、ADDR1和 ADDR0均会下拉36.5K 欧姆、这一点未在第26页的表3中定义。 那么、它将器件绑定到哪个8位十六进制地址?
作为参考、8位地址意味着位[0]处的焊盘0。 您知道 I2C 协议中的位[0]是读取/写入指示器。 一个7位地址7'b1010000将等于8位地址8'b10100000。
谢谢。。。