Other Parts Discussed in Thread: BQ25616
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25616 尊敬的先生/女士:
我对 BQ25616有疑问、从下表中可以看到、只有外部 N-FET 或仅高电压交流/直流才能实现130ns 反应时间?
如果交流/直流是5V 输出、则不需要?
此致、
公里/小时
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.