请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS40050 你(们)好
TPS40050和 TPS40050-Q1之间的区别是什么、后者符合 AEC 标准、温度范围为-40至+125。 性能计算是否有差异? 能否在不更改电路的情况下将 TPS40050-Q1替换为 TPS40050?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
TPS40050和 TPS40050-Q1之间的区别是什么、后者符合 AEC 标准、温度范围为-40至+125。 性能计算是否有差异? 能否在不更改电路的情况下将 TPS40050-Q1替换为 TPS40050?