Other Parts Discussed in Thread: LM3410, TPS61500
主题中讨论的其他器件: TPS61500
可以有人确认 LM3410能够驱动我的电路吗
我的应用电路如下所示
输入
VIN = 3.1V - 4.2V (锂聚合物电池)
ILED = 25mA
VFB = 2.1V
15个串联10个 LED 的灯串
假设
VOUT ~ 22V (小于24V)
总电流~ 250mA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.