请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:TIDA-00127您好!
我必须设计具有以下详细信息的交流/直流转换器、
输入电压: 30至500VAC (L-L)、三相、50Hz
2.输出电压:24V、10A。
应符合 MIL-STD-461E 标准
请向我们推荐符合上述要求的任何设计/想法/电路。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我必须设计具有以下详细信息的交流/直流转换器、
输入电压: 30至500VAC (L-L)、三相、50Hz
2.输出电压:24V、10A。
应符合 MIL-STD-461E 标准
请向我们推荐符合上述要求的任何设计/想法/电路。