请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ25606、 BQ25895、 BQ25601你好
我们是否有可在 60°C 温度下充电的充电器、输入5V、输出电流最大3A 解决方案? 谢谢你。
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.