This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS54240-Q1:产品性

Guru**** 1138100 points
Other Parts Discussed in Thread: TPS54240
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/792898/tps54240-q1-productiveness

器件型号:TPS54240-Q1
主题中讨论的其他器件:TPS54240

我们在使用 TPS54240时遇到了一些问题、因此请查看输入:12? 36V 输出需要5V? 2A、实际测量、低效率(在输入电压12V 下测试) 1A 效率78% 0.5A 效率82% 1.5A 效率50%