请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:UCC2897A您好!
我们是否有 适用于200W 的直流/直流9V~36V 至12V 隔离式电源解决方案以及适合客户的任何参考设计? 谢谢你。
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.