请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM74501-Q1 你(们)好
我客户的应用是24V 汽车、浪涌测试要求是 +150V 和-450V 脉冲。
LM74501-Q1添加一些外部组件是否可以通过 +150V 和-450V 脉冲测试?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
我客户的应用是24V 汽车、浪涌测试要求是 +150V 和-450V 脉冲。
LM74501-Q1添加一些外部组件是否可以通过 +150V 和-450V 脉冲测试?