请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC27712 您好、TI 专家,
使用ucc27712半桥驱动,
输入由MCU直接输入,输出驱动电阻10mohm
输入电压50V没问题,输入电压高于70V就烧驱动,上管驱动总也损坏,请帮忙看分析下可能的问题原因。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.