Other Parts Discussed in Thread: LM5177
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5177大家好、
我的客户正在寻找一种能够处理30-60V 输入电压和48V 输出电压、恒定15A 输出电流的电源解决方案。 您可以推荐一款器件吗?
Br
锡鲁伊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.