Other Parts Discussed in Thread: LM5146
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5146 您好!
Q29、Q30 FET 出现热问题。
请查看原理图并提供您对散热问题的看法。

条件如下所示。
- 输入:65~80VDC
- 输出:24 VDC
- 2A ~3A
- L1电感 : SRP1038C-330M (33uH/4A、112m Ω)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.