请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2642 我已经通读了该部件的数据表、并查看了适用于3V/5V 单相/双通道应用(图2)和双相/单通道1.8V 应用(图3)的典型应用电路。 我想知道12V 两相/单通道典型应用电路是否存在于任何地方、因为我认为此配置是此芯片的常见用例。 在我的特殊情况下、我要输入24V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我已经通读了该部件的数据表、并查看了适用于3V/5V 单相/双通道应用(图2)和双相/单通道1.8V 应用(图3)的典型应用电路。 我想知道12V 两相/单通道典型应用电路是否存在于任何地方、因为我认为此配置是此芯片的常见用例。 在我的特殊情况下、我要输入24V。