This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ27Z561-R2:小电流应用感测电阻

Guru**** 2771175 points

Other Parts Discussed in Thread: BQ27Z561-R2, BQSTUDIO

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1357570/bq27z561-r2-sense-resistor-for-small-current-application

器件型号:BQ27Z561-R2
主题中讨论的其他器件:BQ25792、、 BQSTUDIO

您好!

我正在使用一个由3节并联 LiFePo4电池供电的系统、可提供约3.2V 的总电压和4500mA 4552的容量。

该系统抽取:

  • 正常运行时从2mA 切换到500mA
  • 以较低功耗模式运行时从100µA 转换为300µA

充电器(BQ25792)经配置可提供最大2.5安培的充电电流。

在浏览 TI 电量监测计时、我发现 BQ27Z561-R2符合我的需求、但技术文档明确指出"该器件旨在支持1-mΩ 至3-mΩ 感应电阻器"

我原本打算使用30mΩ 转50mΩ 传感电阻器、但我不确定它是否会正常发挥功能、尤其是因为我需要具有大于250µA 电流分辨率且大于0.2µA 电流精度。

是否可以放置一个30mΩ 感应电阻器? BQStudio 能否直接校准此值以进行电流计算?

谢谢。