请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62933 使用数据表上的基准电路、我能够在第一次上电时获得5V 的输出电压。 但是、在第二次上电后、我无法再获得5V 输出电压。 输入电压为正确的8V。
我还检查了除 TPS62933之外的所有电阻器和电容器的正确性。
我不确定我是否会在从同一个8v 电源驱动两个 TPS6933时遇到问题。
下面是电路原理图


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.