This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ28Z610-R1:BQ28Z610-R1

Guru**** 2516170 points
Other Parts Discussed in Thread: BQ28Z610-R1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1478122/bq28z610-r1-bq28z610-r1

器件型号:BQ28Z610-R1

工具与软件:

BQ28Z610-R1配置有高温降压充电。 0~45℃ 时的完整充电电压为8.648V、45~60℃ 时的完整充电电压为8.4V。

电池以8.648V 5A 开始以30℃ 充电、一段时间后、电池温度开始上升、当电池达到46℃ 时、RSOC 为70%、然后降压充电开始、充电器开始下降到8.4V、1152mA 电流为电池充电、 但是当电荷达到91%时、就会达到满电荷切断条件。此时、RSOC 直接从91%跳到100%、有没有办法让 RSOC 不跳跃而是平滑到100%呢?

gg. file 请参阅附件。 电池的化合物 ID 为1735.e2e.ti.com/.../2630.gg.csv