工具与软件:
尊敬的专家:
但我在三个任务上失败了:
| /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_texturedsp_init' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_avg_qpel8_mc32_old_c' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_texturedspenc_init' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_put_no_rnd_qpel16_mc32_old_c' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_put_no_rnd_qpel16_mc33_old_c' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_avg_qpel16_mc32_old_c' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_avg_dirac_pixels32_l4_c' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_put_dirac_pixels8_l2_c' | /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/recipe-sysroot-native/usr/bin/aarch64-oe-linux/../../libexec/aarch64-oe-linux/gcc/aarch64-oe-linux/13.3.0/ld: libavcodec/libavcodec.so: undefined reference to `ff_sheervideo_decoder' | collect2: error: ld returned 1 exit status | make: *** [/home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/ffmpeg-6.1.1/Makefile:133: ffmpeg_g] Error 1 | ERROR: oe_runmake failed | WARNING: /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683:183 exit 1 from 'exit 1' | WARNING: Backtrace (BB generated script): | #1: bbfatal_log, /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683, line 183 | #2: die, /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683, line 167 | #3: oe_runmake, /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683, line 162 | #4: autotools_do_compile, /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683, line 157 | #5: do_compile, /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683, line 152 | #6: main, /home/ht/yocto/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/ffmpeg/6.1.1/temp/run.do_compile.2329683, line 196 ERROR: Task (/home/ht/yocto/tisdk/sources/oe-core/meta/recipes-multimedia/ffmpeg/ffmpeg_6.1.1.bb:do_compile) failed with exit code '1' NOTE: Tasks Summary: Attempted 12919 tasks of which 12916 didn't need to be rerun and 3 failed. NOTE: Writing buildhistory NOTE: Writing buildhistory took: 6 seconds NOTE: Writing buildhistory NOTE: Writing buildhistory took: 5 seconds Summary: 3 tasks failed: /home/ht/yocto/tisdk/sources/oe-core/meta/recipes-devtools/binutils/binutils_2.42.bb:do_compile /home/ht/yocto/tisdk/sources/meta-qt5/recipes-qt/qt5/qtbase-native_git.bb:do_configure /home/ht/yocto/tisdk/sources/oe-core/meta/recipes-multimedia/ffmpeg/ffmpeg_6.1.1.bb:do_compile Summary: There were 6 ERROR messages, returning a non-zero exit code.我试图删除整个 tisdk 文件夹,并重做了一切,但得到了 thoese 失败一次又一次。
我使用的是 Ubuntu 22.04。 造成此问题的原因可能是什么?
此致、
Adam