请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SK-AM68 工具与软件:
我使用的是 09.02.00.05 SDK、由于补丁无法正常运行、这些步骤无法正常运行。 有人想解决问题吗?
software-dl.ti.com/.../faq.html
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
我使用的是 09.02.00.05 SDK、由于补丁无法正常运行、这些步骤无法正常运行。 有人想解决问题吗?
software-dl.ti.com/.../faq.html
尊敬的 Fheem:
[quote userid="616101" url="~/support/processors-group/processors/f/processors-forum/1459024/sk-am68-error-due-to-streaming-multiple-usb-cameras 由于补丁无法使用。您是否意味着无法正确应用补丁?
您能否共享错误日志?
这是当我做一个干式的贴片时得到的
(Stripping trailing CRs from patch; use --binary to disable.) checking file p1 Hunk #1 FAILED at 33. Hunk #2 FAILED at 2389. 2 out of 2 hunks FAILED (Stripping trailing CRs from patch; use --binary to disable.) checking file p1 Hunk #1 FAILED at 196. 1 out of 1 hunk FAILED (Stripping trailing CRs from patch; use --binary to disable.) checking file p1 Hunk #1 FAILED at 718. 1 out of 1 hunk FAILED patch unexpectedly ends in middle of line
有更新吗? 我还尝试手动应用补丁中的更改、结果是这样。
~/ti-processor-sdk-linux-edgeai-j721s2-evm-09_02_00_05/board-support/ti-linux-kernel-6.1.80+gitAUTOINC+2e423244f8-ti$ make ARCH=arm64 CROSS_COMPILE="$CROSS_COMPILE_64" ./drivers/media/usb/uvc/uvcvideo.ko
SYNC include/config/auto.conf.cmd
HOSTCC scripts/dtc/dtc.o
HOSTCC scripts/dtc/flattree.o
HOSTCC scripts/dtc/fstree.o
HOSTCC scripts/dtc/data.o
HOSTCC scripts/dtc/livetree.o
HOSTCC scripts/dtc/treesource.o
HOSTCC scripts/dtc/srcpos.o
HOSTCC scripts/dtc/checks.o
HOSTCC scripts/dtc/util.o
LEX scripts/dtc/dtc-lexer.lex.c
YACC scripts/dtc/dtc-parser.tab.[ch]
HOSTCC scripts/dtc/dtc-lexer.lex.o
HOSTCC scripts/dtc/dtc-parser.tab.o
HOSTLD scripts/dtc/dtc
HOSTCC scripts/dtc/libfdt/fdt.o
HOSTCC scripts/dtc/libfdt/fdt_ro.o
HOSTCC scripts/dtc/libfdt/fdt_wip.o
HOSTCC scripts/dtc/libfdt/fdt_sw.o
HOSTCC scripts/dtc/libfdt/fdt_rw.o
HOSTCC scripts/dtc/libfdt/fdt_strerror.o
HOSTCC scripts/dtc/libfdt/fdt_empty_tree.o
HOSTCC scripts/dtc/libfdt/fdt_addresses.o
HOSTCC scripts/dtc/libfdt/fdt_overlay.o
HOSTCC scripts/dtc/fdtoverlay.o
HOSTLD scripts/dtc/fdtoverlay
HOSTCC scripts/kallsyms
HOSTCC scripts/sorttable
HOSTCC scripts/asn1_compiler
WRAP arch/arm64/include/generated/uapi/asm/kvm_para.h
WRAP arch/arm64/include/generated/uapi/asm/errno.h
WRAP arch/arm64/include/generated/uapi/asm/ioctl.h
WRAP arch/arm64/include/generated/uapi/asm/ioctls.h
WRAP arch/arm64/include/generated/uapi/asm/ipcbuf.h
WRAP arch/arm64/include/generated/uapi/asm/msgbuf.h
WRAP arch/arm64/include/generated/uapi/asm/poll.h
WRAP arch/arm64/include/generated/uapi/asm/resource.h
WRAP arch/arm64/include/generated/uapi/asm/sembuf.h
WRAP arch/arm64/include/generated/uapi/asm/shmbuf.h
WRAP arch/arm64/include/generated/uapi/asm/siginfo.h
WRAP arch/arm64/include/generated/uapi/asm/socket.h
WRAP arch/arm64/include/generated/uapi/asm/sockios.h
WRAP arch/arm64/include/generated/uapi/asm/stat.h
WRAP arch/arm64/include/generated/uapi/asm/swab.h
WRAP arch/arm64/include/generated/uapi/asm/termbits.h
WRAP arch/arm64/include/generated/uapi/asm/termios.h
WRAP arch/arm64/include/generated/uapi/asm/types.h
WRAP arch/arm64/include/generated/asm/early_ioremap.h
WRAP arch/arm64/include/generated/asm/mcs_spinlock.h
WRAP arch/arm64/include/generated/asm/qrwlock.h
WRAP arch/arm64/include/generated/asm/qspinlock.h
WRAP arch/arm64/include/generated/asm/parport.h
WRAP arch/arm64/include/generated/asm/user.h
WRAP arch/arm64/include/generated/asm/bugs.h
WRAP arch/arm64/include/generated/asm/delay.h
WRAP arch/arm64/include/generated/asm/div64.h
WRAP arch/arm64/include/generated/asm/dma-mapping.h
WRAP arch/arm64/include/generated/asm/dma.h
WRAP arch/arm64/include/generated/asm/emergency-restart.h
WRAP arch/arm64/include/generated/asm/hw_irq.h
WRAP arch/arm64/include/generated/asm/irq_regs.h
WRAP arch/arm64/include/generated/asm/kdebug.h
WRAP arch/arm64/include/generated/asm/kmap_size.h
WRAP arch/arm64/include/generated/asm/local.h
WRAP arch/arm64/include/generated/asm/local64.h
WRAP arch/arm64/include/generated/asm/mmiowb.h
WRAP arch/arm64/include/generated/asm/msi.h
WRAP arch/arm64/include/generated/asm/serial.h
WRAP arch/arm64/include/generated/asm/softirq_stack.h
WRAP arch/arm64/include/generated/asm/switch_to.h
WRAP arch/arm64/include/generated/asm/trace_clock.h
WRAP arch/arm64/include/generated/asm/unaligned.h
WRAP arch/arm64/include/generated/asm/vga.h
UPD include/config/kernel.release
UPD include/generated/uapi/linux/version.h
UPD include/generated/utsrelease.h
UPD include/generated/compile.h
GEN arch/arm64/include/generated/asm/cpucaps.h
GEN arch/arm64/include/generated/asm/sysreg-defs.h
CC scripts/mod/empty.o
HOSTCC scripts/mod/mk_elfconfig
MKELF scripts/mod/elfconfig.h
HOSTCC scripts/mod/modpost.o
CC scripts/mod/devicetable-offsets.s
UPD scripts/mod/devicetable-offsets.h
HOSTCC scripts/mod/file2alias.o
HOSTCC scripts/mod/sumversion.o
HOSTLD scripts/mod/modpost
UPD include/generated/timeconst.h
CC kernel/bounds.s
UPD include/generated/bounds.h
CC arch/arm64/kernel/asm-offsets.s
UPD include/generated/asm-offsets.h
CALL scripts/checksyscalls.sh
CHKSHA1 include/linux/atomic/atomic-arch-fallback.h
CHKSHA1 include/linux/atomic/atomic-instrumented.h
CHKSHA1 include/linux/atomic/atomic-long.h
LDS arch/arm64/kernel/vdso/vdso.lds
CC arch/arm64/kernel/vdso/vgettimeofday.o
AS arch/arm64/kernel/vdso/note.o
AS arch/arm64/kernel/vdso/sigreturn.o
LD arch/arm64/kernel/vdso/vdso.so.dbg
VDSOSYM include/generated/vdso-offsets.h
OBJCOPY arch/arm64/kernel/vdso/vdso.so
CC [M] drivers/media/usb/uvc/uvc_driver.o
CC [M] drivers/media/usb/uvc/uvc_queue.o
CC [M] drivers/media/usb/uvc/uvc_v4l2.o
CC [M] drivers/media/usb/uvc/uvc_video.o
drivers/media/usb/uvc/uvc_video.c: In function ‘uvc_fixup_video_ctrl’:
drivers/media/usb/uvc/uvc_video.c:240:17: error: implicit declaration of function ‘uvc_trace’ [-Werror=implicit-function-declaration]
240 | uvc_trace(UVC_TRACE_VIDEO,
| ^~~~~~~~~
drivers/media/usb/uvc/uvc_video.c:240:27: error: ‘UVC_TRACE_VIDEO’ undeclared (first use in this function); did you mean ‘UVC_DBG_VIDEO’?
240 | uvc_trace(UVC_TRACE_VIDEO,
| ^~~~~~~~~~~~~~~
| UVC_DBG_VIDEO
drivers/media/usb/uvc/uvc_video.c:240:27: note: each undeclared identifier is reported only once for each function it appears in
cc1: some warnings being treated as errors
make[5]: *** [scripts/Makefile.build:250: drivers/media/usb/uvc/uvc_video.o] Error 1
make[4]: *** [scripts/Makefile.build:502: drivers/media/usb/uvc] Error 2
make[3]: *** [scripts/Makefile.build:502: drivers/media/usb] Error 2
make[2]: *** [scripts/Makefile.build:502: drivers/media] Error 2
make[1]: *** [scripts/Makefile.build:502: drivers] Error 2
make: *** [Makefile:2010: .] Error 2尊敬的 Faheem:
我们的软件团队尚未能够对此做出响应。
复制我的朋友 Brijesh Jadav 的评论。