This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:[ Edgeai image ]使用 cmake find_package 生成时出现 OpencvConfig 错误

Guru**** 2455360 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1487256/tda4vm-edgeai-image-opencvconfig-error-is-occured-when-build-using-cmake-find_package

器件型号:TDA4VM

工具与软件:

您好!

Hhere 是对我的程序执行 find_package (需要 OpenCV)的结果。

The imported target "multiview" references the file
[cmake] 
[cmake]      "/usr/lib/opencv4/3rdparty/libmultiview.a"
[cmake] 
[cmake]   but this file does not exist.  Possible reasons include:
[cmake] 
[cmake]   * The file was deleted, renamed, or moved to another location.
[cmake] 
[cmake]   * An install or uninstall procedure did not complete successfully.
[cmake] 
[cmake]   * The installation package was faulty and contained
[cmake] 
[cmake]      "/usr/lib/cmake/opencv4/OpenCVModules.cmake"
[cmake] 
[cmake]   but not all the files it references.
[cmake] 
[cmake] Call Stack (most recent call first):
[cmake]   /usr/lib/cmake/opencv4/OpenCVConfig.cmake:126 (include)
[cmake]   modules/vision/CMakeLists.txt:18 (find_package)

我检查了路径并确认没有3rdparty 目录。
不存在文件或目录"/usr/lib/opencv4/3rdparty /"
libconfentence.a 也出现了同样的问题、但我暂时修改了 OpenCVConfig、只检查了错误消息。

如果我直接指定它而不使用 find_package、则会正常构建、但我想使用 find_package 构建应用程序。

我修改了 OpenCVConfig (注释掉了相应的器件)并确认 cmake 中没有错误。

我需要的解决方案是在 TI SDK 中创建映像时解决该问题。

1.修改,以便在创建映像时可以正常构建和添加丢失的软件包。
2.修改、使配置文件在创建映像时不涉及第三方程序的相关信息。

是否有办法实现上述目标?

BR、

Lee

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Lee:

    我们 在发行版中不支持 OpenCV。  

    此致、

    Brijesh