This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VEN-Q1:锁定所有 RX 端口失败

Guru**** 2460850 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1491213/tda4ven-q1-failed-to-lock-all-rx-ports

器件型号:TDA4VEN-Q1

工具与软件:

大家好、我在 uEnv.txt 中添加了两个.dbto (融合板和 imx390)并重新启动。 然后、运行`apps_cpp/bin/Release/app_edgeai configs/imx390_cam_example.yaml`并进行报告

root@j722s-evm:/opt/edgeai-gst-apps# apps_cpp/bin/Release/app_edgeai configs/imx390_cam_example.yaml
libtidl_onnxrt_EP loaded 0x2e0d9610 
Final number of subgraphs created are : 1, - Offloaded Nodes - 283, Total Nodes - 283 
APP: Init ... !!!
   138.458833 s: MEM: Init ... !!!
   138.458925 s: MEM: Initialized DMA HEAP (fd=5) !!!
   138.459185 s: MEM: Init ... Done !!!
   138.459217 s: IPC: Init ... !!!
   138.525037 s: IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
   138.533530 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
   138.533820 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
   138.533862 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
   138.533872 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
   138.535876 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-0 
   138.536538 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-1 
   138.536959 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-2 
   138.538131 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-3 
   138.538255 s:  VX_ZONE_INFO: [tivxInitLocal:126] Initialization Done !!!
   138.538324 s:  VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
[15:00:00.000.000000]:ERROR:[addGstPipeline:0256] Invalid source.
[15:00:00.000.000135]:ERROR:[initialize:2246] addGstPipeline() failed.
Segmentation fault (core dumped)
root@j722s-evm:/opt/edgeai-gst-apps#

root@j722s-evm:/opt/edgeai-gst-apps# dmesg | grep ds90
[    8.327960] ds90ub960 5-0036: supply vddio not found, using dummy regulator
[    8.356684] ds90ub960 5-0036: ub960_write: cannot write register 0x01 (-121)!
[    8.372234] ds90ub960 5-0036: reset failed: -121
[    8.372360] ds90ub960 5-0036: ub960_read: cannot read register 0x03 (-121)!
[    8.372372] ds90ub960 5-0036: error -EREMOTEIO: Cannot read first register, abort
[    8.382710] ds90ub960: probe of 5-0036 failed with error -121
[    8.399102] ds90ub960 5-003d: supply vddio not found, using dummy regulator
[    8.518177] ds90ub960 5-003d: Fixed dependency cycle(s) with /bus@f0000/ticsi2rx@30102000/csi-bridge@30101000
[    9.534897] ds90ub960 5-003d: error -EIO: Failed to lock all RX ports
[    9.551036] ds90ub960: probe of 5-003d failed with error -5

我使用 ds90ub954并将跳线连接到 IDX 以选择0x3D i2c 地址。 我还`在引导` i2cset -y 7 0x3D 0x01 0x03 μ s 后进行硬复位、但两者都不起作用。 我确信电路板位于正确的 i2c 总线上、而且.dtbo 生效、但./init_script.sh 未显示任何内容。

这个融合板是坏了还是漏掉了一些东西? 如果我更改为 ds90ub960、它会停留在:

root@j722s-evm:/opt/edgeai-gst-apps# ./apps_cpp/bin/Release/app_edgeai configs/imx390_cam_example.yaml
libtidl_onnxrt_EP loaded 0x1fe63f50 
Final number of subgraphs created are : 1, - Offloaded Nodes - 283, Total Nodes - 283 
APP: Init ... !!!
    77.363299 s: MEM: Init ... !!!
    77.363415 s: MEM: Initialized DMA HEAP (fd=5) !!!
    77.363767 s: MEM: Init ... Done !!!
    77.363803 s: IPC: Init ... !!!
    77.430531 s: IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
    77.439949 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
    77.445049 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
    77.445127 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
    77.445140 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
    77.448761 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-0 
    77.449211 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-1 
    77.449468 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-2 
    77.450118 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-3 
    77.450161 s:  VX_ZONE_INFO: [tivxInitLocal:126] Initialization Done !!!
    77.450211 s:  VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
graph
==========[INPUT PIPELINE(S)]==========

[PIPE-0]

v4l2src device=/dev/video-imx390-cam0 io-mode=5 ! queue leaky=2 ! capsfilter caps="video/x-bayer, width=(int)1936, height=(int)1100, format=(string)rggb12;" ! tiovxisp dcc-isp-file=/opt/imaging/imx390/linear/dcc_viss.bin sensor-name=SENSOR_SONY_IMX390_UB953_D3 format-msb=11 ! capsfilter caps="video/x-raw, format=(string)NV12;" ! tiovxmultiscaler name=multiscaler_split_00
multiscaler_split_00. ! queue ! capsfilter caps="video/x-raw, width=(int)484, height=(int)416;" ! tiovxmultiscaler target=1 ! capsfilter caps="video/x-raw, width=(int)416, height=(int)416;" ! tiovxdlpreproc out-pool-size=4 data-type=3 tensor-format=1 ! capsfilter caps="application/x-tensor-tiovx;" ! appsink max-buffers=2 drop=true name=flow0_pre_proc0
multiscaler_split_00. ! queue ! capsfilter caps="video/x-raw, width=(int)1280, height=(int)720;" ! tiovxdlcolorconvert out-pool-size=4 ! capsfilter caps="video/x-raw, format=(string)RGB;" ! appsink max-buffers=2 drop=true name=flow0_sensor0

==========[OUTPUT PIPELINE]==========

appsrc do-timestamp=true format=3 block=true name=flow0_post_proc0 ! tiovxdlcolorconvert ! capsfilter caps="video/x-raw, width=(int)1280, height=(int)720, format=(string)NV12;" ! queue ! mosaic0.sink0

tiovxmosaic target=1 background=/tmp/background0 name=mosaic0 src::pool-size=4
sink_0::startx="<320>" sink_0::starty="<150>" sink_0::widths="<1280>" sink_0::heights="<720>"
! capsfilter caps="video/x-raw, format=(string)NV12, width=(int)1920, height=(int)1080;" ! queue ! tiperfoverlay title=IMX390 Camera ! kmssink sync=false max-lateness=5000000 qos=true processing-deadline=15000000 driver-name=tidss connector-id=40 plane-id=31 force-modesetting=true fd=42

[17:45:14.000.000000]:ERROR:[getBuffer:0233] [flow0_pre_proc0] Could not get data from Gstreamer appsink.

此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     陈孟鸿

    您能否确保摄像机已连接到端口0
    另外、您能否分享您在 uEnv.txt 中添加的确切 dtbo 名称

    此致
    Rahul T R

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、我连接到 ub960的端口、标签贴纸1 (有1、2、3、4)、uEnv.txt 的修改内容是:

    name_overlages=ti/k3-j722s-vision-apps.dtbo ti/k3-j722s-evm-fpdlink-Fusion.dtbo ti/k3-fpdlink-imx390-0.dtbo

    此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     陈孟鸿

    看起来您使用的似乎是 ADAS SDK、
    在 ADAS 中、SDK 捕获在 R5F 中启用、在 Linux 中禁用

    请使用 EDGEAI SDK
    SDK-AM67A 软件开发套件(PROCESSOR-SDK-LINUX)|德州仪器 TI.com

    此致
    Rahul T R

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    嗨、ub960在重新安装 EDGEAI SDK 后可以正常工作、但 ub954仍抱怨:

    root@j722s-evm:/opt/edgeai-gst-apps# dmesg | grep ds90
    [    8.327960] ds90ub960 5-0036: supply vddio not found, using dummy regulator
    [    8.356684] ds90ub960 5-0036: ub960_write: cannot write register 0x01 (-121)!
    [    8.372234] ds90ub960 5-0036: reset failed: -121
    [    8.372360] ds90ub960 5-0036: ub960_read: cannot read register 0x03 (-121)!
    [    8.372372] ds90ub960 5-0036: error -EREMOTEIO: Cannot read first register, abort
    [    8.382710] ds90ub960: probe of 5-0036 failed with error -121
    [    8.399102] ds90ub960 5-003d: supply vddio not found, using dummy regulator
    [    8.518177] ds90ub960 5-003d: Fixed dependency cycle(s) with /bus@f0000/ticsi2rx@30102000/csi-bridge@30101000
    [    9.534897] ds90ub960 5-003d: error -EIO: Failed to lock all RX ports
    [    9.551036] ds90ub960: probe of 5-003d failed with error -5

    此致

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

     陈孟鸿

    您正在使用哪个版本的 imx390摄像头?
    有 CM 和 RCM、我们都有 dtbos

    我看到您正在应用 RCM、您能否尝试使用 cm dtbos

    此致
    Rahul T R