请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM620-Q1 主题中讨论的其他器件:AM62P
工具与软件:
嗨、专家
参考本页、
几个问题、
(1)我们是否具有缓冲器大小(字节) 128k/64k/16k 的测试结果?
(2)我们如何进行这些测试? 是否有实用程序支持?
谢谢你。
Gibbs
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
1.没有 文档中仅提到了可用的数字。
2.
这些命令用于触发 eMMC 测试。 请注意、这些命令仅在默认文件系统中可用。
cd /opt/ltp ./runltp -P am62pxx_sk-fs -f ddt/emmc_perf_ext4 -s "EMMC_L_PERF_EXT4_FIO_1G ",timeout=3600,perf_metrics_file=LSP/A-PCI/fio_parser.rb
随附是在 TI AM62P HSFS 电路板上收集的示例测试日志
root@am62pxx-evm:~# cd /opt/ltp/ root@am62pxx-evm:/opt/ltp# ./runltp -P am62pxx_sk-fs -f ddt/emmc_perf_ext4 -s "EMMC_L_PERF_EXT4_FIO_1G ",timeout=3600,perf_metrics_file=LSP/A-PCI/fio_parser.rb ... <<<test_start>>> tag=EMMC_L_PERF_EXT4_FIO_1G stime=170 cmdline="source 'common.sh'; install_modules.sh "emmc"; do_cmd 'blk_device_filesystem_perf_test.sh -p "fio" -f "ext4" -s 1g -B "4m 1m 256k 4k" -d "emmc" '" contacts="" analysis=exit <<<test_output>>> incrementing stop |TRACE LOG|Inside do_cmd:CMD=blk_device_filesystem_perf_test.sh -p "fio" -f "ext4" -s 1g -B "4m 1m 256k 4k" -d "emmc" | ls -al /dev/disk/by-id total 0 drwxr-xr-x 2 root root 160 Jan 1 00:00 . drwxr-xr-x 7 root root 140 Jan 1 00:00 .. lrwxrwxrwx 1 root root 13 Jan 1 00:00 mmc-G1M15L_0x2dc165d1 -> ../../mmcblk0 lrwxrwxrwx 1 root root 15 Jan 1 00:00 mmc-G1M15L_0x2dc165d1-part1 -> ../../mmcblk0p1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 mmc-G1M15L_0x2dc165d1-part2 -> ../../mmcblk0p2 lrwxrwxrwx 1 root root 13 Jan 1 00:00 mmc-SC16G_0x568ab999 -> ../../mmcblk1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 mmc-SC16G_0x568ab999-part1 -> ../../mmcblk1p1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 mmc-SC16G_0x568ab999-part2 -> ../../mmcblk1p2 ls -al /dev/disk/by-path total 0 drwxr-xr-x 2 root root 200 Jan 1 00:00 . drwxr-xr-x 7 root root 140 Jan 1 00:00 .. lrwxrwxrwx 1 root root 13 Jan 1 00:00 platform-fa00000.mmc -> ../../mmcblk1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 platform-fa00000.mmc-part1 -> ../../mmcblk1p1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 platform-fa00000.mmc-part2 -> ../../mmcblk1p2 lrwxrwxrwx 1 root root 13 Jan 1 00:00 platform-fa10000.mmc -> ../../mmcblk0 lrwxrwxrwx 1 root root 18 Jan 1 00:00 platform-fa10000.mmc-boot0 -> ../../mmcblk0boot0 lrwxrwxrwx 1 root root 18 Jan 1 00:00 platform-fa10000.mmc-boot1 -> ../../mmcblk0boot1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 platform-fa10000.mmc-part1 -> ../../mmcblk0p1 lrwxrwxrwx 1 root root 15 Jan 1 00:00 platform-fa10000.mmc-part2 -> ../../mmcblk0p2 |TRACE LOG|DEV_NODE return from get_blk_device_node is: /dev/mmcblk0p2| |TRACE LOG|STARTING FILE SYSTEM PERFORMANCE Test for emmc| |TRACE LOG|FS_TYPE:ext4| |TRACE LOG|DEV_NODE:/dev/mmcblk0p2| |TRACE LOG|MOUNT POINT:/mnt/partition_emmc| |TRACE LOG|BUFFER SIZES:4m 1m 256k 4k| |TRACE LOG|FILE SIZE:1gMB| |TRACE LOG|SRCFILE SIZE:10MB| |TRACE LOG|DEVICE_TYPE:emmc| |TRACE LOG|Inside do_cmd:CMD=printout_model /dev/mmcblk0p2 emmc| |TRACE LOG|model info is not available for non scsi devices.| |TRACE LOG|Inside do_cmd:CMD=printout_mmc_ios| |TRACE LOG|===== printout of mmc ios =====| |TRACE LOG|Inside do_cmd:CMD=cat /sys/kernel/debug//mmc0/ios| clock: 200000000 Hz actual clock: 200000000 Hz vdd: 7 (1.65 - 1.95 V) bus mode: 2 (push-pull) chip select: 0 (don't care) power mode: 2 (on) bus width: 3 (8 bits) timing spec: 10 (mmc HS400) signal voltage: 1 (1.80 V) driver type: 0 (driver type B) |TRACE LOG|Inside do_cmd:CMD=cat /sys/kernel/debug//mmc1/ios| clock: 200000000 Hz actual clock: 200000000 Hz vdd: 21 (3.3 ~ 3.4 V) bus mode: 2 (push-pull) chip select: 0 (don't care) power mode: 2 (on) bus width: 2 (4 bits) timing spec: 6 (sd uhs SDR104) signal voltage: 1 (1.80 V) driver type: 0 (driver type B) |TRACE LOG|===== end of mmc ios =====| |TRACE LOG|Device Partition Size is 22159 MB| /opt/ltp/testcases/bin/ddt/blk/blk_device_filesystem_perf_test.sh: line 186: [: 1g: integer expression expected |TRACE LOG|Inside do_cmd:CMD=mkdir -p /mnt/partition_emmc| |TRACE LOG|Inside do_cmd:CMD=blk_device_prepare_format.sh -d emmc -n /dev/mmcblk0p2 -f ext4 -m /mnt/partition_emmc -o async| |TRACE LOG|DEV_NODE: /dev/mmcblk0p2| |TRACE LOG|MNT_POINT: /mnt/partition_emmc| |TRACE LOG|FS_TYPE: ext4| |TRACE LOG|MNT_MODE: async| |TRACE LOG|Erasing/Formatting this partition and then mount it| |TRACE LOG|Inside do_cmd:CMD=blk_device_erase_format_part.sh -d emmc -n /dev/mmcblk0p2 -f ext4 -m /mnt/partition_emmc| |TRACE LOG|DEVICE TYPE: emmc| |TRACE LOG|DEVICE NODE: /dev/mmcblk0p2| |TRACE LOG|FS TYPE: ext4| |TRACE LOG|Umount /dev/mmcblk0p2 or /dev/mmcblk0 if it is mounted| /dev/mmcblk0p2 on /run/media/mmcblk0p2 type ext4 (rw,relatime) |TRACE LOG|Inside do_cmd:CMD=umount /dev/mmcblk0p2| [ 225.579004] EXT4-fs (mmcblk0p2): unmounting filesystem. |TRACE LOG|Inside do_cmd:CMD=mkfs.ext4 -E lazy_itable_init=1,lazy_journal_init=1 -F /dev/mmcblk0p2| mke2fs 1.46.5 (30-Dec-2021) /dev/mmcblk0p2 contains a ext4 file system last mounted on /mnt/partition_emmc on Thu Jan 1 00:00:14 1970 Discarding device blocks: done Creating filesystem with 5672704 4k blocks and 1419840 inodes Filesystem UUID: b255230c-952f-4a02-889b-d876c022f9e0 Superblock backups stored on blocks: 32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208, 4096000 Allocating group tables: done Writing inode tables: done Creating journal (32768 blocks): done Writing superblocks and filesystem accounting information: done |TRACE LOG|Inside do_cmd:CMD=blk_device_do_mount.sh -n /dev/mmcblk0p2 -f ext4 -d emmc -m /mnt/partition_emmc -o async| |TRACE LOG|Umount /mnt/partition_emmc if it is mounted| |TRACE LOG|Mounting the partition| |TRACE LOG|Inside do_cmd:CMD=mount -t ext4 -o async /dev/mmcblk0p2 /mnt/partition_emmc| [ 231.220650] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Quota mode: none. |TRACE LOG|Inside do_cmd:CMD=mount | grep /mnt/partition_emmc| /dev/mmcblk0p2 on /mnt/partition_emmc type ext4 (rw,relatime) |TRACE LOG|BUFFER SIZE = 4m| |TRACE LOG|Inside do_cmd:CMD=fio --name emmc_TEST --directory=/mnt/partition_emmc --size=1g --rw=write --blocksize=4m --ioengine=libaio --iodepth=4 --numjobs=1 --direct=1 --group_reportin| |TRACE LOG|Inside do_cmd:CMD=sleep 5| emmc_TEST: (g=0): rw=write, bs=(R) 4096KiB-4096KiB, (W) 4096KiB-4096KiB, (T) 4096KiB-4096KiB, ioengine=libaio, iodepth=4 fio-3.30 Starting 1 process emmc_TEST: Laying out IO file (1 file / 1024MiB) |TRACE LOG|Inside do_cmd:CMD=wait| emmc_TEST: (groupid=0, jobs=1): err= 0: pid=2324: Thu Jan 1 00:04:57 1970 write: IOPS=22, BW=90.5MiB/s (94.9MB/s)(5440MiB/60135msec); 0 zone resets slat (usec): min=571, max=131328, avg=4630.99, stdev=7924.73 clat (msec): min=36, max=4259, avg=172.09, stdev=205.33 lat (msec): min=71, max=4261, avg=176.73, stdev=205.02 clat percentiles (msec): | 1.00th=[ 106], 5.00th=[ 150], 10.00th=[ 150], 20.00th=[ 153], | 30.00th=[ 159], 40.00th=[ 163], 50.00th=[ 163], 60.00th=[ 163], | 70.00th=[ 165], 80.00th=[ 165], 90.00th=[ 167], 95.00th=[ 169], | 99.00th=[ 201], 99.50th=[ 236], 99.90th=[ 4212], 99.95th=[ 4245], | 99.99th=[ 4245] bw ( KiB/s): min= 8192, max=106496, per=100.00%, avg=98358.92, stdev=9635.52, samples=113 iops : min= 2, max= 26, avg=23.93, stdev= 2.36, samples=113 lat (msec) : 50=0.07%, 100=0.88%, 250=98.68%, >=2000=0.37% cpu : usr=1.99%, sys=2.60%, ctx=11075, majf=0, minf=22 IO depths : 1=0.1%, 2=0.1%, 4=99.8%, 8=0.0%, 16=0.0%, 32=0.0%, >=64=0.0% submit : 0=0.0%, 4=100.0%, 8=0.0%, 16=0.0%, 32=0.0%, 64=0.0%, >=64=0.0% complete : 0=0.0%, 4=100.0%, 8=0.0%, 16=0.0%, 32=0.0%, 64=0.0%, >=64=0.0% issued rwts: total=0,1360,0,0 short=0,0,0,0 dropped=0,0,0,0 latency : target=0, window=0, percentile=100.00%, depth=4 Run status group 0 (all jobs): WRITE: bw=90.5MiB/s (94.9MB/s), 90.5MiB/s-90.5MiB/s (94.9MB/s-94.9MB/s), io=5440MiB (5704MB), run=60135-60135msec ...
此致、
Prashant